Toshiba Satellite P50-AST3NX1 Laptop

Average Customer Rating:
Free ground shipping on laptops $499+
up to $50 OFF Microsoft Office

Limit 5 per household

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Issues with External WiFi

POSTED BY: Pete , St Louis
Overall rating: 4 out of 5 4 out of 5

Great product especially for the price point. I was looking for a 4th gen I7 with BueRay. I've always had good luck with Toshiba laptops at work. This is my first laptop for home use. HOWEVER - I should have upgraded the WI-Fi at purchase. Compatibility issues now in trying to get an ASUS USB-AC56 (USB3.0) with the existing Toshiba WIFI drivers - even when disabling the Toshiba drivers. Soooo sad.

good value and features for the price

POSTED BY: First time reviewer
Overall rating: 4 out of 5 4 out of 5

I have an older Toshiba ultrabook that was working just fine but I wanted to get something a bit larger that had a full keyboard. After quite a long search, I came up with this one. It has all the features I was looking for: Full backlit keyboard and a full HD screen. The only thing it lacked was a touch screen. But the last wasn't a priority. The only thing I wasn't thrilled about was Windows 8. After using it for a couple months I am pleased with it. It is pretty speedy. I like the size and weight and everything works just fine. The battery life isn't quite a good as my ultrabook but it is better than my last full sized laptop. I have even managed to banish most of the Windows 8 features I don't like. Unless something unexpected happens, I can see this being my main laptop for a few years.
  • $1,099.99
  • -$250.00
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $849.99
  • »
  • Free Ground Shipping

add to cart
  • Laptop summary This product is prebuilt.
  • Intel® Core™ i5-4200U Processor
  • Windows 8.1
  • 12GB DDR3L 1600MHz memory (max 16GB)
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Intel® Dual Band Wireless-N 7260 2x2 AC Plus Bluetooth
  • Bluetooth® V4.0
  • Buttonless touchpad pointing device with multi-touch control
  • One Touch Function Keys
  • Premium Frameless LED Backlit Raised Tile Keyboard with 10-Keypad (black)
  • Li-Ion (43Wh, 4-Cell)
  • 1-USB (3.0) port
  • 1-USB (3.0) port with USB Sleep and Charge
  • 2-USB (2.0) ports
  • Accessories Added: