Toshiba Satellite P70-ABT3G22 Laptop

This product will be custom-built for you.

Average Customer Rating:
up to $50 OFF Microsoft OfficeFREE 8GB MEMORYFREE 1TB Hybrid Drive
Free ground shipping on laptops $499+

Limit 5 per household
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

The lap top is great.

POSTED BY: Bree
Overall rating: 5 out of 5 5 out of 5

I like the laptop. I installed an SSD as my operating system drive, and use the HDD that it came with as my secondary drive, and it is fast. And I am also a fan of Windows 8.1.

Great Laptop

POSTED BY: JG , Portland, OR
Overall rating: 5 out of 5 5 out of 5

Pros: (1) Very fast ( I ordered mine with SSD primary). Photoshop and Lightroom open quickly. CPU intensive tasks perform extremely well. (2) Comfortable keyboard, feels solid - I like the separate number keypad (3) Easy customization to your liking (4) Shipping was fast. Received 3 days earlier than expected, even though it shipped from China (although I'm on the west coast, your experience may vary) (5) I wanted to upgrade the 8GB of RAM. I like how Toshiba left the easy-to-access RAM slots open, and put factory installed RAM in harder-to-access RAM slots. They also left the easy-to-access third HD slot open for future expansion (yes, you can have 3 HDs in this beast). Well done Toshiba for this detail! (6) Price. I dare you to find a comparable laptop with SSD primary, second HD, 2GB separate graphics card and i7 CPU for less. No one comes close. Cons: (1) The function keys. You can't use ALT+F4 to close an application. You have to use Fn+ALT+F4. Maybe there is a way to override this functionality? I haven't looked hard enough. (2) Windows 8. Wish you could have a Windows 7 option (3) The display is nice, but wish it were more matte than glossy. I work on a lot of photos. For critical work, I use my main professional graphics monitor, but for on-the-road work, this laptop serves nicely. Is it heavy? Yes. Does the battery not last very long? Yes. Do I care? No. I bought this as a desktop replacement. Weight and battery life are not issues with me. If they are important to you, don't get this model. Get something with a smaller footprint.

Pretty Good Laptop

POSTED BY: Customer
Overall rating: 4 out of 5 4 out of 5

If you are a demanding customer, this laptop's more likely not to be suitable for you. Pros: + 1920x1080 display w/ LED; + 17.3" screen; + Full keyboard w/ back-light; + Fast booting; + 4th Gen. Intel i7; + NVidia Graphics (GT 740M). Cons: - Battery life's about 2h, as expected; - Battery charger makes noise, specially when the laptop is at heavy duty; - The fan decides to make noise even when the laptop is on, though not doing anything, rather than regular tasks, such as browsing sites that don't include plug-ins, on the foreground. Overall, if you don't bother with noise or having to plug the charger all the time, it's a very good computer for you.

Toshiba Satellite P70-ABT2G22

POSTED BY: MrMojo , New England
Overall rating: 3 out of 5 3 out of 5

BD drive's front bezel cover is VERY flimsy and must be used with care or it WILL snap off. Lousy battery life but expected <3 hours. Toshiba's basic Wifi chip is weak so you better upgrade to Intel's Wifi chip. Why does Toshiba NOT use the faster 7200rpm 1Tb HDD or its own SSD drives? It's available aftermarket and the HDD in the laptop I have was made by HGST, Hitachi's HDD unit. The keyboard is OK but the backlit lighting is TOO dull which explained why it was updated to feature better lighting! It figures that the replacement model has a better keyboard though just about everything else is almost the SAME! Performance is decent but make sure you buy the 1080 resolution screen. Recently upgraded the RAM from 12Gb to 16Gb as memory price has fallen somewhat. The average PC user won't use more than 8Gb but having slightly more does help esp. if you do lots of multimedia work. It's a decent laptop but it could've been better.

Select Processor What's This?

  • add $100.00

Select Microsoft® Operating System What's This?

  • add $99.99
  • add $199.99

Select Microsoft® Office Software What's This?


Select Memory What's This?

  • FREE
  • add $50.00
  • add $100.00
  • add $200.00
  • add $400.00
  • add $600.00

Select Hard Disk Drive What's This?

  • FREE
  • add $30.00
  • add $30.00

Select SSD Drive (Primary Drive if chosen) What's This?

  • add $300.00

Select 2nd Hard Disk Drive What's This?

  • add $80.00
  • add $110.00
  • add $200.00

Select Graphics Controller What's This?


Select Optical Drive What's This?

  • add $50.00
  • add $75.00

Select KeyBoard Color What's This?


Select Wireless LAN & Bluetooth® What's This?

  • add $25.00
  • add $45.00

Select Anti-Virus Software What's This?

  • add $49.99

Warranty Upgrades and Extended Service Plans 


Select Toshiba recommended accessories 


recommended accessories

Toshiba 120-Watt Global AC Adapter ($89.99 value)  

Keep a spare handy!
Save 20% for a limited time!

$71.99


Toshiba dynadock® U3.0 Universal USB 3.0 Docking Station ($179.99 value)  

Connect additional devices to your computer quickly and easily with one USB cable!

$149.99


Laplink® PCmover® Ultimate for PC (CD-ROM) ($49.99 value)  


Save 40% when purchased with this order!

$29.99


  • $1,189.99
  • 899.99
  • -$190.00
  • -$999.99
  • -$100.00
  • -$1089.99
  • $0.00
  • $0.00
  • $899.99
  • $899.99
  • »
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • Free Ground Shipping

add to cart

This product will be custom-built for you.

Estimated Ship Date from Toshiba is 05/06/2014.

  • laptop summary
    • Customized

  • Intel® Core™ i5-4200M Processor (3M Cache, up to 3.10GHz) with Intel® Turbo Boost Technology 2.0
  • Windows 8.1
  • 1 month trial for new Office 365 customers
  • 8GB DDR3L 1600MHz (4GB + 4GB)
  • 1.0TB (5400rpm); Hybrid 8G Serial ATA hard disk drive
  • No SSD Drive
  • No Secondary Hard Drive Installed
  • 2GB GDDR3 NVIDIA ® GeForce® GT 740M with Optimus™ Technology
  • DVD SuperMulti (+/-R double layer) drive
  • Premium Frameless LED Backlit Raised Tile Keyboard with 10-Keypad (black)
  • Wi-Fi® Wireless networking (802.11b/g/n)+ Bluetooth 4.0 (150Mbps)
  • Norton™ Internet Security 2013 (30-day trial subscription)
  • 1 Year Standard Limited Warranty (1 Year on Battery)
  • Accessories Added: