Satellite P755-S5269 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent

POSTED BY: ricko
Overall rating: 5 out of 5 5 out of 5

Excellent

Mid-range gaming/Multimedia Laptop

POSTED BY: lobby0ne , Fresno, CA
Overall rating: 5 out of 5 5 out of 5

For the price I got it, it has the features and hardware I was looking for! The Geforce GT540M is a very capable video card as it could play Unreal 3 at MAX settings with virtually no lag, even with about 16 players duking it out. I mostly use this laptop to do Photoshop while listening to music, downloading stuff, surfing for research and it has not bog down on me one bit. The only time it would slow down is when installing a program via CD/DVD media, then again, this could be the limits of the HDD. Well worth the price!

Great buy

POSTED BY: AbrahamGuitar , Tujunga, CA 91042
Overall rating: 5 out of 5 5 out of 5

2nd Gen i7, thin and portable despite large screen. Currently it is running Fedora 15 on a SSD drive and is awesome!

great laptop

POSTED BY: Trejos
Overall rating: 5 out of 5 5 out of 5

pro's: excellent performance great sound for a laptop executive design great keyboard mouse pad is good good graphics not for intensive gaming con's: very poor web cam graphic card is not so compatible with ubuntu system(you need to use experimetal driver) not so good battery life

Excellent Laptop

POSTED BY: Rocking RN
Overall rating: 5 out of 5 5 out of 5

I've owned a Toshiba laptop that served me well for years with dependable service. So far, this one appears to fall into that same mold. Fast trouble free setup. Because my eyesight isn't what it once was, I especially like the backlit screen. I was pleased to be able to buy an i7 computer at such a great price. It comes with 6GB of RAM which can be increased to 8gb max. This is the only thing I can think of that could be improved. Even still, it performs more than fast enough. I've yet to find anything wrong with it.

Fantastic Laptop

POSTED BY: cousin vinny , Hasbrouck Heights,NJ
Overall rating: 5 out of 5 5 out of 5

This laptop has everything you need plus everything you could want

Excellant Product with all required

POSTED BY: purushottam , india
Overall rating: 5 out of 5 5 out of 5

This laptop having everything what you need as professional required with fear price

I love this computer!

POSTED BY: misplacedtxn , saint louis, Mo
Overall rating: 5 out of 5 5 out of 5

I even got my daughter to buy one.

more than laptop

POSTED BY: mostafa
Overall rating: 5 out of 5 5 out of 5

its the best of the best just need to be 3d

Good Laptop

POSTED BY: Critter890 , Largo, FLorida
Overall rating: 5 out of 5 5 out of 5

Battery life is less than expected from the promotions, other than that I'm happy with it. It meets all my needs for graphic work and does well with movies. Not a gamer so I can't comment on that. Overall it's OK, would have been nice if the hard drive was 7200 rpm instead of 5400.

Short review

POSTED BY: JayCee , Tampa Bay, Fl
Overall rating: 5 out of 5 5 out of 5

This is my first laptop though I have been using my wifes for the last few years when not on my desktop. I purchased this laptop as a replacement for my old desktop and couldn't be happier with it's performance.

Love Toshibas in this family

POSTED BY: CK , Lincoln, NE
Overall rating: 5 out of 5 5 out of 5

I have had a Toshiba since 2001 and only bought a new one because I needed more capacity. I still have the older one, which is still going strong, and will gift it to some lucky person. When my husband needed a new computer a few years ago, he got a Toshiba because I have been so happy with mine.

excellent

POSTED BY: mhmdv
Overall rating: 5 out of 5 5 out of 5

excellent

POSTED BY: Anton
Overall rating: 5 out of 5 5 out of 5

Been using my new Laptop for a few months now and I like everything about it. I think these laptops are well built, perform great and are a value for the features.

Great game lap top!

POSTED BY: zman1331 , yelm, wa
Overall rating: 5 out of 5 5 out of 5

I have had this lap top for about a month now. I can say this lap top is great for gaming if you don't want to spend more than a thousand dollars and game. this is the computer to get. I can run Skyrim on max graphics, I also can run L.A Noire on max. Games that need internet like APB: "All Points Bulletin" runs great. the CPU runs like a champ iv peak it once when i was downloading 15 games at once all from steam. I totally recommend this to every one who want to game on the move like i do.

Almost Perfect

POSTED BY: Robbie , Argentina
Overall rating: 5 out of 5 5 out of 5

Excellent laptop, best buy by far! Compared features and price with competitors before buying and am very pleased I chose this Toshiba. Webcam is only negative feature.

Nice Laptop

POSTED BY: Catastrophe , RockHill, SC
Overall rating: 5 out of 5 5 out of 5

I really like the laptop, so far it is blowing through everything I give it. Even the fan works good, it tends to blow out cool air at times. I really like the light-up keyboard and the nVidia graphics card. Pros: i7 Processor, nVidia Graphics Card, Lit-Keyboard, Fan. Cons: Battery Life

Fantastic Value

POSTED BY: GGSL , Cerritos, CA.
Overall rating: 5 out of 5 5 out of 5

I bought the Toshiba P755 s5269 laptop about a month ago. It has performed flawlessly through all my tinkering of programs and settings. It is solid. Pros: Lighted keyboard, I7 CPU and "Briteview" screen. Cons: Battery life is a little short.

Better than average.

POSTED BY: vm
Overall rating: 4 out of 5 4 out of 5

For having an i7 intel core, I was expecting something much faster. My 2 year old HP, costing much less, performs at this speed. There is excellent screen resolution. Nice, loud speakers. Built quality is about average. If you want image resolution, it is great. Built and speed could be better.

Good CPU but Lame Audio volume

POSTED BY: HG , Eugene Oregon
Overall rating: 4 out of 5 4 out of 5

This PC has solid specs and lives up to them in actual use with one exception, its audio. Oh, it is fine through an external speaker or headphone, but its maximum volume through its own built in harman/kardon speakers wouldn’t get me into trouble in the library reading room. I’ve checked every setting to see if the factory preset set the volume to half power or something, but I haven’t been able to boost the volume more than a couple of dbs. Without headphones, watching a movie or playing a game is very disappointing. I mean what’s the use of listening to a Blue ray with a heart pumping sound track with sound down so low you constantly want to turn it up and it is already at 100%. I just don’t understand this especially when my wife’s satellite (an M645) uses the same internal speakers and it has impressive sound volumes. So beware if sound volume matters to you then I recommend that you actually hear this laptop for yourself before you buy it.

Great Value/Performance

POSTED BY: JMc , Knoxville, TN
Overall rating: 4 out of 5 4 out of 5

More features for the money...great value.

Great value for the money!

POSTED BY: Texan
Overall rating: 4 out of 5 4 out of 5

I've had this laptop for about a month, and so far, have been very satisfied. Every time I get on it I discover some new feature that I didn't know was there. I only wish the battery would last a little longer than 3 or 4 hours, but other than that, I really don't have any complaints. This laptop is loaded with goodies which makes it a great value for the money.

Descent Laptop

POSTED BY: T-Lo , San Antonio, TX
Overall rating: 4 out of 5 4 out of 5

The laptop is working pretty fast. It has a very nice display. The fan, even though it is pretty quite, turns periodically on and off, which is pretty annoying. The battery partially discharges over night, even though the computer is off and all USB-ports are disabled. I like the display. My games are displayed very nicely, the performance of the graphic card is excellent. However, it requires constant cooling. The keyboard is fun to write with. The manual for the computer has a large room for improvement.

Good Machine, but too much Bloatware

POSTED BY: Coach Gadget , Crystal Mountain, !@
Overall rating: 4 out of 5 4 out of 5

This is my 2nd Toshiba laptop. I have found them to be strong and reliable, but loaded with too much junk software from the factory. I reloaded my last one from scratch and it worked much better/faster. This machine leaves my old one in the dust, but it is bogged down too. My i3 desktop is much faster than this i7 laptop because I loaded it from scratch. Please Toshiba: make it easier to buy/use a laptop without all the extra junk.

Very good

POSTED BY: jos
Overall rating: 4 out of 5 4 out of 5

This is ok

Good Laptop

POSTED BY: jsacerot , Bogotá D.C., Colombia
Overall rating: 4 out of 5 4 out of 5

It need a best video card.

Very satisfied

POSTED BY: ael , Kentucky
Overall rating: 4 out of 5 4 out of 5

i work for another computer maker, but decided to buy another's over theirs even with employee discount. I considered 2 other makers before settling on this unit. I'm very pleased with the unit's features and performance.

Great computer unless you want a good webcam

POSTED BY: lmccat , Las Vegas, NV
Overall rating: 4 out of 5 4 out of 5

I've only had this computer for under a week, but so far, so good. The dedicated 1GB of memory for the graphics is one of the reasons why I purchased this machine. The Core i7 processor was another. I wanted a desktop replacement and I believe it fits that purpose. However, if you really want a great webcam, run away from this machine. I'm very surprised that Toshiba put such a lousy webcam on a higher budget machine. The rest of the machine is great. Super fast processor with the core i7. 6GB of Ram, upgradeable to 8GB (although I would prefer if they would be upgradeable to 16GB). Love the design and durability. Great machine, but again, lacking on the webcam. To put it into perspective, it feels like a webcam from 1990. It's really bad quality.

Great Laptop with Dedicated Graphics

POSTED BY: lmccat , Las Vegas, NV
Overall rating: 4 out of 5 4 out of 5

This laptop performs fast once you remove most of the Mfr software which bloats it down. The Core i7 processor is top of the line, and the it comes packed with 6GB of Ram, 1GB Dedicated Nvidia Graphics and a 750GB HD. It's a perfect desktop replacement, which is what I bough it for. The only items Toshiba needs to address on this model is too much MFR software loaded on the machine actually slows it down tremendously. It would be nice to have a model that upgrades to 16GB of RAM instead of just 8GB (I've already maxed out mine to 8GB). And, the worst thing of all on this computer... the webcam. You may not care about this, but with all the new video chat programs, which I like to use Skype, it really is a huge disappointment that Toshiba would have done everything else right except for the webcam. I'll have to plug in a better quality USB camera if I plan on using a webcam. All in all, great computer, good looking, fast and responsive.

A very good Laptop

POSTED BY: draco9388 , Barranquilla, Colombia
Overall rating: 4 out of 5 4 out of 5

I'm a Graphic Designer, and to be able to say that I can run, 3 or more design programs at the same time in this laptop, it just says everything about it, is a powerful laptop, with a very good graphics. 100% recommended

pretty good!!

POSTED BY: kim , brooklyn,ny
Overall rating: 4 out of 5 4 out of 5

This model is pretty good . I like the back light on the keyboard and the features are cool but it could have used a dvd burn and battery could last a lot longer.

Worst Laptop EVER!!!

POSTED BY: Susie , Haleyville, Ala
Overall rating: 1 out of 5 1 out of 5

I have had it for 4 months. It has been sent back 4 times. Still not working correctly. 1st webcam didn't work. disk drive tore up, DVD makes terrible noise, disk drive door fell off, has just been a terrible experience! Will NEVER buy another Toshiba product!!!

MSRP: $979.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-2630QM processor
  • Windows 7 Home Premium (64-bit)
  • 6GB DDR3 1333MHz memory
  • 1GB GDDR3 NVIDIA® GeForce® GT 540M with NVIDIA® Optimus™ Technology
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories