Satellite P755-S5285 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent Product

POSTED BY: none , OR
Overall rating: 5 out of 5 5 out of 5

This computer runs hard and runs cool. I recently compared it to 2 other computers running a slide show. One got so hot it kept shutting off, the other got very warm but remained running. This Toshiba ran without getting noticeably warm for 8 hours of use. I am impressed.

shes a beast

POSTED BY: bobbo , ft. worth, texaas
Overall rating: 5 out of 5 5 out of 5

I love this cpu. For the first time ever, i can multitask without it locking up or freezeing up. The harmon kardon speakers, niceeeee. On looks shes a 10. watching movies, the picture is sweet. If i had to find a flaw, it would b all the apps that were preloaded and running. Should have let me choose.

Great features vs Price

POSTED BY: FPY , Manila, Philippines
Overall rating: 5 out of 5 5 out of 5

The display is very large, crisp and bright. Although battery life could use a boost, the ecoSave function is very helpful.I really like the full keyboard and the pinch-zoom display. The quick access keys on the keyboard are really useful plus the 5 usb ports (1 usb 3.0). Nice laptop overall.

First Laptop

POSTED BY: GG , St. Charles, IL
Overall rating: 4 out of 5 4 out of 5

Like the way it looks and I can take it with me.

Sleek and Savy

POSTED BY: Linjeans , St. John, IN
Overall rating: 4 out of 5 4 out of 5

This is the first Toshiba I have owned or worked on. It has far more capabilities than I expected. Although only for casual home use I look forwad to my journey! it sure looks good.

MSRP: $779.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-2630QM processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD SuperMulti (+/-R single layer) drive

shop for accessories