Toshiba Satellite S50-AST3NX1 Laptop

Average Customer Rating:
Free ground shipping on laptops $499+
up to $50 OFF Microsoft Office

Limit 5 per household

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent Laptop !

POSTED BY: T-Cat , Johnson, Vermont 05656
Overall rating: 5 out of 5 5 out of 5

Fast and user Friendly !!!

A GREAT Laptop!

POSTED BY: John , Carbondale, IL
Overall rating: 5 out of 5 5 out of 5

I have used laptops by a number of manufacturers over the years and Toshiba's laptops (this is my second one) are hands-down, the best on the market! The display is excellent, the keyboard has a good feel when typing, the batteries last a long time between charges, and the features you get for the price are excellent.

A good laptop

POSTED BY: john , buffalo ny
Overall rating: 4 out of 5 4 out of 5

My S50-A laptop arrived in a timely fashion. All components and functions seemed to work as expected, except for the WiFi connection. Toshiba support spent well over an hour with me on the phone, trying to diagnose the problem with WiFi. All the diagnostic tests came up negative (i.e. all components, both hardware and software, were operating properly). No further problems have been encountered. There was a significant 'learning curve' associated with Windows 8.1, but I finally overcame the challenge. Toshiba support was also very helpful in answering several other technical questions, and I commend them on their understanding and willingness to help.

Toshiba Lap Top

POSTED BY: Elk , Madison, Wi
Overall rating: 4 out of 5 4 out of 5

Recently I purchased a new Toshiba Satellite S50-AST3NX1 Laptop. The product is clean, well designed and very easy to use. It is lightweight and loaded with apps. Lot of pros to this. The more I use it, the more I like it. The downside: I had to create a Microsoft email account to "get started"......and everytime I login, I have to login to that account. It's possible I can delete it and just haven't explored enough, but forcing a user into a product they don't need or want is petty.....Although Windows 8 is pretty slick, I was surprised when I found out Microsoft Office was not included. I have purchased dozens of computers for personal and business use and this is the first that didn't ship with Office. I didn't even think to check on this as I just assumed it would be there. My mistake.....and I bought two of these. With that said, I would probably by another but I would check the competitors for features/price and make sure it has everything I needed and was not forced to use products I don't want.

SIGNIFICANT TROUBLE WITH TOUCHPAD

POSTED BY: UNSATISFIED USER , AVENTURA , FLORIDA
Overall rating: 2 out of 5 2 out of 5

DON'T LIKE IT!
  • $799.99
  • -$100.00
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $699.99
  • »
  • Free Ground Shipping

add to cart
  • Laptop summary This product is prebuilt.
  • Intel® Core™ i5-4200U Processor
  • Windows 8.1
  • 12GB DDR3L 1600MHz memory (max 16GB)
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Intel® Dual Band Wireless-N 7260 2x2 AC Plus Bluetooth
  • Bluetooth® V4.0
  • Buttonless touchpad pointing device with multi-touch control
  • One Touch Function Keys
  • Premium Raised Tile LED backlit Keyboard with 10-Keypad (black)
  • Lithium Ion (43Wh, 4-Cell)—*Not user replaceable
  • 1-USB (2.0) port
  • 1-USB (3.0) port
  • 1-USB (3.0) port with USB Sleep and Charge
  • Accessories Added: