Toshiba Satellite S55t-A5237 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»


POSTED BY: mitchbob , temperance mi
Overall rating: 5 out of 5 5 out of 5

great laptop, great specs for the price! the speakers sound amazing, very fast computer with and intuitive touch screen. for the price you cannot beat it. the only thing I dislike about the computer is the black around the computer gets scratched if your not careful. other than that great buy.

I Love this laptop!

POSTED BY: Brian Lozar , Springfield, OR
Overall rating: 5 out of 5 5 out of 5

My granny bought me this exact one for my going in to college present and I love it. it is super fast and super easy to use I would DEFINITELY recommend this one!!


POSTED BY: Francesca , Philippines
Overall rating: 5 out of 5 5 out of 5

It has a sleek style. The wide screen is perfect for watching movies online not to mention it comes with Harman/kardon stereo speakers. It's 16 GB is good for photo and video editing. The only problem I got was Windows 8 keeps on dropping the Wi-FI connection. I made a little research and found out that all PC brands that run an OS Windows 8 has this problem. Thanks to those comp geeks, they have solved this problem. Just google it. When it comes to battery life, it drains a little bit fast so you just need to adjust the brightness setting to save power. Other than that, this laptop is superb! Would definitely recommend to anyone!

Pretty Good but...

Overall rating: 4 out of 5 4 out of 5

The laptop is great but only big disappointment is it does not have bluetooth. I would have thought that by now, bluetooth would have been on all the latest laptops. If you get this laptop, just remember do not buy a bluetooth mouse for it like I did...

A fine machine :-)

POSTED BY: Ichibon Brosan , Santa Maria, CA US
Overall rating: 4 out of 5 4 out of 5

I bought this machine to do software development using language tools that only run on Windows. It sits side by side with my Apple MacBook Pro 15". I find it interesting that the screen intensity function keys and the spearer volume function keys are in almost the identical position as on the MacBook Pro. It is a difficult comparison setting the two side by side. The 15" Retina screen on the MacBook blows away the Toshiba. The Toshiba screen is washed out in comparison, where the MacBook is brighter and clearer. I did notice that the Toshiba screen has a narrower viewing angle than I would have expected, again compared to the Apple. Lots of cores, plenty of memory, great processor, good speakers... My only regret is that the machine runs Windows 8. I have been through this before on countless machines... When you run an OS other than the bundled one, you have driver problems and unsupported hardware. I seriously dislike Windows 8, but I have to live with it. I am sure this hardware runs it as well as any other. So aside from the screen issues, and the Windows 8, this machine is a dream. I could have returned it, but I don't know of a better machine for running what I have to run. (IAR Embedded Workstation). The backlit keyboard is very nice. The keypad is responsive. It's nice to have the internal optical drive. Overall I would recommend it for a Windows user. The lack of internal bluetooth can be easily fixed with a BT USB dongle.

very gool laptop :)

POSTED BY: SamZezo , Abu Dhabi - U.A.E
Overall rating: 4 out of 5 4 out of 5

actually i love this product, very good performance for my work , i really recommended it for any on e ask, except the one ask for full hd screen..

MSRP: $1049.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 16GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S50 shop for accessories