Toshiba Satellite S55T-A5334 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Grate performance and stability

POSTED BY: SONTECH , Carlsbad, CA
Overall rating: 5 out of 5 5 out of 5

I'm an Information Technology Support Solutions Specialist. Its very important that I'm able to offer field support in a timely manner, so it necessary for me to have fast, and stable laptop for supporting my clients. The Toshiba S55T-A5334 Intel i7 processor and 16Gigs of RAM gives me the power to run multiple high resource applications with out slowing down I am able to load several Virtual Machines so I can have a copy of Windows 95, ME, XP, 7 all open at the same time so I'm able to walk my clients through what ever functions they are in need of support from me. Also the chip-set offering me 3.0 usb is a huge help when transferring large amounts of data between external drives and my laptop it saves me hours of time every week versus my old laptop with 2.0 usb and the CD/DVD burner comes in handy when i'm unable to use a bootable USB drive on a clients workstation and a bootable CD is required. The only down side i find with this unit is it does not come with Bluetooth witch is not a big deal for most people because the average user never end up using their laptops Bluetooth capability.

Quality Laptop

POSTED BY: dj , Minnesota
Overall rating: 5 out of 5 5 out of 5

I am very satisfied with the Toshiba. I have had no problems or issues.

Sweet Laptop!

POSTED BY: Arrow
Overall rating: 5 out of 5 5 out of 5

This is our 3rd Toshiba in 13 years, The other 2 are still working. I tried a Dell right before I bought this one. It lasted 9 days!!! Everything went wrong with it... I knew I should have stuck with Toshiba, they have not let me down yet! I love Windows 8, thought I would have a big learning curve, but I have I have crused right through it! I get on one of my older Toshiba's and find myself trying to tap the screen. I just love this computer with the back lite keys and the 10 key!!!

A Laptop that feels like a Computer

POSTED BY: zHawk , West Caldwell, NJ
Overall rating: 5 out of 5 5 out of 5

Finally a laptop that has a solid feel, and good looking fit and finish, looks like world class value is back !!

Nice machine for the money!

POSTED BY: olimpo de bahia blanca , gypsum, colorado
Overall rating: 3 out of 5 3 out of 5

i like the fact this unit still has the "old" school dvd player, it is quick, has tons of memory. battery life appears average for a unit this size around two-three hours internet and computing. one downside is the crazy swipe and touchpad combo that constantly swaps u off the screen you are looking at, its kinda of a pain. too many features on the home page as well, its just confusing to see that many tabs and apps at once?

MSRP: $1049.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 16GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S50 shop for accessories