Toshiba Satellite S55T-A5337 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop for use as only computer

POSTED BY: Catlover , Tucson, AZ
Overall rating: 5 out of 5 5 out of 5

This laptop is well designed, especially the keyboard which has larger keys and types like a regular keyboard, light weight so is easy to carry around, and the screen has wonderful color.

Good Value but can be improved.

POSTED BY: TheBad0 , Miami, FL
Overall rating: 5 out of 5 5 out of 5

Generally it is a good laptop at a reasonable price. Powerful and with lot a features. The 2 main disadvantages I found are: 1. Don't like the fixed battery, it doesn't allow me to have a spare if needed and force to send back to Toshiba for replacement. 2. There is a small vibration on the pad near the hard drive when it is operating, needs to be fixed. Additionally I HATE the preinstalled software that force to buy after a trial period. If you want to include (for your profits) just include but don't install to force me to uninstall.

Great Laptop!

POSTED BY: Joe , Norco, CA
Overall rating: 5 out of 5 5 out of 5

From the moment you take this laptop out of the box, you can tell that it was built with quality. The brushed aluminum case, the raised and lit keyboard, and the high quality touch screen are only some of the immediately apparent items you like to see on a higher-end laptop. In the month I've owned mine, I'm impressed with it's quick start-up time, as well as the overall look and feel of the unit.

Good for price/value

POSTED BY: Kevin , Fremont,CA
Overall rating: 3 out of 5 3 out of 5

Nice design laptop and performance but the Bluray dic player software is not working to play a movie. So sad.

Good intentions on design but.......

POSTED BY: Tl1 jaime , Temecula
Overall rating: 3 out of 5 3 out of 5

Tohiba quality is good but for this system was short in not including Bluetooth. And also tech supp... Needs to improve

MSRP: $1137.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 16GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • Blu-ray Disc™ ROM (BD-ROM) and DVD SuperMulti drive (+/-R double layer)

build your own S50 shop for accessories