Toshiba Satellite S70-ABT3N22 Laptop

This product will be custom-built for you.

Average Customer Rating:
Free ground shipping on laptops $499+
FREE 12GB MEMORYup to $50 OFF Microsoft Office

Limit 5 per household
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

BUILT WITH WRONG KEYBOARD

POSTED BY: N/A , TN & MA
Overall rating: 4 out of 5 4 out of 5

Like most Toshiba notebook computers the quality was excellent. Only problem was that the LIGHTED KEYBOARD I paid for was not installed as I received a regular keyboard. Only other thing, unlike other Toshiba notebooks I have had the motherboard must be mounted upside down as the CD/DVD and other plugs and jacks were on other side of notebook right to left side reversed/. [DVD opens at front left side instead of expected back, right side. Was told that this was standard for this particular model. Otherwise, a really excellent notebook

ok but not the greatest

POSTED BY: no one
Overall rating: 3 out of 5 3 out of 5

Overall the computer seems to be ok. Upgrade screen is really clear and looks great. features are ok so far but the keyboard is sad and the trackpad is the worst I've ever seen. It jumps all over despite sensitivity being turned down and the buttons are part of a tipping pad so its impossible to get the buttons to work consistently. I'll be deactivating it and using a mouse. So much for compact. Despite the factory Win 7 install all documentation (when you can find it) is for the win 8 version so not much help there. I'm replacing an earlier satellite version that has a broken screen. I really miss it....I think this one will be ok in the long run with some work. If I had a choice to put win 7 on any computer I wouldn't have chosen this one. It was one of 2 choices and probably the best of the two but that isn't saying much. win 8 is a user interface disaster..... I don't know how the battery life, features and performance look yet. I just got the computer but the site requires you to give a rating. It may be better than 3 stars on all of them but only the overall and price-value ratings are real.

be careful

POSTED BY: momo2788 , atlanta, ga
Overall rating: 1 out of 5 1 out of 5

Just received it, they forgot to install the nvidia card, keyboard and mouse does not work properly, and the best part is that they actually put the nvidia sticker on the laptop.

Select Processor What's This?

  • add $100.00
  • add $200.00

Select Microsoft® Operating System What's This?

  • add $99.99
  • add $99.99
  • add $199.99

Select Memory What's This?

  • FREE
  • add $50.00
  • add $100.00
  • add $100.00

Select Hard Disk Drive What's This?

  • add $30.00
  • add $60.00

Select Graphics Controller What's This?

  • add $75.00

Select Display What's This?

  • add $100.00

Select Touchscreen Options What's This?

  • add $200.00

Select Optical Drive What's This?

  • add $50.00
  • add $75.00

Select KeyBoard Options What's This?

  • add $20.00

Select Wireless LAN & Bluetooth® What's This?

  • add $15.00
  • add $25.00

Select Microsoft® Office Software What's This?


Select Anti-Virus Software What's This?

  • add $49.99

Warranty Upgrades and Extended Service Plans 


Select Toshiba recommended accessories 


  • $949.99
  • 629.99
  • -$200.00
  • -$749.99
  • -$120.00
  • -$829.99
  • $0.00
  • $0.00
  • $629.99
  • $629.99
  • »
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • Free Ground Shipping

add to cart

This product will be custom-built for you.

Estimated Ship Date from Toshiba is 04/25/2014.

  • laptop summary
    • Customized

  • Intel® Core™ i3-4000M Processor, (3M Cache, 2.40GHz)
  • Windows 8.1
  • 12GB DDR3L 1600MHz SDRAM (8GB + 4GB)
  • 500GB HDD (5400rpm, Serial ATA)
  • Integrated Graphics
  • 17.3" diagonal widescreen HD+ (1600x900) TruBrite® LED Backlit display
  • No Touchscreen
  • DVD SuperMulti (+/-R double layer) drive
  • Premium Raised Tile Keyboard (black)
  • Wi-Fi® Wireless networking (802.11b/g/n) (150Mbps)
  • 1 month trial for new Office 365 customers
  • Norton™ Internet Security 2013 (30-day trial subscription)
  • 1 Year Standard Limited Warranty (1 Year on Battery)
  • Accessories Added: