Toshiba Satellite S75-A7111 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Laptop I Ever Had!

POSTED BY: oldiebutgoodie , Bridgewater, NJ
Overall rating: 5 out of 5 5 out of 5

Love my new Toshiba Laptop! It is speedy and easy to get use to!

My Second Toshiba

POSTED BY: Saus , Kirkland, WA
Overall rating: 5 out of 5 5 out of 5

Ease of use, never have had any problems.

Excellent Laptop

POSTED BY: Retired Guy , Greensboro, NC
Overall rating: 5 out of 5 5 out of 5

This is the third consecutive Toshiba laptop I have owned (over a 18 year period), and recommended to others the purchase of Toshiba. The workmanship and quality is second to none, though a few manufacturers are closer than in the past.

Good Laptop but hard to use

POSTED BY: 1st time laptop , Alabaster, AL
Overall rating: 4 out of 5 4 out of 5

I am a little disappointed with the Toshiba S75. I read an earlier review of another Toshiba laptop where the poor performance of the mouse pad was noted and hoped the S75 would perform better. However, the operation of the pad at times is very frustrating and requires at times up to 5-8 taps to operate. The battery life is also not what I was expecting. Everything else seems to work well. The Windows 7 Professional seems to operate without any problems.

Disappointed

POSTED BY: nick , South Carolina
Overall rating: 3 out of 5 3 out of 5

Am disappointed in touch pad most of all. It does not always pick up your touch and when you tap the pad, sometimes it reacts and some time it does not.The buttons on the pad does not help a lot because the curser moves with the slight movement of your finger. I put a wireless mouse on and it is a lot better. Lid does not close easy. You almost have to use two hands. Overall not impressed with quality.

MSRP: $868.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 7 Professional
  • 16GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S70 shop for accessories