Toshiba Satellite S75-A7140 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop

POSTED BY: student
Overall rating: 5 out of 5 5 out of 5

Works great. I play games, use microsoft office and it has the latest version of windows 8. i use this mostly to stream movies and music, play games like halo and gta and do homework for school.

Beautiful Laptop

POSTED BY: Menu , Omaha, Ne
Overall rating: 5 out of 5 5 out of 5

I really love my new laptop. Its sharp in design. I'm not wild about Windows 8.1 but I found a work around that. I've got everything loaded on it now just haven't had a lot of time to work on it. It was very quick and easy to set up out of the box.

POSTED BY: straykitty , Casa Grande, AZ
Overall rating: 5 out of 5 5 out of 5

Good one for the money

Overall rating: 4 out of 5 4 out of 5

With the 8g ram it was fast when processing my Photomatix 5 program and sufficient power to use multiple programs at the same time. It opened faster than my old HP but downloading programs such as Norton it was very slow (12 hours). Keyboard feels good, lighter than my HP. It would have been nice if it had two more ram slots.

MSRP: $769.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-4200M Processor
  • Windows 8.1
  • 8GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories