Toshiba Satellite S75t-A7220 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

None Better out there

POSTED BY: Aint
Overall rating: 5 out of 5 5 out of 5

I have been a Toshiba User for about 15 years and can honestly say, dollar for dollar, I haven't see a better product on the market. As a technician dabbling in Computer repairs and servicing I've seen two Toshiba machines with issues over these years. The one shortcoming of my present purchase is the absence of Bluetooth connectivity. One was destroyed when the owner spilled coffee in it. The other though still working, simply could not support the Windows 7 basic requirements. I unhesitatingly recommend Toshiba to all my friends and clients.

POSTED BY: Angelofheart , bakersfield.Ca
Overall rating: 5 out of 5 5 out of 5

I really like feature, but confusing on all the windows. how to get in and out of things and updating.

Nice PC But...

POSTED BY: Mike , Boulder CO
Overall rating: 1 out of 5 1 out of 5

While the laptop performance and features are very good, reliability is very poor. This is the third S75-A4220 Toshiba laptop I have bought. On the first laptop the keyboard shift keys stopped working within the first week. I returned it and got a new one. The display on that one went dark in the first week. So back to the store one more time. Now the third laptop has passed the one week mark without complaint. I'm holding my breath.

MSRP: $1149.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 12GB DDR3L 1600MHz memory (max 16GB)
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD SuperMulti (+/-R single layer) drive

build your own S70 shop for accessories