Toshiba Satellite S855-S5164 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Laptop...

POSTED BY: Mzymac , Cleveland,Ohi
Overall rating: 5 out of 5 5 out of 5

I love my Toshiba Laptop, easier for me to handle. I am a Toshiba "fanatic"..I also purchased a tablet and I have my old stand-by Toshiba P205.

My 3rd Toshiba Laptop

POSTED BY: Layton , North Carolina
Overall rating: 5 out of 5 5 out of 5

Each of my previous Toshiba laptops have been excellent products and very reliable. Thus far the same is the case with this one. Although I detest Windows 8 it isn't a Toshiba driven issue. The keyboard on this model isn't as nimble as previous models but I am adjusting.

S855 Satellite great value

POSTED BY: inthechateau , Kosovo
Overall rating: 5 out of 5 5 out of 5

All the features i needed and performance with gusto in this 855. I find as usual offered software is lacking, but after getting a few of my old programs working(installed with ease) this Satellite is performing with satisfaction for both web, and software based ussage. Camera pixilates on the web once in a while but satisfactory. Thanks for another fine product Toshiba.

Toshiba Satellite S855-S5164 Laptop

Overall rating: 4 out of 5 4 out of 5

In my opinion it is better than I expected by design, with low weight and very comfort, in hand design looks more attractive than in the pictures. For me and my work as programmer is quite enough, The processor and the main memory is very good and enough, and the video card which is ideal for price comparison. One of the things I wouldn't have liked is a screen, for some reason it is not such a clear image as I expected, it will be good in the future to be able to increase the screen Hertz. For the games not tested yet :)

MSRP: $749.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3230M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • 2GB DDR3 AMD Radeon™ HD 7670M Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories