Toshiba Satellite S855-S5380 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Value

POSTED BY: Oden69 , Tucson, AZ
Overall rating: 4 out of 5 4 out of 5

This is a great laptop for gaming. I play Battlefield 3, Star Wars: The Old Republic, Guild Wars 2, and just about any game I want on it the AMD/ATI Radeon 7670 is awesome with 2GB dedicated graphics memory. Love that it has a full keyboard with number pad. Battery is ok wish it would last a couple more hours then it does.

Electrostatic problem on the casing

POSTED BY: kev , Lima, PE
Overall rating: 4 out of 5 4 out of 5

Hi, the laptop is very cool really but I have a problem when I connect the battery charger, the electrostatic appears on the aluminium surface, so is very uncomfortable because I feel the current on my hands every time I using it when its connected. Can sombody help me with this?

Good Value

POSTED BY: billybob , Butte montana
Overall rating: 3 out of 5 3 out of 5

My previous laptop was a satellite A665-s5199x but it didnt have enough video ram for AutoCad. The S855 came with 2 megs video ram which made all the difference in the world. In comparison the older laptop was build tougher and had a better keyboard and speakers, one more USB drive and a quad core I5. The new one isn't a quad core and had one USB drive broken out of the box. I really like the features but hope Toshiba will keep quality standards higher.

MSRP: $799.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3210M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • 2GB DDR3 AMD Radeon™ HD 7670M Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories