Satellite T135-S1309

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»


POSTED BY: UMAR , Pakistan
Overall rating: 5 out of 5 5 out of 5

Its amazing and charming........ I like it very much....


POSTED BY: Gustrago , San Clemente, CA
Overall rating: 5 out of 5 5 out of 5

I love this laptop... I"ve been using this laptop for school the past weeks and I just love this computer. It is lightweight, small, and kind of fast. I was thinking of getting a netbook and a few months ago i heard that this computer was coming out and I waited. I'm glad i waited. The computer runs AutoCAD, SAP and other programs wihtout a problem. Thank you Toshiba for not disapointing me yet.

Great Laptop

POSTED BY: tech , Las Cruces, NM
Overall rating: 5 out of 5 5 out of 5

Very nice laptop. Windows 7 is fast and easy to adapt to for Windows XP users. The screen is bright and easy to read and the full-size keyboard makes typing smooth and effortless. I really like this laptap and I strongly recommend it to all of my colleagues. The performance of the built-in speakers is nothing like you would get from external speakers but I suppose that is true for all laptops. In general, this is a great product that I am very satisfied with.

Peak point

POSTED BY: berkayv
Overall rating: 5 out of 5 5 out of 5

I think I deserved to have such a sophisticated laptop to be my first laptop although I am near to 40.

The best laptop I've ever owned!

POSTED BY: hdbdude , Austin, TX
Overall rating: 5 out of 5 5 out of 5

I love it! Great quality, light, neat trackpad, ultra-slim, and great performance. Its dual-core processor is fast, windows 7 runs nicely, tons of ram, huge hard drive. I would absolutely recommend this laptop to anyone who wants great machnery!

great laptop but touchpad needs improvement

POSTED BY: jpab , Rome, Italy
Overall rating: 5 out of 5 5 out of 5

I've owned this since Oct 2009. PROS: great laptop all around- light, powerful, fast. CONS: have to agree with previous comments. .. the touchpad is TOUCHY. When it works its seamless, then out of the blue it will not respond. The speakers aren't as good as previous Satellites I've owned and one of my usb ports is already getting loose.

Excellent Value

POSTED BY: Norrellek , Tampa, FL
Overall rating: 5 out of 5 5 out of 5

I needed an ultra light laptop that was small and portable, but had excellent battery life and solid performance. I tried a netbook first, and loved the battery life, but hated the performance and the trade offs (10" screen for one). This is the perfect compromise, imho. BAttery life is solid, the performance is very usable and the screen size is likewise usable. Best part is that I can keep it in my briefcase and forget it's there. Terrific value.

First Laptop

POSTED BY: sueser , Chapel Hill, NC
Overall rating: 5 out of 5 5 out of 5

Had a little difficulty but disabled the touch pad to keep the curser from going wild - love the quietness of operation, brightness of the screen, light to carry - overall very happy.


POSTED BY: Little One , Laguna Woods, CA
Overall rating: 5 out of 5 5 out of 5

This is a great little laptop, small enough to stick in your bag or briefcase but with enough memory and speed to surf the net or keep up with friends with ease. You get a lot of bang for your buck with this laptop.

I Love Everything About It

POSTED BY: onpoint , the state of Washington
Overall rating: 4 out of 5 4 out of 5

I've been using this laptop for about a week now, and I am quite pleased with it. This is my second Toshiba, and I was pleased with my first one as well. I really like how thin and light it is due to not having an internal cdrom drive. This is the lightest laptop I've ever owned. It also feels quite sturdy when I'm carrying it around. It doesn't creak and flex like some of my past laptops. The screen is bright with no dead pixels, it's runs cool and quietly, and the battery life is fantastic. Although I hate fingerprints, I love the glossy exterior. It looks very sleek. At first, the only “con” was the lack of internal cdrom drive because most of my applications are still on cd/dvd media. Without purchasing an external cd/dvd rom drive, you'll have to get a little creative (i.e. network install, thumb drive, etc.) when installing your applications. Once you get past that, it's not really a con since I prefer it without the drive and extra weight anyway. My only other “gripes” are the keys – I wish they weren't so slick, and the audio isn't as loud as I prefer. Nonetheless, my conclusion is it's a great laptop for what it offers and it meets all of my needs.


POSTED BY: Vagus , Bethesda, MD
Overall rating: 4 out of 5 4 out of 5

One problem I can think of is that the touch pad doesn't always move mouse smoothly. Great overall though.

good deal

POSTED BY: chuck , prairieville, la
Overall rating: 4 out of 5 4 out of 5

i bought it to use while watchin tv @ nght fits on my lap and easy to manage.


POSTED BY: Rick , Brownsville,Texas
Overall rating: 4 out of 5 4 out of 5

This is a great laptop,The battery life is one of the main items I was looking for in a Laptop.Windows & is good.

POSTED BY: Honey , McMinnville, Tn.
Overall rating: 4 out of 5 4 out of 5

I really like the compact size and light weight of this laptop. I like the built in wireless feature. The only thing I wish was better was the volume. In some instances, I can barely hear the sound.

basic deficiencies great battery

POSTED BY: Annnnnnnnnnna
Overall rating: 3 out of 5 3 out of 5

After lengthy research and shopping around I decided to buy this model as I was looking for light, small laptop, with lng battery and possibly optical drive.. to put it in a nutshell everything you need to work/surf in internet/watch movies/talk to friends wherever you are (I travel a lot). The laptop is really light, but the nova black leaves a lot of fingerprints on the lid and elsewhere. The major deficiency for me is: webcam is REALLY low quality, so are the speakers.. you can hardly hear the skype calling with 100% of the volume (!). Also, the battey is a bit loose on my unit (but think I can exchange it so it shouldn't be a big deal). The computer doesn't run as smoothly as I would expect... For sure - battery life and its weight make it competitie among other 13.3 models, but I am still waiting for my perfect laptop to be constructed.. MANUFACTURERS - contact me if you want a mobile laptop bestseller.. it seems like you do find out what your customer needs are!

Great Lap aside from the mouse pad

POSTED BY: Scott , Chicago, IL
Overall rating: 3 out of 5 3 out of 5

The laptop is great, this is actually my second Toshiba Satelite. My last Toshiba still works, but my kids use it. Although, this is my second laptop BEWARE THE MOUSE PAD OCCASIONALLY STARTS MALFUNCTIONING AFTER A FEW HOURS OF USE.

HUGE dissapointment

POSTED BY: ashley , manhattan, nyc
Overall rating: 2 out of 5 2 out of 5

I got this laptop about 3 months ago. I hate the speakers, its very difficult to hear (youtube, or webcam convos etc.) lastly the keypad is just as bad, it will literally take me 10 mintues to move the mouse pointer to the start button. I wish I couldve found something better. too bad my return day is up. i hate this laptop. only cute thing is its small, light weight. other then that its trash.

terrible touchpad

POSTED BY: laptop guru , Atlanta, GA
Overall rating: 1 out of 5 1 out of 5

The pros: It's light weight and sleek. The cons: The touchpad on this unit is terrible. The cursor does not respond and unless you are prepared to use an external mouse, don't buy this unit. It's functionally unworkable.

MSRP: $649.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor SU4100
  • Windows 7 Home Premium (32-bit)
  • 3GB DDR3 1066MHz memory
  • 320GB HDD (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories