Toshiba Satellite U945-S4110 Ultrabook

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great laptop!

POSTED BY: usavol
Overall rating: 5 out of 5 5 out of 5

It's very light, easy to manage, fast to boot, and simple to use and navigate.

Not Liking Very Much

POSTED BY: awesme622 , Central FL
Overall rating: 5 out of 5 5 out of 5

I did not know when I bought this ultrabook there was no CD Rom drive. The keyboard keys are hard to push down and spaced too far apart. It is fast though and I need that. But overall, I am not thrilled with this laptop. I am getting used to Windows 8 and cannot wait for the upgrade in October...hopefully it will fix all the issues people are having with it.

Average Laptop

POSTED BY: Luv4lyfe
Overall rating: 4 out of 5 4 out of 5

touchpad continuously freezes even after updating the Synaptics Touchpad driver - touchpad will automatically disable itself when external mouse is in use - battery life is about average - would love to upgrade to 6 cell battery - Win 8 OS will take some getting use to; everything is hidden - overall the laptop is good for the price and the basic user

Great laptop

POSTED BY: Cat , Warwick, RI
Overall rating: 4 out of 5 4 out of 5

This laptop is reliable and can handle most jobs. It can't really handle multitasking and playing games like minecraft here is so-so. Just upgrade the ram and this baby will handle a game like a pro.

POSTED BY: Lizardo , North Dakota
Overall rating: 4 out of 5 4 out of 5

bright crisp graphics, good processor speed. Very light and easy to cary. Lose 1 star as no NOTICE no CD!!. with CD drives industry standard for years, should have had specific mention. Difficulty starting Windows 8 as is different from prior versions. Still getting used to it. Should have some minimal instructions based on in8

Really Good Laptop

POSTED BY: Liz , Louisville,KY
Overall rating: 4 out of 5 4 out of 5

I think so far my Toshiba Laptop has been a really good Laptop. It's normally really fast, It has a lot of memory and it came in the perfect size for me.

POSTED BY: Bunny
Overall rating: 1 out of 5 1 out of 5

Returned this laptop because of Windows 8. Started to set up email, and the response went to my old computer. I tried everything but couldn't get it to the new computer, so I returned it. There were lines of people returning because of Windows 8.

Windows 8

POSTED BY: K , Lake City, FL
Overall rating: 1 out of 5 1 out of 5

I returned this laptop several days after purchasing it. I already owned a Toshiba with Windows 7. That one I liked very much. This Toshiba I returned, not because of Toshiba, but because I can't stand Windows new OS. I will wait until a new system comes out or buy a computer with another OS.
recommended accessories

Toshiba USB 2.0 Portable DVD Super Multi Drive (Tray Load) ($99.99 value)

Installation, file sharing and backup make easy!
Save 40% for a limited time

$59.99

learn more

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3227U Processor
  • Windows 8
  • Intel® Integrated Graphics
  • 500GB HDD (5400 RPM, Serial ATA) with 32GB (system use only) mSATA solid state disk cache
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Intel® Centrino® Wireless-N 2200, 2x2 BGN + Wi-Di Capable