Toshiba Satellite U945-S4140 Ultrabook

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: Eddie , Buenos Aires
Overall rating: 5 out of 5 5 out of 5

It is too heavy!

Enjoying my new Laptop

POSTED BY: Pat , Ft Worth, TX
Overall rating: 5 out of 5 5 out of 5

I am loving my new Toshiba. This is the third one I have owned over the years and all have performed like champs. It doesn't have a combo drive but adding one over the USB 3.0 is more than quick enough to watch a movie or install software.

A cool notebook

POSTED BY: turboczi , Budapest, Hungary
Overall rating: 4 out of 5 4 out of 5

I like this notebook. I wouldn't call it an ultrabook because of the battery life, which is about 4 hrs in my case, but apart from that, it is a great plus! It boots quicker than my phone (Nokia E52), which is about 20 seconds. Amazing. Any program I click on starts within 2 seconds. I am absolutely satisfied (apart from battery life).

So far . . . So good

POSTED BY: Sammy , Montebello, Ca
Overall rating: 4 out of 5 4 out of 5

The performance is good. Just hit a learning curve with Windows 8 which I really haven't used very much in the past. But thus far . . . So far/so good!

A great little laptop with great features!

POSTED BY: Commander , New York City
Overall rating: 4 out of 5 4 out of 5

A great little laptop with great features but wish I could disable the lighted keyboard when not needed so as to extend battery life. Otherwise a very nice laptop for the price. Sound quality is not all that but it make up fo that in other features.


POSTED BY: ps, marietta, ga , gau
Overall rating: 4 out of 5 4 out of 5

The rating may be a bit unfair but the heart of a computer isthe operating system and Windows 8 is truly the worst I have ever used. Microsoft reall laid an egg with this OS. My other laptop is also a Toshiba(Vista OS) which is why I bought this one. I guess it is not Toshiba's fault that you are trapped into offering Windows 8 but as a computer manufacturer, you should be all over Microsoft's case.

average laptop

Overall rating: 3 out of 5 3 out of 5

Windows 8 needs clock on the desk Windows 8 needs improvement in terms of opening two subscreens simultaneously The keyboard is not comfoortable to click the body looks very cheap

MSRP: $612.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400 RPM, Serial ATA) with 32GB (system use only) mSATA solid state disk cache
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive