Please wait...action in progress.

Toshiba Q-Series Pro Solid State Drives

Speed up
without
spinning up

Drive faster. Play harder.

If you simply can't work fast enough—or get enough full-throttle gaming—you need a Toshiba Q-Series Pro Solid State Drive in your Ultrabook system or laptop. It doesn't spin like traditional hard drives. But it does provide much faster and more reliable performance that will knock your socks off.


Bring Your Old PC Back to Life

Toshiba Q-Series Pro Solid State Drives can revive your sluggish PC that is running on a traditional hard drive by reducing your OS boot time and speeding up your PC data transfer rate by leaps and bounds. This means you can spend more time enjoying your applications, and less time staring at the hour glass icon on your computer screen.

1Measured by timing power on to Windows chime as of August 23, 2013.

2Per ATTO Disk Benchmark v2.47 (MB/s) as of August 23, 2013.


Made for Multitasking

If you could only do more, and do it quicker. Now you can—with a Toshiba Q-Series Pro Solid State Drive in your PC. You'll multitask like mad with significantly less lag than a traditional hard drive. You'll enjoy faster access to applications. And you'll also experience speedier Windows® startups, web browsing, emailing, antivirus scans and more. Toshiba Q-Series Pro Solid State Drives offer best-in-class performance in Everyday Applications3 on Windows 8 PCs.

3As measured by PriceG2.com on August 23, 2013 via PCMark 7 v1.2.0 Benchmark Test (MB/s).


Great for Gaming

Toshiba Q-Series Pro Solid State Drives offer best-in-class sequential speeds2 and achieve one of the highest Gaming scores.3 So you'll drool over faster frame rates and more responsive play—with no gaps in the action. Your games will load in a flash. Plus, you can load an entire title onto one of these drives, then just sit back and enjoy the fun.

2As measured by PriceG2.com on August 23, 2013 via AS SSD v1.7.4739.38088 Benchmark Test (MB/s).

3As measured by PriceG2.com on August 23, 2013 via PCMark 7 v1.2.0 Benchmark Test (MB/s).


Lower Power Consumption

Since they don't spin up, Toshiba Q-Series Pro Solid State Drives use a lot less power. The result? More time to work and play on your laptop. You may also experience less downtime by going longer between battery charges. Toshiba Q-Series Pro Solid State Drives are so efficient, they consume up to 50% less power than competing models.4

4Measured by PriceG2.com using ATTO Disk Benchmark Test v2.47 (Watts) based on sequential write activities as of August 23, 2013


Better Durability

With no moving parts, Toshiba Q-Series Pro Solid State Drives are more resistant to shocks and vibrations. That's important when you're pushing to send that email and answer IMs—at the same time, of course. They also help ensure that your documents, games, pictures and videos will be there when you want them. Toshiba Q-Series Pro Solid State Drives offer excellent long-term performance for extended or heavy workloads.5

5As measured by PriceG2.com on August 23, 2013 via Iometer 2010 Test results (IOPS, Queue Depth 1-10).


Lots of Sizes

Got tons of pictures, videos and games? Or maybe not so much. Either way, you'll find a Toshiba Q-Series Pro Solid State Drive to suit your needs, and give you room to grow. They come in 128GB, 256GB and 512GB sizes.


Thin and Light

With the new 7mm slim and lightweight (just under 2 oz) design, the Toshiba Q-Series Pro Solid State Drive is ideal for your Ultrabook systems. A mounting spacer is included to work in both slim Ultrabook system designs and laptops with traditional full-height 9.5mm drive bays. Lose the bulky hard drive weight and make your laptop and Ultrabook system lighter to carry and travel-friendly.


Upgrades and Data
Transfers Made Easy

Toshiba Q-Series Pro Solid State Drives make it easy for you to upgrade your PC. It comes with an easy-to-use migration software to help you transfer your data from your existing drive to the Toshiba Q-Series Pro Solid State Drive. Just download the free software6, run the program and complete the migration process in a few simple steps.

6Use of NTI Echo software in a Notebook or Ultrabook™ will require the use of a SATA to USB bridge cable (not included.)


Supreme Reliability

For the last 25 years, Toshiba has been one of the world's leading flash memory manufacturers, so you can count on our solid state drives to work wherever and whenever. It's no wonder why they're used in so many major PC brands, or why we back them with a solid three-year limited warranty.


shop all solid state drives

Ultrabook, Celeron, Celeron Inside, Core Inside, Intel, Intel Logo, Intel Atom, Intel Atom Inside, Intel Core, Intel Inside,
Intel Inside Logo, Intel vPro, Pentium, Pentium Inside, vPro Inside, are trademarks of Intel Corporation in the U.S. and/or other countries.