Please wait...action in progress.
Sorry, Toshiba 55G300U 55" Class 1080P LCD HD TV is not available for sale through Toshibadirect.com. But...
We can give you details about the Toshiba 55G300U 55" Class 1080P LCD HD TV:
Toshiba 55G300U 55
Images
IMAGES
 »

Toshiba 55G300U 55" Class 1080P LCD HD TV

  • Screen Size: 54.6" diagonal widescreen
  • Display Type: LCD
  • Native Display Resolution: 1920x1080
  • Refresh Rate: ClearFrame™ 120Hz
Part Number: 55G300U
Average Customer Rating: 
Read 3 reviews

Questions? Call us at 800-316-0920
Toshiba 55G300U 55" Class 1080P LCD HD TV Toshiba 55G300U 55" Class 1080P LCD HD TV
Rated 4.0/5 based on 3 customer reviews
Product description: Explore Toshiba's innovative laptops, accessories, projectors and electronics. Find the best fit for your home or business.
 

Sorted by:  Rating (high to low) »  Rating (low to high) »  Most Recent »  Most Helpful » 

Overall Rating: 5 out of 5 5 out of 5
Outstanding valueDecember 16, 2010
by Iva from Boise, ID
Features: 5  out of 5 5 out of 5
Performance: 5 out of 5
Battery Life: 0 out of 5
Price–Value: 5 out of 5
Lots of great connections that handle all my consoles, media PC, regular PC, blu ray player, sat tv, etc. Has a great menu to do everything that is needed, and is logical. Really a great picture - crisp, clear, good colors and blacks, no ghosting, and a fast refresh. Perfect for gaming as well as any show you watch. This is easily equal the tv that you might spend 500 hundred more dollars on another brand - just for the brand sticker. Get this one and spend your other money on a blue ray and a media PC instead...
What is your level of technical expertise?   TechSavvy
How long have you been using this product?   One month to a year

Overall Rating: 4 out of 5 4 out of 5
Toshiba 55G300U - 55" class 1080p 120Hz LCD TVSeptember 6, 2011
by rmac442 from El Paso, TX
Features: 5  out of 5 5 out of 5
Performance: 4 out of 5
Battery Life: 0 out of 5
Price–Value: 5 out of 5
I really like the tv. It has great features, seemly easy to use and set-up. The picture is fantastic. That said, I find that the sound is VERY LOW. It has 60 levels and it has to be set on 60 to barely hear it. Either I don't have the sound set correctly or the sound-level quality is really bad.
What is your level of technical expertise?   Newbie
How long have you been using this product?   One month to a year

Overall Rating: 3 out of 5 3 out of 5
Great for the moneyMarch 29, 2011
by chingaso from Arizona
Features: 4  out of 5 4 out of 5
Performance: 3 out of 5
Battery Life: 0 out of 5
Price–Value: 4 out of 5
This is a great deal for the money. The low cost has some glitches, though. There is the "turns itself on" issue (even with regza set to OFF), and there is a delay in the video due to the image processing. If you set it to "gaming" mode, this is much better, but still present. So if you send the audio to a surround sound system, it won't sync. If you use the optical pass through from the tv, it will be synced perfectly, problem is that it is only in stereo. So the only way to watch a show or movie in surround sound is out of sync or get a surround system that has an audio delay, then play with it till it syncs up. Also, if you put it in "gaming" mode, it will not keep this setting when you switch inputs or turn the tv off. You have to go back to the menu every time and turn it on. You won't forget to do this, though, as the audio will be way off if you don't.
What is your level of technical expertise?   ProficientUser
How long have you been using this product?   One month to a year
Customer Rating Summary
Toshiba 55G300U 55" Class 1080P LCD HD TV
Averages based on 3 customer reviews
Overall Rating: 4.0 out of 5
Features: 4.7 out of 5
Performance: 4.0 out of 5
Battery Life: 0.0 out of 5
Price–Value: 4.7 out of 5
3 of 3 (100%) customers would recommend this product to a friend.

Toshiba 55G300U 55" Class 1080P LCD HD TV - Write a Review Close  Close