Please wait...action in progress.

ClearFrame™ Anti-Blur Technology

If you love watching action-packed movies and fast-paced sports, blurring may be one of the things that bugs you the most. The good news is that Toshiba ClearFrame™ Anti-Blur Technology all but eliminates it. Found on our select HD TVs, it provides significantly clearer full-motion video compared to standard 60Hz TVs. Isn’t that what great HD TV is all about?

Faster Frame Rates Clarify the Action
Toshiba ClearFrame™ 120Hz doubles normal 60Hz performance to reduce blurring caused by fast-action video. And our ClearScan™ 240Hz goes a step beyond, quadrupling the 60Hz rate to create a 240Hz effect. They both improve picture clarity dramatically, without impacting brightness or adding flicker. And for those who prefer a more film-like picture, ClearScan™ 240Hz also offers a 5:5 Pull-Down option.
Which TVs have this great technology? Find them all using our TV Finder »

Ultrabook, Celeron, Celeron Inside, Core Inside, Intel, Intel Logo, Intel Atom, Intel Atom Inside, Intel Core, Intel Inside,
Intel Inside Logo, Intel vPro, Pentium, Pentium Inside, vPro Inside, are trademarks of Intel Corporation in the U.S. and/or other countries.