Toshiba All-in-One DX735-D3330 Desktop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Minor meltdown

POSTED BY: olecoach , Dallas, TX
Overall rating: 4 out of 5 4 out of 5

Really excited about the DX735. Was working extremely well for about 6 weeks. Then suddenly it would not power up. Is presently at a warranty provider for repair. If it comes back and continues to function as it did previously I'll be extremely happy, if not ...

Gaming

POSTED BY: iNeedIess , Candyland, CA
Overall rating: 4 out of 5 4 out of 5

I use this for gaming, it's works very well (Unless you're streaming.) So it should perform very well for just browsing the internet, etc. The only thing I disliked was what the keyboard and mouse was made out of. They got greasy very easily, and my fingerprints stick on it. One week into using it, my mouse acted up strange as well, and I had to change it to a wired mouse rather than wireless (Was not due to cursor speed or anything.)

MSRP: $999.99

not available for sale from
the toshiba online store

  • Desktop summary
  • Intel® Core™ i5-2450M processor
  • Windows 7 Home Premium (64-bit), SP1
  • 6GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 1.0TB HDD (7200rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)