Toshiba All-in-One DX735-D3360 Desktop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great All-in-One PC

POSTED BY: Chris , Naperville, IL
Overall rating: 5 out of 5 5 out of 5

This is my first All-in-One Desktop, and thus far I am very impressed. I would purchase this exact model for my work as well if I wasn't using three monitors to do my job. At home though, it's perfect. The size is great, and so are the hardware features. There is so much technology packed into something no larger than the average widescreen monitor. I do wish that Windows 7 Professional was an option. I had to pay more for an upgrade disc. Also, it doesn't seem to come with a backup CD. There is a recovery partition, but it won't do me much good in case of a hard-disk failure. Finally, I would ask that Toshiba take it easy with the pre-installed software packages. These are minor inconveniences though. Overall, I am extremely satisfied with this product, and would definitely recommend it to others!

THE BEST DESKTOP I HAVE EVER OWNED

POSTED BY: Denny , CT
Overall rating: 5 out of 5 5 out of 5

I HAVE ALWAYS OWNED TOSHIBA LAPTOPS AND ALWAYS RATED THEM TO BE THE BEST AND NOW THE ALL-IN-ONE DESKTOP IS BY FAR ONE OF IF NOT THE BEST DESKTOP I HAVE EVER OWNED. THE SPEED WITH THE INTEL I7 PROCESSOR WILL BLOW YOU AWAY. ALSO, MY WIFE IS SO HAPPY NOT TO HAVE THE BULKY PROCESSOR SITTING ON TOP OF OUR DESK ANYMORE. SHE LOVES THE COMPACTNESS OF THE ALL-IN-ONE AND THRILLED WITH THE 23" SCREEN AND BUILT IN SPEAKERS. TOSHIBA, YOU CERTAINLY HAVE OUTDONE YOURSELVES WITH DX735-D3360 All-in-One Desktop. WOULD I RECOMMEND THIS TO A FAMILY MEMBER OR FRIEND? HECK YES AND ALREADY HAVE.

All-in-one

POSTED BY: YiaYia , Huntington Beach, CA
Overall rating: 4 out of 5 4 out of 5

I bought this all-in-one to replace my laptop. I really appreciate the small footprint and 23-inch screen.

All in One

POSTED BY: Deeglo the Glo , Chicago, IL
Overall rating: 4 out of 5 4 out of 5

So, excited to get this all in one. The computer works fine the screen is great. It's a small thing like the mouse (mice) not work properly.

FAIR COULD HAVE BEEN BETTER

POSTED BY: JIM , FLORIDA
Overall rating: 4 out of 5 4 out of 5

FIST REALLY BIG PROBLEM IS - NO HDMI OUT TO SECOND SCREEN. EVEN CHEAP LAPTOPS HAVE THAT OPTION BUILT IN.

Nice, but.....

POSTED BY: captain , Philippines
Overall rating: 3 out of 5 3 out of 5

A nice responsive computer with a good value for money

somewhat ok

POSTED BY: Butch , Santa Ana
Overall rating: 3 out of 5 3 out of 5

I bought this computer without researching it and that was a big mistake on my part. I bought it thinking that it being a "Toshiba" computer it would be top notch, I was wrong. After setting up the thing I discovered that two of the reasons I bought it was missing. #1- NO VGA PORT, #2 NO WAY TO HOOK-UP A SURROUND SYSTEM. After looking at 2 different user manuels for this AIO one shows both in and out HDMI ports and the other shows only the in port, "What's up with that"? Now as far as the surround system, I currently am running Windows 7 Home and cannot get anything more than stereo out the the sound system. Is there a problem with Windows 7 Home? or is it a problem with Toshiba programing? The reason I ask this is because my brother has a Dell Desktop with Windows 7 "PRO" and he has Stereo, Quad, 5.1 and 7.1 . Any comments on this? One other "Bad" thing is Toshibas Wireless mouse, the darn thing jumps the cursor all over the screen. In short with all the laptops and T.V.s and AIO's I've bought from Toshiba Direct, I'm really sorry I bought this DX-730.

MSRP: $1199.99

not available for sale from
the toshiba online store

  • Desktop summary
  • Intel® Core™ i7-2670QM processor
  • Windows 7 Home Premium (64-bit), SP1
  • 6GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 1.0TB HDD (7200rpm, Serial ATA)
  • Blu-ray Disc™ ROM (BD-ROM) and DVD SuperMulti drive (+/-R double layer) with Labelflash®