Toshiba All-in-One LX815-D1310 Desktop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

best laptop ever

POSTED BY: deedee , binghamton,ny
Overall rating: 5 out of 5 5 out of 5

I like this Toshiba so much i think i'm going to keep using this product forever. Thank You

All-In-One Desktop

POSTED BY: MAD1048 , Bradenton FL
Overall rating: 5 out of 5 5 out of 5

At least, I think it's an All-in-One Desktop Computer. Toshiba keeps sending me information to buy this or try that for my new Laptop ( I thought they were called "Notebooks".) that would not work with my desktop. The computer itself is amazing and works beautifully. I love that I don't have to carry a Laptop anymore.

Very Good Computer

POSTED BY: Rick , Sheffield, AL
Overall rating: 5 out of 5 5 out of 5

This is the first computer of this type, I am very impressed with the entire system. I would highly recommend it to everyone.

Just plain satisfied

POSTED BY: Ezo107 , Clarksville, TN
Overall rating: 4 out of 5 4 out of 5

I love it, just plug in outlet and start becoming amazed of all the features this All in One computer has to offer!!! Thank you :)

works well

POSTED BY: winave , u.s.a
Overall rating: 4 out of 5 4 out of 5

This i purchased from HD online it was advertised as also being touch scene, however it is not, wished i had gotten what i purchased. However overall the unit works well, is a space saver and realitively quick. Overall i like it just would also like touch scene ability when doing some activities. wish Toshiba was offering a solution to make this also touch scene capable.

Great Laptop

POSTED BY: Buz , Kentucky
Overall rating: 4 out of 5 4 out of 5

Not sure about the name as it is on my desk a to big to put in my lap. The all in one is great. The only problem is the key board is to small for me. Well worth the price.

Great Laptop

POSTED BY: Kotton , Las Vegas, NV
Overall rating: 4 out of 5 4 out of 5

Performs well-has all the memory I need even after adding Adobe Photoshop Elements. Other than having a couple of tiles not working for some reason this laptop has exceeded my expectations.

MSRP: $699.99

not available for sale from
the toshiba online store

  • Desktop summary
  • Intel® Pentium® Processor B980
  • Windows 8
  • Intel® Integrated Graphics
  • 1.0TB HDD (7200rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)