Toshiba All-in-One LX835-D3250 Dekstop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

best desktop

POSTED BY: fcemyuksel , Nashville, TN
Overall rating: 5 out of 5 5 out of 5

I BOUGHT THIS DESKTOP AND I WORRIED ABOUT SPEED. BUT IT IS INCREDIBLE. FASTER THAN LAPTOP. AWESOME UTILITIES. I LOVE IT. I FORGET MY LAPTOP. THIS KIND OF DEKTOP THIS PRICE!!! I LOVE IT...!!!!

A Good Computer, But...

POSTED BY: Dicko , Pahrump, NV
Overall rating: 4 out of 5 4 out of 5

The computer is all that that is advertised and works just fine. However, I was extremely disappointed to discover that it has a single 2Tb HD rather than the dual 1Tb HDs that are advertised. I have always used a second HD to back up my primary but I cannot do it with this computer. Imagine my surprise today when I downloaded the Windows 8 Upgrade Manager and it told me that my touchscreen only includes Windows 7 capability and falls ahort on Windows 8. It also told me that there was no Windows 8 driver for the USB 3.0 hardware and that other components were not compatible. I bought this computer (and a second one) specifically to be ready for Windows 8. I guess that I'm not ready. Although it is a fine computer, I would not purchase it again for the reasons cited above.

MSRP: $1399.99

not available for sale from
the toshiba online store

  • Desktop summary
  • Intel® Core™ i7-3610QM Processor
  • Windows 7 Home Premium (64-bit), SP1
  • 16GB DDR3 1600MHz memory
  • 2GB DDR3 NVIDIA® GeForce® GT 630M
  • 2.0TB: 1.0TB (5900rpm, Serial ATA) + 1.0TB (5900rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)