Toshiba All-in-One LX835-D3300 Desktop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent Product!

POSTED BY: Rosie , San Diego, CA
Overall rating: 5 out of 5 5 out of 5

Beautiful screen, very responsive and quick to use. Love it!

Great product

POSTED BY: Dr. C , Los Angeles, CA
Overall rating: 5 out of 5 5 out of 5

I really like the features -- there are so many.

Excellent

POSTED BY: florida sunshine , florida
Overall rating: 5 out of 5 5 out of 5

This computer is amazing the features are slow for me because I am learning Win 8 and apps. I somehow "messed up" the computer's ability to run properly. Turned the system off and Toshiba corrected the errors automatically and I'm up and running again.

great all in one

POSTED BY: hoagie , louisville, ky
Overall rating: 5 out of 5 5 out of 5

all in one is great

POSTED BY: shirlita , albuquerque,nm
Overall rating: 5 out of 5 5 out of 5

Still in early stages of learning and experimenting but so far, just love it

LOVE MY NEW COMPUTER

POSTED BY: ANGEL , ALBUQUERQUE,NEW MEXICO
Overall rating: 5 out of 5 5 out of 5

IT'S SO FUN AND PRETTY EASY EVEN THOUGH I'M A NEWBIE WITH COMPUTERS. THE TOUCH SCREEN IS SO AMAZING. THE 360 PANORAMIC VIEW IS SO COOL . WOW !!!!

New Toshiba computer

POSTED BY: Marie , Venice, Fl
Overall rating: 4 out of 5 4 out of 5

Well, I think I love this computer, however, the keypad keys do seem to stick. But I simply hate the Windows 8. Rather than let me use the computer and programs that I want, it is so invasive and wants to control my use -- I bought this computer to use the way I want to -- not be always in conflict with the Windows 8 trying to manipulate me its way. I'm nearly ready to remove it and go back to Windows 7--though I only had XP and loved it. We'll see how it goes. My Emails are always being affected -- difficult to open, not able to delete or send, and I still need to have my Sony Laptop with Windows XP nearby so I can access and send Emails.

POSTED BY: Dave , Windham, ME
Overall rating: 4 out of 5 4 out of 5

I return 2 different computers because didn"t work as stated

Windows 8 confusion

POSTED BY: theblondielou , Bowie, MD
Overall rating: 4 out of 5 4 out of 5

This computer is too heavy....I am ill and need to be able to use it in bed and reclining chair and find It very cumbersome. Laptops don't work as the connection port keeps breaking. Windows 8; can't get Google Taskbar and Zoom to stay; reading Dummies/Senior books.

Excellent Desktop

POSTED BY: junebug , Orlando, Florida
Overall rating: 4 out of 5 4 out of 5

Very good desktop. It's fast and reliable so far. The only problem I have is ; when I shutdown It take too long to start and the key board has no indicator lights.

MSRP: $1088.99

not available for sale from
the toshiba online store

  • Desktop summary
  • Intel® Core™ i3-3110M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB HDD (7200rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)