Toshiba Qosmio X75-A7180 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Worth the upgrade!

POSTED BY: Nanner , Waco, TX
Overall rating: 5 out of 5 5 out of 5

Excellent laptop for high end computing and gaming. Super sonic FAST! My only complaint so far is the cord detaches too easily. Wish it had a better connection.

Happy customer

POSTED BY: JJ , Mel AU
Overall rating: 5 out of 5 5 out of 5

I am quite new to this machine however so far I'v found the X75 A7180 to be better than I expected, Very fast on boot up and fast performance. unlike many reviews I'v seen for this product, it does not overheat, my unit does not even get hot. Battery life is longer than I heard it to be I get around 3hrs out of a full charge. The only thing I feel Toshiba should address is the power cord which have a tendency to detach far too easy.

Very good gameing machine

POSTED BY: Old gamer , Bethany, OK
Overall rating: 5 out of 5 5 out of 5

Extremely fast boot up. Running the operating system from a Solid State Drive makes Qosmio X75_A7180 Laptop extremely quick. At first I didn't like Windows 8.1 but it is starting to grow on me. It is different from previous Windows operating systems so was a little hard to get around in the first couple of days. I like it better every day.

POSTED BY: datrop , florida
Overall rating: 4 out of 5 4 out of 5

I'm liking my birthday present very much. Only problem so far is the poor battery life. I purchased a Satellite for a friend and the Qosmio for myself and am totally envious of the battery life on hers as opposed to mine. For an item in this price range I definitely expected the battery life to be better.

Great Laptop - OS letdown

POSTED BY: OS Optionless , Detroit
Overall rating: 4 out of 5 4 out of 5

This is my third Qosmio (G25 & G55). The hardware on this laptop is terrific and it is fast. The one and only let down about the entire machine is the OS. I am not a fan of Windows 8.1. I ran Windows 7 ultimate on the G55 and it was a great laptop and provided daily performance for 5+ years. The only way this laptop could be improved is if Toshiba allowed buyers to choose between Microsoft's nannie OS and offer drivers for 7, so we could load up OS 7. I figured out work-arounds for most of problems and have my machine setup simiar to 7 ultimate but still have to deal with occasional 8.1 nuisances. I am comntemplating upgrade to 8.1 Pro for peace of mind, encryption capability on 2nd drive like I had on G55.

Overall Satisfied wish there was a better manual

POSTED BY: SharePointStacy , Florida
Overall rating: 4 out of 5 4 out of 5

I'm very satisfied with this machine. I run a virtual environment inside it via Windows Hyper-V, that supports two domain controllers, a SQL server, a Web Front end, and an app server for a sharepoint development farm. The disk speed is screaming fast! Wish the memory ports were more accessible and wish I would've bought a qosmio with 32 GB ram, vs this one with only 16GB Also, wish I had a better manual that showed how to access the other two slots, have to do some digging on that one. I bought the dynaDock U that was recommended off the spec sheet, it works like a champ. Make sure to follow the install directions to a T though. Don't just plug and play, else you'll be in for a world of hurt, if you're not tech savvy. Happy computing and cheers!! Stacy

It's overheating !!

POSTED BY: m1rkata , Rehoboth Beach, DE
Overall rating: 4 out of 5 4 out of 5

It's overheating when i play games and turn off for 2 min :( And i have coolpad !!

Disapointed with external monitor connections

POSTED BY: photodave , Grand Junction, MI
Overall rating: 2 out of 5 2 out of 5

While I am not a gamer, the video card, Gforce 770m, was a large part of why I bought this laptop. I do a fair amount of photo editing which is why I wanted the upgraded graphics. When I found the Gforce graphics only works on some games and the system defaults to the Intel graphics, I was very disappointed. When I connected two external monitors and found the best resolution I could get on them was 1920 by 1080 (they are 1980 x 1200 monitors) I was irritated. If not the for software and files I had already loaded on the computer, and the fact it works fine as a stand alone laptop, I likely would of returned it due to the limitations when connected to external monitors.

Screen Damaged

POSTED BY: Alejo , Medellin, Colombia
Overall rating: 1 out of 5 1 out of 5

I was using the laptop for one week, and suddenly, the screen started to look red. Im outside the US the the warranty is only in the US, so Its like I wasted the money.

MSRP: $1799.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8.1
  • 16GB DDR3L 1600MHz memory
  • 3GB GDDR5 NVIDIA® GeForce® GTX 770M with Optimus™ Technology
  • 1.25TB: 256GB Solid State Drive (mSATA, SSD) + 1.0TB (5400 RPM, Serial ATA)
  • Blu-ray Disc™ Rewriteable (BD-RE) and DVD SuperMulti drive

shop for accessories