Toshiba Satellite C55-A5126 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great laptop!

POSTED BY: nidianinoche , Las Vegas, NV
Overall rating: 5 out of 5 5 out of 5

I was upgrading from an XP computer and was thrilled to find this Toshiba, runs very fast and smoothly, easy to navigate and overall user friendly.

Great affordable laptop

POSTED BY: deadhorse , salt lake utah
Overall rating: 5 out of 5 5 out of 5

Great laptop acked with features and easy to use, my previous toshiba laptop lasted almost 6 yrs and still worked but i figured time for this new one, if i get 5yrs of life from this one ill be very happy

POSTED BY: Bitty Bug
Overall rating: 5 out of 5 5 out of 5

M first laptop and I love it!

Great Laptop

POSTED BY: Ftowns , Florissant Mo
Overall rating: 5 out of 5 5 out of 5

Windows 8.1 was not hard to get use to, love the look

Love this Laptop!

POSTED BY: Deanny , Raleigh, NC
Overall rating: 4 out of 5 4 out of 5

At first this laptop took some getting use to. But the tutorials taught me how to maneuver around the apps. I caught on quickly and now I love this laptop. The keyboard has keys large enough for my fingers. I'm enjoying this laptop.

Excellent value

POSTED BY: stilljerry , Mount Vernon, WA
Overall rating: 4 out of 5 4 out of 5

I am very happy with the Toshiba Satellite C55-A5126. It was an excellent value and has plenty of capability. I'm much less happy with Windows 8.1, but really appreciate that this Toshiba allows you to use the older desktop display.

Nice

POSTED BY: Bulls1754 , Scranton, Pa
Overall rating: 4 out of 5 4 out of 5

Great computer!!

Desktop replacement

POSTED BY: Biggie , Cheney, KS
Overall rating: 3 out of 5 3 out of 5

I bought as a desktop replacement for college and it works great for that. It's light and portable but make sure you carry your charger with you everywhere because the battery life is pretty terrible. Even with the Eco setting on.

POSTED BY: vt , Irvine, CA
Overall rating: 3 out of 5 3 out of 5

My laptop has quit working.

POSTED BY: sam , Pangburn, Ar
Overall rating: 2 out of 5 2 out of 5

My laptop has quit working. Last week the power button would not work and then the screen went dark. I removed the battery and finally with help got the laptop back on. But now I cannot get it connected to the internet. The Windows Security Center is turned off and I cannot get it back on. I WOULD VERY MUCH LIKE FOR SOMEONE TO CONTACT ME SO I COULD RETURN THE LAPTOP TO TOSHIBA FOR A REPLACEMENT OR COMPLETE REPAIR. I HAVE ONLY HAD THE LAPTOP OVER A MONTH AND ALREADY HAVING TOO MANY UNRESOLVED PROBLEMS. CAN SOMEONE PLEASE CONTACT ME. THANK YOU, SHARON POE

what a wast

POSTED BY: professor , massachusetts
Overall rating: 1 out of 5 1 out of 5

windows 8 is awful you have to buy everything new to do anything except email i have very poor internet at home so i can only use the computer at work cant even play solitar

MSRP: $355.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor 3558U
  • Windows 8.1
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories