Toshiba Satellite C55-A5140 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent laptop

POSTED BY: PAmigo
Overall rating: 5 out of 5 5 out of 5

Enjoying my Toshiba Satellite C55 laptop. Heard all the horror stories about Windows 8, but I'm having no problem using Windows 8.1 on this laptop.

Best company ever

POSTED BY: Skye , NC
Overall rating: 5 out of 5 5 out of 5

Ever since my first Toshiba, I have loved this company! I always recommend Toshiba to any of my friends who are looking for computers.

really great laptop

POSTED BY: duke , albuqerque,nm
Overall rating: 5 out of 5 5 out of 5

This is the greatest laptop I have ever owned!!!!!!!!

Windows 8.1 is Difficult

POSTED BY: Bob , Tucson, AZ
Overall rating: 4 out of 5 4 out of 5

I wish that I had not gotten Windows 8.1. I can't figure out how to use it.

it's ok

POSTED BY: Ann , Dallas Tx
Overall rating: 4 out of 5 4 out of 5

it's not what i though it would be.but i am ok with it

School Tool

POSTED BY: 9Flanders , Portland, OR
Overall rating: 4 out of 5 4 out of 5

Room to add to make it user friendly, keyboard is touchy

Not Happy In Texas

POSTED BY: Justice , Marlin, Tx
Overall rating: 3 out of 5 3 out of 5

After having my laptop for a week the hard drive went out which cause me to send it back to the store it was purchased from for repairs instead of replacement. It took almost a month to get my laptop back, which caused me to miss several online classes and now I have to reschedule them. Not happy in TEXAS

Typical Windows Laptop

POSTED BY: Nutmeg
Overall rating: 3 out of 5 3 out of 5

I am used to a MAC and i regret buying this laptop. Far more crashes, slower, many security holes. I has many more feature then i need/want and seems to clutter up the desktop with the "Launchpad" This is more an issue with windows but Toshiba loaded even more features which just slow it down

POSTED BY: Tracy , Canton, IL
Overall rating: 2 out of 5 2 out of 5

This Toshiba has a lot of features for the price however, it runs very slow. I was trying to save some money by purchasing this, but found out it wasn't worth it. I ended up sending it back. Windows 8.1 is awful, and because the computer was so weak it didn't seem to have enough power to run Windows 8.1.

Too much for me

POSTED BY: maxmach , Belleville,IL
Overall rating: 2 out of 5 2 out of 5

m used to receiving more than "scratch pad" manual. Am in my tech eighties and feel as if my tech level is limited to the on/off switch with the current ops. system.

MSRP: $379.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor N2820
  • Windows 8.1
  • 4GB DDR3L 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories