Toshiba Satellite C55-A5166 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Pleasantly pleased

POSTED BY: CR Esteban , Hawaii, Hawaii
Overall rating: 5 out of 5 5 out of 5

My last 4 notebooks were Sony Vaio's, and I was reluctant to change. I am quite happy with this notebook. It starts quickly, and I have none of the problems I have had in the past with Sony. This is not a temperamental machine. It is very stable, and I have yet to do a full system restore. I am concerned about the file structure. When I create a guest account, the "C" drive is shared, and any files I have on the "C" drive are not kept from the guest, even though I have administrative control.

Best Laptop Ever!

POSTED BY: cbryderf600 , Davenport, Florida
Overall rating: 5 out of 5 5 out of 5

This is the best laptop ever as I have a Dell also and it is so slow.

Excellent Laptop!

POSTED BY: Dmw , Az
Overall rating: 5 out of 5 5 out of 5

This laptop is fast and the quality is great for the price point!

Almost Great

POSTED BY: Silverwolf , Decatur,AL
Overall rating: 4 out of 5 4 out of 5

Only real issue is opening the DVD drawer. Should have been less difficult!

Great Laptop

POSTED BY: bob , waldoboro, me
Overall rating: 4 out of 5 4 out of 5

a good laptop but should have a little more software included. Great laptop for the money

MSRP: $439.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3110M Processor
  • Windows 8.1
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories