Toshiba Satellite C55-A5182 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop!

POSTED BY: SuMac , Sumter, SC
Overall rating: 5 out of 5 5 out of 5

I really like my Toshiba laptop. It's lightweight, yet has a big keyboard. It was easy to set up wireless Internet and wireless printer. I haven't depended on the battery life yet.

Suprisingly easy and efficient laptop

POSTED BY: Buckeyenut , San Antonio, TX
Overall rating: 5 out of 5 5 out of 5

All aspects of the C55-A5182 are very good. The laptop speakers are "sound", but using external speakers or earphones you can enhance with the DTS app to make the sound quality 100 times more pleasing. Overall, seems to be the right choice for my personal needs.

Great Laptop1

POSTED BY: Face , Wanaque, NJ
Overall rating: 5 out of 5 5 out of 5

Went looking to replace an 8 year old laptop and did not consider looking at a Toshiba. However, this was recommended to me and I am very pleased with my choice.

Great Laptop

POSTED BY: Mad Dog , Clinton, TN
Overall rating: 5 out of 5 5 out of 5

As I have primarily used desktop computers in the past, this is only the second laptop I have ever purchased. I bought my first one about 10 years ago, and the improvements since then are amazing. The screen size, the weight, and the processing power of this new computer are very impressive. Factor in the reasonable cost, and it becomes a truly great computer. I highly recommend it!

excellent laptop

POSTED BY: homebuilder , Winston-Salem NC
Overall rating: 5 out of 5 5 out of 5

good value and performance for the money. Took a little time understanding Windows 8. I like it now.

Excellent Choice of Laptop

POSTED BY: Trailboss , LaGrange, GA
Overall rating: 5 out of 5 5 out of 5

I have been using laptop computers since 1987 and have experienced many different brands over the years. I like the Satellite the best of any I have had. The performance is excellent, the graphics crisp and clear and this computer works very well for word processing, spreadsheets and gaming. I have only had to contact Support once, and I was immediately speaking with a technician who quickly and efficiently resolved the problem. I like the wide screen and the light weight of the Satellite makes the computer highly portable. My only negative observation is that the keys are a bit "sticky" leading to above average typos when word processing.

High quality lap top

POSTED BY: Albert , San Diego, CA
Overall rating: 5 out of 5 5 out of 5

Fast, high capacity, convenient, high quality lap top.

Enjoying my new laptop

POSTED BY: Annie , Mendon, MA
Overall rating: 5 out of 5 5 out of 5

I needed a new Laptop for my work. This has certainly done the job.. Nice big screen that is easy to see. Not too heavy to carry to and from the office.

Good value

POSTED BY: Kurt , Jasper, IN
Overall rating: 4 out of 5 4 out of 5

I would like to have a touchscreen, but it doesn't seem to be worth the extra cost. This computer does everything I need it to do. I would recommend using a mouse, though. It seems to work better with Windows 8 and 8.1 than the touchpad.

Great for a college student

POSTED BY: Al , New York
Overall rating: 4 out of 5 4 out of 5

I have used Toshiba laptops and that is why I bought this brand. I however am still trying to understand Windows 8. I overall am pleased with this laptop.

Nice Laptop

POSTED BY: jim , Troy,NY
Overall rating: 4 out of 5 4 out of 5

Really enjoy the speed,almost too fast ,only thing windows 8 was a little clunky , but working through the learning curve just fine.

Very Good Laptop

POSTED BY: Travelady , Carnesville, GA
Overall rating: 4 out of 5 4 out of 5

Responsive operation, bright screen, great keyboard, But rather slow to load upon start-up. Very inconvenient to have accessory ports on the right side instead of at the back. Too many unwanted pre-installed programs on the start-up screen.

good laptop

POSTED BY: Old man , Lakeville, MA
Overall rating: 4 out of 5 4 out of 5

Laptop is great 8.1 is too confusing Should have stayed with Windows 7

Great laptop

POSTED BY: Kaylie , Glendale, AZ
Overall rating: 4 out of 5 4 out of 5

Getting use to a laptop

POSTED BY: Maxine , Hartland, VT
Overall rating: 4 out of 5 4 out of 5

I am new to a laptop, and purchased this one on a recommendation. Very pleased with it, but still getting use to using the mouse pad. I am learning as I go. Would be nice to have the instructions included with the purchase, not just on line. I am one of the few who does read them!

POSTED BY: dickdot , MA
Overall rating: 4 out of 5 4 out of 5

Poor speakers. Sometimes need earphones to understand talk or music.

Thanks good value

POSTED BY: Kato , Alabama
Overall rating: 4 out of 5 4 out of 5

I am pleasantly pleased with this laptop. I bought two, one for myself and one for the wife. We are pleased so far.

Basic laptop value

POSTED BY: Bill , Cranston, RI
Overall rating: 4 out of 5 4 out of 5

Solid performance from a low priced basic laptop. Display quality very good.

Speakers Stink

POSTED BY: Biker Skier , Northern New hampshire
Overall rating: 4 out of 5 4 out of 5

I had a dell and it was hooked up to a Bose external speaker system. I read the horrible reviews on the sound but figured it would be fine with the external speakers...I could not have been more wrong. Sound is atrocious. I am not quite sure how you can screw up the sound on a laptop so bad but they did.Horrible. I use to spend my time on line cranking my tunes or Pandora and I cannot now. If you like music do not buy this laptop...other than that it is a great unit............

laptop

POSTED BY: handyman , Glendale, AZ
Overall rating: 4 out of 5 4 out of 5

T New laptop is faster, but has some of the same quirks as the old one (HP). Tried to use the finger scroll, but had too much touble with goofy stuff happening and had to go back to the wireless mouse. Was disappointed that after shopping for a new laptop, that by the time you add all the reqd software, the Toshiba was hardly the bargain I thought it would be.

Good Laptop

POSTED BY: mimi , Wilmington, DE
Overall rating: 4 out of 5 4 out of 5

I have beem very happy with my laptop. This is my first laptop and it does everything that I need. I use it mostly for the Internet and email.

Just another value for money laptop

POSTED BY: sudipta178 , Charleston, WV
Overall rating: 3 out of 5 3 out of 5

Good battery life but no Bluetooth. Outer body is not hard enough specially at the back. Not the best key board or soft touch. Overall a value for money deal with 6GB or RAM.

Average in every way

POSTED BY: MJRaleigh , North Carolina
Overall rating: 3 out of 5 3 out of 5

This is a basic machine that handles fundamental tasks fine. It has, though, a variety of small frustrations that add up to a very mediocre experience. Several keys, for example, have to be punched hard to work. The mousepad is frustrating and it's difficult to find out how to change settings. The price was good.

Average laptop

POSTED BY: Cork , Hummelstown, PA
Overall rating: 3 out of 5 3 out of 5

Unable to get it to boot from DVD drive or flash Drive(USB) yet.

Software

POSTED BY: bs , Coeur d'Alene, Idaho
Overall rating: 2 out of 5 2 out of 5

Overall, this is a nice laptop. However, the software is the worst I have ever used. Microsoft has managed to this up. All of the ads that keep popping up while on the net allows very little time for surfing. I have tried to find out how to disable the ads and all of the redirecting to no avail. Tech support is almost non-existent. The knowledge base has nothing to do with the software problems.

Toshiba Satellite Laptop

POSTED BY: ockie , Meadowbrook, Pa
Overall rating: 1 out of 5 1 out of 5

Did not like the Laptop. Returned it after several days

not real happy with this computer

POSTED BY: Lizzy , daytona beach florida
Overall rating: 1 out of 5 1 out of 5

The computer is quirky. Programming and set up are very difficult. Maybe good for a beginner or child.

difficult to use

POSTED BY: dislike windows 8 , lake wales fl
Overall rating: 1 out of 5 1 out of 5

difficult to set up programs programs easy to lose home page problems I believe it was set up for a touch screen not a key board

MSRP: $529.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-4000M Processor
  • Windows 8.1
  • 6GB DDR3L 1600MHz memory (max. 16 GB)
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories