Toshiba Satellite C55-B5202 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: joe , North Carolina
Overall rating: 5 out of 5 5 out of 5

perfect laptop

POSTED BY: florida girl , holiday, fla
Overall rating: 5 out of 5 5 out of 5

This laptop is so simple to use, and I needed simple ! But now I am becoming more and more knowledgeable, because it makes it so easy to venture out of my comfort zone. Thank you for making such high-quality products.

Was stolen shortly after getting it

POSTED BY: Tray , Denver co
Overall rating: 5 out of 5 5 out of 5

I loved my laptop for the short time I had it. Sadly was stolen from my boyfriend room close to 3 weeks after getting it. It was reported and at the end of everything I was in formed that there really isn't anything they can do for me. Thank you for the product for what I do know of it. A wonderful item

Best laptop ever

POSTED BY: Beautiful , Tallassee Ala.
Overall rating: 5 out of 5 5 out of 5

very happy

POSTED BY: slots , dover ohio
Overall rating: 5 out of 5 5 out of 5

was not aware this unit had no cd drive in it. read specs more careful.

great laptop

POSTED BY: brucelee24 , erie pa.
Overall rating: 5 out of 5 5 out of 5

this is my first laptop and I chose Toshiba because of the reviews I read helped. I will suggest to anyone who are looking for a laptop.

Toshiba was Better then Expected...

POSTED BY: MJH- 64 , Green Bay, WI. USA
Overall rating: 5 out of 5 5 out of 5

I found out Toshiba Laptops are pretty nice, Better then I first thought. The model I purchased didn't have a CD / DVD drive installed in it. I really didn't need one because, I down load everything on line any way, ( Most of your stuff you have on the computer is from on line.) Think about it? The best part of this laptop is the speed for getting around on the web. / Down loading speed is good too. The extra large button for the power on is really nice too. I love how the unit powers up pretty fast from the start up. Faster then most I have had before, with Microsoft, windows 8.1 operating system. The brightness and color on the screen seems to be better then some laptops I have seen and used before. I found that this laptop just for everyday use, for getting around on the internet, checking your email, and on line banking, is perfect for this kind of usage, nothing fancy, and with not many bells and whistles. It does the job for what I need it to do. I bought a case for this unit to take with me, where I can WIFI on line almost any where. It's getting more and more popular all the time. (free internet) I love it. One "Con" about this unit ... the ram can not be up graded more then a 4 GB, it seems to be fixed in place on the board. I like to have a least a 6 to an 8 GB ram memory, seems to work better then a four GB. But I still love this laptop.

Innovative design

POSTED BY: cocoette , Erie, PA
Overall rating: 4 out of 5 4 out of 5

Yes, I agree, Toshiba is truly innovation in laptop design. However, what really irritates me about my Toshiba lap top is the share waste of real estate space with the "Switch between apps: Move your mouse pointer all the way into the corner and then click to go back to the last app you were using" that occupies the top left hand corner of my screen. So how do I make this feature to not show up on my window screen. I do not need the info or tip.

It does what I wanted it to do

POSTED BY: Venice Joanne , Venice Florida a
Overall rating: 4 out of 5 4 out of 5

It is really easy to use. Only problem I have is with the print, I must hit the a wrong key and the print gets bigger or smaller, but easy to fix when I know what I'm doing

POSTED BY: sudhir
Overall rating: 4 out of 5 4 out of 5

POSTED BY: sudhir
Overall rating: 4 out of 5 4 out of 5

very good laptap

POSTED BY: adam , lake worth fl
Overall rating: 4 out of 5 4 out of 5

satisfied

POSTED BY: rick , seattle wa.
Overall rating: 4 out of 5 4 out of 5

this is my second Toshiba satellite laptop. I like both windows 7 and 8.1. smart pc for the money rick

i do love it

POSTED BY: coy , moselle ms
Overall rating: 4 out of 5 4 out of 5

i like how you can magnify the screen from the mouse

Solid, affordable laptop

POSTED BY: Lomax , LA, CA
Overall rating: 4 out of 5 4 out of 5

Good value for the price. Fast responsive processing, solid screen, but the keyboard is a bit cheap. Definitely could be better. Positive impression overall.

POSTED BY: Nurse , Conneaut, PA
Overall rating: 4 out of 5 4 out of 5

Laptop

POSTED BY: Ar , Lake worth fl
Overall rating: 4 out of 5 4 out of 5

The computer is great for the value. I hate windows 8

review new unit

POSTED BY: bikerdude , tx
Overall rating: 3 out of 5 3 out of 5

happy with the Toshiba, but still having trouble with windows. the only problem with Toshiba is that I cant lock in a password, so I don't have to enter it EVERY time I start my computer

Needs optical disk drive

POSTED BY: 1977harleyd , Glendale, AZ
Overall rating: 3 out of 5 3 out of 5

It's a good computer for the price. Window's 8.1 takes a bit to get use too. I would not have purchased it, if I had realized there is no optical disk drive. Why would you not include it???

works great for low end PC

POSTED BY: Jim , Lehigh valley, pa
Overall rating: 3 out of 5 3 out of 5

Can`t beat the price. Has too many apps built in for me . Added mouse seems to work better.

No DVD Support

POSTED BY: LL , Chicago, Il
Overall rating: 3 out of 5 3 out of 5

Just got the laptop. Had to go back to buy external DVD player. Not happy. Rented 2 movies but will have to return unused because laptop has no DVD support. Not happy. Angered that I have not found solution. Downloaded several programs to no avail. Gave up, went to sleep. That alone would have kept me from buying the Toshiba Satellite C55-B5202

another laptop

POSTED BY: pa_trick , Yelm, wa
Overall rating: 3 out of 5 3 out of 5

This satellite is good value for money, however the touch pad interface keeps freezing user accounts. The drivers say they are up-to-date. This makes the 38th toshiba laptop that I have purchased.

one USB port and sound ports are not working

POSTED BY: FLURITIBA , Curitiba - Brazil
Overall rating: 2 out of 5 2 out of 5

Good LapTop. Simple, but, good. EXCEPT: One USB port and the sound ports ARE NOT WORKING! I'm very sad with this... I bought two LapTops, same models, C55-B5202, to my sons, but, one of them, is with this related BIG PROBLEM

do not buy! made for look and not function

POSTED BY: domo23
Overall rating: 1 out of 5 1 out of 5

This has to be one of the worst laptop i have ever had.the only thing i like,is the appearance.this is more like a Windows phone(horrible phone) than a computer.I can do more on my cell phone than this.My WiFi never stays connected and my touch pad does not sense well.there are so many useless apps on the pc.It does not include a disc drive or any Microsoft office products as i expected.I really wish i can get my money back.

Worst Laptop I have Had

POSTED BY: Disappointed , Mishawaka, IN
Overall rating: 1 out of 5 1 out of 5

I have had multiple toshiba laptops and always loved them. So when I had to get a new one, I stuck with the brand I like. Wrong answer. I HATE this laptop and have had trouble since day 1. It runs slower than computers I had 10 years ago, has trouble staying connected, and the mouse/sensor has issues too. There is no disk drive which was not apparent when I bought it. I have had it about 4 months and it is useless.

holding internet connection terrible

POSTED BY: Mwife , Iowa
Overall rating: 1 out of 5 1 out of 5

This is the 4th Toshiba that we own. We love the other 3. This one has a terrible time holding an internet connection. Our other computers work just fine. Even if I am the only one on-line I still have a terrible time with it.

Greatest chrasher yet

POSTED BY: gotmeagain , Charlottte, NC
Overall rating: 1 out of 5 1 out of 5

Why everyone who builds these new programs think they are doing a great job. Then why do they continue to need to up date our operating programs over & over again. I had this computer for 18 months when a Micrsoft regular scheduled up date crashed the computer to never work again. I had nothing to do with the reaction, as I just let it do it's up date while I watched tv. When it said it was going to re-boot. I got booted into spending hundreds more for a new laptop. Not this product again. Are they really up dates or privacy thieves?

MSRP: $249.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor N2830
  • Windows 8.1
    1 month trial for new Office 365* customers
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive

build your own C50 shop for accessories