Toshiba Satellite C55D-A5163 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Beatrice Coleman Patrick

POSTED BY: Bea , West Palm Beach, Florida 33401
Overall rating: 5 out of 5 5 out of 5

Overall, I have been very impressed with my Toshiba. It's lightweight which was most important to me.The keyboard is easy to use and sits at the right for me. There is a lot to learn about what my computer can do but, it was easy to start working right out of the box.

Toshiba Laptop

POSTED BY: BOWER013 , Tuscaloosa, AL
Overall rating: 5 out of 5 5 out of 5

This is a great computer and I was able to navigate with Windows 8, even though I had not used it before. I downloaded software with ease and the applications activate in a timely manner. Very pleased with my purchase.

Great laptop but need some changes

POSTED BY: Calex , Jacksonville, Fl
Overall rating: 5 out of 5 5 out of 5

I have used a Toshiba laptop in the past, but much has improved. That other laptop was much heavier and like carrying a case of bricks. The C55 Satellite Series is much lighter and a pleasure to carry around. I don't like the placement of the power cord outlet. Instead of being on left side of the laptop, the power outlet should be relocated behind the monitor or on the right. The hand rest has a lip that makes long-term typing very uncomfortable. This area should be more rounded. Lastly, the optical drive button is very awkward to locate. The optical drive button is so flush against the computer, I have to lift and turn the computer to see it because I can't feel it. Other than that, I very, very happy with my new laptop. Thank-you so much.

Excellent

POSTED BY: rw1751 , Hatboro, Pa
Overall rating: 5 out of 5 5 out of 5

Love this Laptop, just takes a little getting use to windows 8.1 and getting around but I am still learning. Speakers could be a little better, but I hooked up external ones also and makes sound much better. I also bought a wireless mouse makes it a little easier.

easy set up

POSTED BY: seagal , Brookings, Oregon
Overall rating: 5 out of 5 5 out of 5

The instructions were easy to follow to set the computer up for the first time. Coming from an XP I was worried about navigating an 8.1 but it was easier than I expected.

My Awesome Laptop

POSTED BY: Gricy , Pirtleville,AZ
Overall rating: 5 out of 5 5 out of 5

I have a month with my laptop and I love it. It has everything I need it for. All the features it contains are awesome. I should have gotten it sooner.

Great Laptop

POSTED BY: Debfay , Albany, Ga
Overall rating: 5 out of 5 5 out of 5

This laptop is really great and very functional.

Toshiba Satellite C55D-A5163 Laptop

POSTED BY: Openminded , NORTHERN MICHIGAN
Overall rating: 5 out of 5 5 out of 5

Absolutely the Best of the Best Laptops I have ever owned. I personally and highly recommend this product

love it

POSTED BY: sassy , Paulding,ohio
Overall rating: 5 out of 5 5 out of 5

it is very easy to use and very easy to understand

Great laptop

POSTED BY: kenny , Spring Creek,Nevada
Overall rating: 5 out of 5 5 out of 5

awesome laptop

POSTED BY: pabullrider , Mainesburg,PA
Overall rating: 5 out of 5 5 out of 5

I never used a laptop,this is awesome better then a desk top

First laptop ever

POSTED BY: Pam , Castro Valley
Overall rating: 5 out of 5 5 out of 5

So far it's great, it does everything I would want or need in a laptop. I love it so far.

Love my new Laptop

POSTED BY: Shell , Big Sandy,TN
Overall rating: 5 out of 5 5 out of 5

This is my 1st laptop. I really like it & and am also learning more on how to use it.

Very satisfied over all

POSTED BY: Mr. Bill , Taylors,SC
Overall rating: 5 out of 5 5 out of 5

so far great performance, good graphics, large viewing screen, battery is great so far., Good Camera photos and web cam works GREAT./\. no complaints so far..

I really like it!

POSTED BY: evincent2010 , Marshfield, WI
Overall rating: 4 out of 5 4 out of 5

I really like my new laptop. I love the display and how clear it is but, I wish it was a little faster. I have always had intel laptops in the past but, this one is an amd and is slower than my last laptop. It may be because I haven't shut off all the programs that don't need to be running the background.

POSTED BY: toots , Petrolia PA
Overall rating: 4 out of 5 4 out of 5

I real like this laptop and it as very affordable

New Experience

POSTED BY: Niret , Goshen, IN
Overall rating: 4 out of 5 4 out of 5

I am still learning! Must put laptop to more use. At this point I don't understand all setup/apps, etc.

Good laptop

POSTED BY: Markiestar , Philadelphia, PA
Overall rating: 4 out of 5 4 out of 5

This is a good laptop. The only thing I was disappointed with was that it did not come with a program such as office or word. Other than that, it's a pretty good laptop.

laptop

POSTED BY: oldman , jacksonville, FL
Overall rating: 4 out of 5 4 out of 5

easy to operate, and has worked so far on every function--we have asked it to do.

highly recommended

POSTED BY: ruffy , milton,fl.
Overall rating: 4 out of 5 4 out of 5

difficult operational accessories. unaware of how to use all the features. a big difference from using windows7

Grandparent Savvy

POSTED BY: Jblack11
Overall rating: 3 out of 5 3 out of 5

The SLOWEST laptop I've ever had! Not college friendly.

questionable Laptop

POSTED BY: wolfman4 , Northbrook IL
Overall rating: 3 out of 5 3 out of 5

Am having a problem with my Toshiba Satellite laptor. It will not hook up to my home router. the router hooks up to all my other devices. So I am not too happy with Toshiba.

Unhappy Camper

POSTED BY: Nawdx , Spring, TX
Overall rating: 3 out of 5 3 out of 5

I'm not sure if I'm more frustrated with the weight of my lap top or the Windows 8 operating system ... both are causing me the blues ... that is then complicated by the fact that it is my first "AMD" system ... Can I return it for a full refund! ...

Its ok with out Windows 8

POSTED BY: MrGrimm , East Coast, PA
Overall rating: 3 out of 5 3 out of 5

Windows 8 is the key downfall, its not to be used on laptops with out touch screens. Untill they MS gets with it, and comes out with a OS that isn't bad for touchless systems, then i'll keep Windows 7

c55d webcam

POSTED BY: logoduck , treton,nj
Overall rating: 3 out of 5 3 out of 5

the webcam on my new toshiba c55d is way out of focuss

Fair Laptop

POSTED BY: Mike , Cordova Md
Overall rating: 3 out of 5 3 out of 5

I have high speed internet and this Laptop takes a long time to upload

Laptop

POSTED BY: Space , Salyersville ky
Overall rating: 2 out of 5 2 out of 5

I cannot do things like play a disk or take a picture for homepage start up without errors

OK LAPTOP

POSTED BY: CYNDERELA , NASHVILLE TN
Overall rating: 2 out of 5 2 out of 5

I CANNOT FIGURE OUT HOW TO MOVE TO THE SCREEN I WANT. CANNOT FIND THE TURN OFF ON SCREEN OR TO GET OUT OF WHATEVER IM IN AT THE TIME. IT IS NOT USER FRIENDLY. THE COMPUTER AT WORK IS EASIER. MY OLD LAP TOP HAD ICONS AT THE TOP TO CLICK ON TO GET OUT OF A PROGRAM ..I MISS THEM. I HATE THE WINDOWS THING ..ONCE IN THERE IS NO OUT

Very disappointed

POSTED BY: Lanette , Sarasota FLorida
Overall rating: 2 out of 5 2 out of 5

I bought this laptop for school thinking it would be sufficient for me, but I have only had it a month and it is very slow, the processor is slow and not enough memory.. I cant get my school work done most of the time because it freezes up. the keyboard sticks and sometimes does not even work Not happy and want to upgrade

computer

POSTED BY: nbqtie , Nichols, NY
Overall rating: 1 out of 5 1 out of 5

The internet has not worked since I got it

Do not like

POSTED BY: LIZ , Cedar Bluff, Va
Overall rating: 1 out of 5 1 out of 5

Very slow, difficulty connecting to internet, hate 8.1 Camera produces poor quality pictures. Am returning product.

Junk

POSTED BY: Not satisfied
Overall rating: 1 out of 5 1 out of 5

I wish I never had boughten this computer, it's slow, it freezes. I've used apple computers my whole but did not have the extra money to get a new one, what a mistake not sticking with Apple. I do not like anything about this computer and the operating system terrible, toshiba definitely does not make a good computer.

MSRP: $364.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-2100 Accelerated Processor
  • Windows 8.1
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories