Toshiba Satellite C55D-A5381 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

from desk top to lap top

POSTED BY: autotech , wynesville,nc
Overall rating: 5 out of 5 5 out of 5

love it! cranks right up every time and,runs very smoothly.very efficient at gear changes and battery charge seems very stong.impressive! sales person quoted 4 hours battery span but it generally is more like 6 or 7. I am far from an expert on laptops but this one sure works great for every thing i do

POSTED BY: Joe , Greenville,Fia.
Overall rating: 5 out of 5 5 out of 5

it is a good product for the price

laptop c55d

POSTED BY: dary , fort wayne,in
Overall rating: 4 out of 5 4 out of 5

very good machine, disappointed in windows 8. i enjoy it

Adequate

POSTED BY: postmn , New Milford, NJ
Overall rating: 3 out of 5 3 out of 5

Computer is slow, it has one USB 3.0 port which has an intermittent connector on it sometimes it works. No keyboard light meaning you can't use it in low light and videos plays poorly all jittery not smooth at all. If you want to play a DVD put the disc in and go get a cup of coffee, by the time your finished drinking it maybe if you are lucky the movie will be done loading and ready to play, but only maybe. In short if you see this laptop on the shelf RUN don't walk away!

Having Trouble

POSTED BY: John , Glen Rose, TX
Overall rating: 3 out of 5 3 out of 5

Would nor buy again.

Ehhh.

POSTED BY: Eve , Sacramento, CA
Overall rating: 3 out of 5 3 out of 5

Toshiba brand aren't the best. They are quite slow at performances. I rather get Dell if I could choose.

Windows 8 ruined your laptop

POSTED BY: Clyde
Overall rating: 3 out of 5 3 out of 5

If it wasn't for windows 8 it would have been a pleasant experience. I am now getting my first Mac. I'm through with windows.

MSRP: $315.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-1200 Accelerated Processor
  • Windows 8
  • 4GB DDR3 1066MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories