Toshiba Satellite C55t-A5102 Touchscreen Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My New Toshiba Laptop

POSTED BY: MrPG , Schaumburg IL
Overall rating: 5 out of 5 5 out of 5

I had an old slow computer running Windows XP so it was time for a change. I told the salesman what I used the computer for and he recommended this one. No regrets. It is not the most expensive or the top of the line but it is fast, works fine, and I have had no problems at all in the one month I have had it.

great laptop

POSTED BY: mrbhb , Sun City West Az
Overall rating: 5 out of 5 5 out of 5

The resolution is great. It is very easy to use the touch screen. I really like the DVD slot. Most laptops in this price range do not have one.

learning and enjoying

POSTED BY: belle , way north, NY
Overall rating: 5 out of 5 5 out of 5

More fun than my 10 year old Toshiba, very quick and nice screen especially for my photos.

POSTED BY: Ted , Williamsport, Pa., USA
Overall rating: 5 out of 5 5 out of 5

This lap top appears to be performing well. I like the option of using the mouse or touch screen and alternate often. I moved from windows XP to 8.1 and easily adapted to the change. I recently downloaded a book and enjoy reading on this computer. I purchased this computer about a month ago and am satisfied with the performance to date.

Not too shabby!

POSTED BY: mjb1018
Overall rating: 4 out of 5 4 out of 5

Overall the laptop is fast, very responsive. The only issue I have is the terrible sound from the stock speakers, but hey its a laptop, I simply use a sound bar and problem solved. Nice looking design and the 10 keys are handy to have, the HD cam is great for video calls and colors are fairly vibrant not the best but quite good.

Good laptop for the price!

POSTED BY: Bbbbb , Las Vegas w
Overall rating: 4 out of 5 4 out of 5

Needs a lite keyboard, other thn that it is good for your everyday user.

Happy

POSTED BY: Autumn
Overall rating: 3 out of 5 3 out of 5

I am satisfied except for one thing............the sound is terrible. I can't even get it to sound better with ear buds. I've never had this problem with any other computer. I love to watch movies and it is very upsetting to me to have the sound as bad as it is when watching movies. Nearly took it back.

Disappointing Laptop

POSTED BY: mamamia0709 , Dallas, TX
Overall rating: 2 out of 5 2 out of 5

This laptop has issues staying connected to my network. It doesn't download very fast and the flash player has been an issue since I bought it. I do not have many programs loaded on this device but the Toshiba programs running in the background, I believe, are what slows it down. Not happy.

Don't buy this Laptop

POSTED BY: Susan
Overall rating: 1 out of 5 1 out of 5

You really don't want to buy one of these. They're defective right out of the box. Traded it back at the store for an HP which works great -- right out of the box.

Dislike touch screen and lack of tutorial

POSTED BY: robert , Edgerton, WI
Overall rating: 1 out of 5 1 out of 5

no clear help, happy I kept my old XP driven Toshiba.

MSRP: $565.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-4000M Processor
  • Windows 8.1
  • 4GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories