Toshiba Satellite C55T-B5109 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent Laptop

POSTED BY: Rick , Revere,MA
Overall rating: 5 out of 5 5 out of 5

Top of the Line Laptop

POSTED BY: True Blue , New York City, NY
Overall rating: 5 out of 5 5 out of 5

The Toshiba Satellite C55T B5109 Laptop is the best ever. The touch screen features are beyond any ones imagination. This is the best laptop ever!

Great gift

POSTED BY: Jennifer , Newport News, VA
Overall rating: 5 out of 5 5 out of 5

I really am enjoying my new laptop. It is awesome!

Snazzy Laptop!

POSTED BY: Thelma , Denver, CO
Overall rating: 5 out of 5 5 out of 5

Pretty good!

POSTED BY: Legend , Frisco,TX
Overall rating: 5 out of 5 5 out of 5

This is my first laptop to own by myself (I got it for freshman year of HS). Touch Screen works amazing! One this I do not really like is the zoom. Every time you try to move the mouse, it zooms in or out.

first laptop

POSTED BY: dan , Hannibal Mo
Overall rating: 5 out of 5 5 out of 5

so far so good

POSTED BY: Blue , Suffolk, Virginia
Overall rating: 4 out of 5 4 out of 5

great for the price

POSTED BY: average_user_83 , Superior, WI
Overall rating: 4 out of 5 4 out of 5

If your looking for an everyday type laptop that you use on a daily basis to surf the web, check social sites, and listen to music, this is a good laptop for you. I use my laptop everyday to check my favorite websites and such. This laptop has lots of storage, great fit music and pictures, high amount of RAM so it's quick when multitasking. I love the touch screen! I can keep it in my lap and it doesn't burn my legs :-) the new Windows 8 takes a bit to get used to coming from Windows 7 but I'm getting there. Overall I give this laptop 4 out of 5 stars. Great price for it's specs.

LapTop

POSTED BY: jmymcg , KC, Mo
Overall rating: 4 out of 5 4 out of 5

I like it

POSTED BY: chinee , Trinidad
Overall rating: 4 out of 5 4 out of 5

Go with Me Laptop

POSTED BY: Rosie , Harrisonburg, VA
Overall rating: 4 out of 5 4 out of 5

I just needed a computer to do some internet surfing and work with Excel and Word. I found this one with the Touch screen and I absolutely love it. It was very reasonably priced and have found that i use it more and more for other things such as music and apps than I ever thought I would.

Best Value PC I've ever bought.....

POSTED BY: OregonBoy , Lake Oswego, OR
Overall rating: 4 out of 5 4 out of 5

I am really enjoying this Satellite laptop, it's a great size with a full keyboard, etc. and all the touchscreen magic that make sense with Windows8. Thing is I've been a multi OS user for a long time, and probably always will be. This has made me think hard though, it is such a good price and so well balanced a feature set for most of what I do that I've made it my main machine for now!! Nicely done Toshiba

Replaced a Dell that fried the hard drive.

POSTED BY: Phil , Brighton, MI
Overall rating: 4 out of 5 4 out of 5

xxx

Ok for the money.

POSTED BY: Big Mike D , Indianapolis
Overall rating: 4 out of 5 4 out of 5

This is a ok laptop for the money. The touchscreen is great but it does hesitate from time to time. I do have to click some web links with a mouse at times when I cannot select them by touch. The battery lasts about 3 hours. Overall it's a cheap intro touchscreen laptop and works for my purposes.

Love Hate relationship

POSTED BY: 1coolRN , Memphis, TN
Overall rating: 4 out of 5 4 out of 5

I love my new laptop. I love the touch screen. I'm getting use to how to use it. We somehow overlooked the fact that there is no optical drive on this thing and can't watch movies on it. Bummer! And at times I can't get anything done for all the Norton pop-ups. Wish it came with more user friendly instruction. but the battery life is crazy good. Great price. Love , love, love my touchscreen and being able to enlarge everything!!!!!

Good Buy

POSTED BY: Sailor , Florida
Overall rating: 4 out of 5 4 out of 5

Overall this is a very good value laptop, however, if you left click below the touch pad and contact any of the touch pad, it acts like a right click and requires a second click to clear it and proceed. Designing a small margin between the touch pad and the buttons would cure that problem.

Great Laptop

POSTED BY: Grannie , Milwaukee WI
Overall rating: 4 out of 5 4 out of 5

Very happy with the Toshiba Satellite B5109 Laptop. Still getting used to Windows 8 but am loving the touchscreen for some of the apps.

Sleep Issues

POSTED BY: Julie , Canberra, Australia
Overall rating: 3 out of 5 3 out of 5

When the laptop is working it is a fantastic machine, however when I put it to sleep overnight it does have problems waking up. After a few nights of sleeping I have to shutdown the laptop and then restart, otherwise the laptop does not power up .

what a piece of junk

POSTED BY: vick , julian, pa
Overall rating: 3 out of 5 3 out of 5

too many bells and whistles for my needs

ok but could have been better

POSTED BY: RN , mountainview Ca
Overall rating: 3 out of 5 3 out of 5

the build quality is a bit flimsy ..although the look and design is aesthetic and nice. also a basic dvd writer would have been a welcome addition I don't know why Toshiba needs to make a separate model by omitting it in this one. its like making a usb 3.0 or card reader as a special feature which is not available in all laptops ..just weird in this day and age

woest laptop ever

POSTED BY: none
Overall rating: 1 out of 5 1 out of 5

Hard to use. Response is very slow. I have an older Toshiba Sattelite that is the best laptop I have ever owned. Compared to it, this new one is garbage.

Not very impressed

POSTED BY: tj , Bonita Springs FL
Overall rating: 1 out of 5 1 out of 5

This is a birthday gift from my children. Normally, it would take me a week to be satisfied with the necessary basic operation. Unfortunately, it didn't come with a disk drive, it is very sensitive and responds slowly to commands. I could never tell the kids that I am not satisfied. Hopefully I'll learn to take full advantage very soon.

Very Disappointing

POSTED BY: thegeneral , Milpitas CA
Overall rating: 1 out of 5 1 out of 5

This laptop stopped working within 2 weeks of purchase. It is now in for repairs.

Not so great

POSTED BY: Kristin , Mashpee, MA
Overall rating: 1 out of 5 1 out of 5

Not very user friendly...very hard to figure out things on this computer. Computer and screen get stuck too. Wish I returned it earlier:( Forces you to create a Hotmail account and have that as your primary email. I have Comcast and would rather use that. I had to link it to my husbands account as to not create another email account. Now I see his emails all the time and forced to use his email as the login to the computer-NOT COOL!

MSRP: $535.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-4005U Processor
  • Windows 8.1
  • 4GB DDR3L 1600MHz (Memory is not user upgradeable, factory installed only)
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive

build your own C50 shop for accessories