Toshiba Satellite C75D-A7102 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great general purpose laptop

POSTED BY: chuckb
Overall rating: 5 out of 5 5 out of 5

I basically want a new laptop for document purpose and it is a great value.

toshiba saved my life!

POSTED BY: mardiclaw , new orleans, la
Overall rating: 5 out of 5 5 out of 5

I have a guy who repairs and does all the maintenance on my computers. I have always recycled my old ones with him, and have bought used as well. this time though? I wanted new, so her recommended this to me, and I am very pleased.

Good Value

POSTED BY: CPeter
Overall rating: 5 out of 5 5 out of 5

I needed a replacement for an older HP laptop that was running Windows XP. This is a second computer and not my main machine so I did not need the world's fastest. This has a nice 17" wide screen and at 500 gig the hard drive is plenty big enough. The processor is plenty fast for what I do, email and browsing and showing PowerPoint presentations.

Love my machine!!

POSTED BY: Barb , Ashville, AL
Overall rating: 5 out of 5 5 out of 5

Given to me as a gift. Have always had desktop and Dells. I love everything about this laptop. Easy to use and if I have a question I go straight to help and tips and get my answers.

toshiba is good lapot

POSTED BY: kw34 , brooklyn ny 11223
Overall rating: 5 out of 5 5 out of 5

i thank every one should try it

Doing well

POSTED BY: Flower , Lancaster, PA
Overall rating: 5 out of 5 5 out of 5

Basic laptop and has the features I was looking for. Long battery life. So far, all is well.

Great laptop at any price

POSTED BY: IL , Columbus, GA
Overall rating: 5 out of 5 5 out of 5

This laptop is as functional for home office use as laptops costing twice or three times as much. Great value for the money.

Great lap top!!!

POSTED BY: Doc , Houston, Texas
Overall rating: 5 out of 5 5 out of 5

It does everything I needed...

Nice laptop

POSTED BY: cigar guy , Philadelphia, PA
Overall rating: 5 out of 5 5 out of 5

Like Toshiba brand. Have used or owned other Toshiba products and have never had any problems.

My choice from many

POSTED BY: Sadim , New Port richey, FL
Overall rating: 5 out of 5 5 out of 5

My wife has a Toshiba Satellite and she loves it, but I wanted a larger screen so my choice was the 17''. I love the features.

Excellent laptop

POSTED BY: kp , Pine Valley CA
Overall rating: 5 out of 5 5 out of 5

Replaced an old 8086 xp laptop that my wife used mainly for the Web with this. What a difference! Bluetooth, WiFi to TV and Home easy as could be. And FAST!

Great laptop

POSTED BY: Bob , Thornton, Co
Overall rating: 5 out of 5 5 out of 5

Works great easy to use very fast

Excellent Performance and Value

POSTED BY: Continuing Education , Southern California
Overall rating: 5 out of 5 5 out of 5

Lower end PC purchase this time around. Very pleased with laptop. Lower end does not mean poor performing PC.

First Laptop ever

POSTED BY: dennis , Florida
Overall rating: 5 out of 5 5 out of 5

Having nothing else to compare my laptop to I would have to say it does what I want it to, when I want it to!

Great laptop

POSTED BY: golfnut , saratoga,n.y.
Overall rating: 5 out of 5 5 out of 5

This laptop is a great value. It is fast and feature filled. The HD screen is great.

Win8undecided

POSTED BY: Win8undecided , Southeast, US
Overall rating: 4 out of 5 4 out of 5

The screen size and it not being a Dell were two reasons i was drawn to this Toshiba. My issue is with Win8 and how difficult it is to use compared top earlier versions: Especially difficult with a second screen attached.

Nice and big

POSTED BY: Grackle , Arizona
Overall rating: 4 out of 5 4 out of 5

I like the full size keyboard and the screen. I only wish it came with Windows 7.

nice laptop

POSTED BY: Mike , Canada
Overall rating: 4 out of 5 4 out of 5

Laptop is nice with a big 17 inch screen. Getting used to windows 8 which gets better the more I learn about it. The computer is responsive and lots of features for the price.

my 1st. laptop

POSTED BY: Eskimo , Barrow,Ak.99723
Overall rating: 4 out of 5 4 out of 5

wish it had windows 7 so my mom of 78 years old had it easier to use.

Good laptop

POSTED BY: Dude , Newark, CA
Overall rating: 4 out of 5 4 out of 5

Over all it seems a little slower on boot up than my last computer probably all the apps they cram in there. Not especially happy with the new windows OS which seems more work than it should be, aren't revisions supposed to make use easier and not harder. The rest seems fine.

Windows 8.1 is confusing

POSTED BY: Rufus , Lansing, Michigan
Overall rating: 4 out of 5 4 out of 5

I am struggling with Windows 8.1. The Toshiba laptop I love.

Great Value

POSTED BY: Tom , Blue Bell, PA USA
Overall rating: 4 out of 5 4 out of 5

I think this laptop is a great value. Excellent speed, graphics, et al. However, I do not like WIN 8.1 and may revert to WIN 7. I think 8 might be a decent OS for touch screen, but complicates use in general.

Good laptop

POSTED BY: Stone , indianapolis,IN
Overall rating: 3 out of 5 3 out of 5

Good laptop for the money. Not a lot of extras. Advertised as having Bluetooth but it does not come with it.

So so...

POSTED BY: Charly , Vista, CA
Overall rating: 3 out of 5 3 out of 5

Laptop, OK, but Windows 8 stinks!!!! Not intuitive at all. Had to download features to make it more manageable. And is very time consuming. Hard to rate a product so soon! My old Toshiba Laptop overheats and read is a common problem, I don't know why.

ok laptop

POSTED BY: rick , mount airy,md.
Overall rating: 3 out of 5 3 out of 5

windows 8.1 is no good it is hard to navigate I don't know if is my laptop or windows but I would be on one page browsing and for no reason it swishes to one of the apps such as calculator or video player very frustrating

C75D-A7102

POSTED BY: phoneguy , Grand Forks, ND
Overall rating: 3 out of 5 3 out of 5

Not happy with this laptop....

Mixed emotions

POSTED BY: perfesser , Mankato, MN
Overall rating: 3 out of 5 3 out of 5

Toshiba makes a good product. The hardware is fine, no complaints. Unfortunately, they installed Windows 8 in it. It's hard to separate my feelings of frustration and irritation for the OS from the computer. This is by no means my first Toshiba laptop, and I have never had one die on me, but this is the first computer of any brand I've ever had that I have seriously considered killing!

not happy with laptop

POSTED BY: volybl4evr , Oakdale, CA
Overall rating: 2 out of 5 2 out of 5

I have the "C" key that does not type very well. I have to really press down hard for it type out. Also, for being a quad processor, it is really quite slow on several occassions.

Hopefully a lemon

POSTED BY: Petsi , Wisconsin
Overall rating: 1 out of 5 1 out of 5

I purchased this laptop after researching that it had greater than needed specs to run all the applications I use. It could barely run a majority of them. I checked all the settings, reviewed the forums and was unable to make it perform like it should have. I am hoping it was a combination of the horrible OS 8.1 and possible a bad build. I have since returned the laptop and purchased a competitor's laptop with lesser specs than the Toshiba and it is vastly outperforming it for about half the price. Toshiba in the past has built great machines, but I fear they may be going the way of Dell, Hp and Gateway.

Keys Randomly Won't Type

POSTED BY: Author Lori , St. Peters, MO
Overall rating: 1 out of 5 1 out of 5

After reading several of the reviews, I see that I'm not the only one who has problems with keys not typing. The main thing I bought the laptop for is to write. I normally type upwards of 90 WPM and that drops drastically when I have to go back and correct all the typos. The G, C, A, are the worst offenders. It's in the repair shop now, but I suspect they'll tell me it's in my head. :( I'm glad I kept my L505D-5983 as a back up. I LOVE that one. I just wanted a laptop with a bigger screen.

Not a computer, Windows 8 terrible

POSTED BY: jb
Overall rating: 1 out of 5 1 out of 5

I thought I was getting a computer. The most basic task that one should be able to do with a computer is to write a letter. There is no word processing program, therefore it is not a computer. Windows 8 is terrible. I can't navigate to "My Computer" or find documents as in previous Windows systems. Also, when trying to move the mouse pointer across the screen when in internet explorer the window jumps back to the Toshiba Home Page screen.

Recalled

POSTED BY: Nocare , Pa
Overall rating: 1 out of 5 1 out of 5

It was recalled

worst laptop i have ever owned

POSTED BY: vic , batavia, oh
Overall rating: 1 out of 5 1 out of 5

it came with no instructions it is very difficult to use I have had it a month now and am still having problems including loging on

Pop Ups

POSTED BY: bloodtrakker , Tennessee
Overall rating: 1 out of 5 1 out of 5

I'm STILL trying to get enough of the junk out of that computer to make it usable. From the minute I turned it on I've gotten pop up after pop up. Every time I change pages on Google Chrome I get pop ups. And it's not Chrome because I have Chrome on all my computers. Also the keys on the key pad do not work half the time - So I have to double check every thing I type in. I realize it's a budget computer - But this is rediculous! I will never buy another Toshiba.

MSRP: $443.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-5200M Accelerated Processor
  • Windows 8.1
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C70 shop for accessories