Toshiba Satellite C75D-A7130 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

NICE LAP TOP FOR THE $$

POSTED BY: DUCK1128 , BROADVIEW HTS, OH
Overall rating: 5 out of 5 5 out of 5

The laptop worked as advertised out of the box. DVD player and other options are easily used. Keyboard is well positioned. This is my second Toshiba laptop and will likely buy another when the time comes.

second time around

POSTED BY: dew , Dayton Oregon
Overall rating: 5 out of 5 5 out of 5

I just recently had to replace my old Satellite Laptop with vista, it finnaly wore out after many hard years of use. Of course I wanted another Satellite Laptop. I was pleased to find that I could get a 17" as my vision is not so good. I am still getting use to the new Satellite as there has been some changes, but the only complaint I have is not Toshiba's fault--windows 8.1 would not be my choice, hopefully I can fix that.

LITTLE DIFFERENT BUT SO AM I!!

POSTED BY: YO , EVANSVILLE, IN
Overall rating: 4 out of 5 4 out of 5

I love the bigger 11.3" screen and once i got used to the Windows 8.1 i like it alot. Took some adjusting but makes sense to me now.

New Laptop

POSTED BY: Sue A , Cookeville, TN
Overall rating: 4 out of 5 4 out of 5

I had the large laptop so the smaller size is taking a little time to get use too.

Absolutely love my laptop!

POSTED BY: Wicked Obsession , Kuna, Idaho
Overall rating: 4 out of 5 4 out of 5

I love my laptop and recommend it to my friends!

First Good Laptop

POSTED BY: Jwurgz
Overall rating: 4 out of 5 4 out of 5

Easy to use, amazing setup options, a lot of different features, and great performance.

Nice laptop with new Windows 8.1 OS

POSTED BY: GodfatherRob311 , Florida
Overall rating: 4 out of 5 4 out of 5

This laptop has a large screen with the latest Window OS with long battery life. I currently use MS Office 2013 on it and it preforms great. The only downside is it is not touch screen which could have made it a even better product with the new Windows OS functionality.

Good computer, bad keyboard

POSTED BY: types-a-lot , Conneaut, OH
Overall rating: 2 out of 5 2 out of 5

My previous laptop was a Toshiba as well, and I was very pleased with it, so I ordered another one. My big issue with this one is the keyboard. I have to constantly go back and fix words because letters will be missing. I purchased the laptop online, so I didn't have the opportunity to try it out. I still think Toshiba is a reliable laptop as far as performance, but I'm really disappointed in the keyboard on this model. It makes it very difficult to type. I would probably buy another one in the future, but I will definitely test the feel of the keys when typing before purchasing one again.

POSTED BY: BlueScreen , York PA
Overall rating: 1 out of 5 1 out of 5

Not a good time to talk about this...used it for almost a month..now returning it w/ Blue Screen...not happy.

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-5200M Accelerated Processor
  • Windows 8.1
  • 6GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C70 shop for accessories