Toshiba Satellite C855D-S5116 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Product

POSTED BY: Nina , Fontana, CA
Overall rating: 5 out of 5 5 out of 5

I love my laptop! still getting use to and familiarize myself with all the functions, but it's fun learning where everything is.

Very fast , easy operation , nice computer

POSTED BY: Ross , Austin Tx
Overall rating: 5 out of 5 5 out of 5

This has been a very easy computer to operate , I haven't had any freeze ups or slow starts . It has many great features , and for an older person who eirgrew up using a pen and paper it has been a breeze to learn. Well when the children let me use it , two college and one senior level , it is fast enough for their games , movies and music , and even sometimes their homework, I really enjoy it compared to some of the top name brands, it is a great computer with a great price

Toshiba laptop

POSTED BY: Nitro , Texas
Overall rating: 5 out of 5 5 out of 5

I have bought 4 Toshiba laptops of the last 5 years. All have performed very well, and reliable products. The price for such a quality product is superior to most on the market.

Great Laptop.

POSTED BY: Smiley , Lawrence, KS
Overall rating: 5 out of 5 5 out of 5

The Toshiba computer is very nice with a large screen, good battery life and lightweight. The only thing I don't like is the Windows 8 programming. I personally think it is hard to navigate from program to program, but I like the computer itself.

Nice laptop

POSTED BY: HAPPYGATOR , Jacksonville, FL
Overall rating: 5 out of 5 5 out of 5

Nice laptop, good features. Windows 8 a complete surprise.

Good buy

POSTED BY: Bandit , Yerington NV
Overall rating: 5 out of 5 5 out of 5

Overall, the price to feature ratio was excellent. Good speed and performance for the lower end price range. Great connectivity options and expandable.

Great laptop.

POSTED BY: Don , Milwaukee, WI
Overall rating: 5 out of 5 5 out of 5

I love the computer and the only problem I am having is getting used to Window 8. I will accomplish that and then all will be well.

Very nice Laptop

POSTED BY: Autumndust , Winsted, CT
Overall rating: 5 out of 5 5 out of 5

Still learning, but this easy to use.

Excellent Value

POSTED BY: aparrish3 , Durham, NC
Overall rating: 5 out of 5 5 out of 5

It is hard to beat this computer for price and processor as well as the ability to upgrade the RAM. I upgraded this laptop to a full 16 Gigabytes of RAM. Performance is excellent. I would recommend this computer to anyone. I would suggest to anyone compare the price plus adding the extra RAM to off the shelf computers with 16 GB RAM

replacement computer

POSTED BY: nicky , Detroit mi
Overall rating: 5 out of 5 5 out of 5

I have heard good things and bad things about Toshiba and I have been pretty impressed with this computer.

THE laptop

POSTED BY: happybirds , Baltimore MD
Overall rating: 4 out of 5 4 out of 5

It took me a while to get used to a laptop keyboard as I've never had one before, but as the days go by I'm getting better at it! This is a nice little laptop and quick. Overall I'm quite please with it and would purchase it again.

POSTED BY: sakari26 , florida
Overall rating: 4 out of 5 4 out of 5

I am enjoying my new laptop. The only problem is getting used to Windows 8. Have not had any problems with the computer itself.

Laptop Love

POSTED BY: Sassy , Texas
Overall rating: 4 out of 5 4 out of 5

However, I'd rather have had the option to have another operating system. 2nd Toshiba laptop I've bought.

toshiba laptop

POSTED BY: OH Football mom , oak hills ca
Overall rating: 4 out of 5 4 out of 5

has a lot of features that make it fast not really a fan of windows 8 but i'm sure that it is because it is so different than other windows programs not a fan of no document applications without purchasing separately but that is not toshiba's fault but microsoft's way of getting more money out of the consumer

Great Laptop...

POSTED BY: Cass , Istra
Overall rating: 4 out of 5 4 out of 5

Overall, I am satisfied with my new laptop. The only complaint I might list is the cheap plastic keyboard.

Toshiba laptop

POSTED BY: Mike , Lakeland Fl
Overall rating: 4 out of 5 4 out of 5

Bought this computer while on vacation in NY so far has been very good and easy to use .Windows 8 has taken a. little while to get use to but is ok This is my second Toshiba laptop and no problems yet with either

OK Laptop

POSTED BY: MommyD , Longmont, CO
Overall rating: 4 out of 5 4 out of 5

For the money it's what I expected. Have been having problems with the keyboard, sometimes the key doesn't push down. Will have to contact Toshiba to have this fixed. Will also have to get used to Windows 8 --- but that Is just new technology to learn. This is my 2nd Toshiba, wish the battery lasted a bit longer

First laptop

POSTED BY: Miss Diva , Albquerque, New Mexico
Overall rating: 4 out of 5 4 out of 5

this laptop is really nice

good value for $ spent

POSTED BY: Den , Nashville TN
Overall rating: 4 out of 5 4 out of 5

Overall very happy this is the second Toshibia I have purchased my old lap top is still running and going on 8 years old.

so-so laptop

POSTED BY: ivy , north hollywood, ca
Overall rating: 4 out of 5 4 out of 5

thats why i bought this laptop because of the brand, toshiba. i need to replace my old laptop. i just need a laptop that is so user friendly, proficient, has strong and longer battery life, fast and has big memory and of course, versatile. except for one, the internet of this laptop sometimes fails. how would i know that? i have two laptops, and an ipod. i am using them simultaneously but this laptop fails to advance with the internet while my ipod is not stopping. so even if its new, it fails. maybe this model lacks something, but its definetly fails sometimes. battery life is 3 hours.

My Laptop

POSTED BY: Meemaw , Ft. Myers, FL
Overall rating: 4 out of 5 4 out of 5

This is my second Toshiba laptop, and I find it easy to use and very reliable. I used my first one to train nurses how to use a large computer program, and actually worked the keys to death.

Keyboard

POSTED BY: runner , Las Vegas
Overall rating: 3 out of 5 3 out of 5

Only thing I want to say is I don't like the keyboard. Seems as though I have to strike really hard on some keys to get the letter or punctuation to show. I had another Toshiba and that was fine. This one feels like a cheaper model.

Battery life is very poor.

POSTED BY: Fryier , Ayer Massachusetts
Overall rating: 3 out of 5 3 out of 5

No one could tell how long the battery life was prior to me buying the lap top. Nor did I see anywhere in the on line info of how long the battery life was. I have come to find out the battery life is only apox 2 hours. If I had of known the life was so short I would never have bought this computer.

speakers are annoying

POSTED BY: Nanny , Warren,OHIO
Overall rating: 3 out of 5 3 out of 5

This laptop is fine for light use.

POSTED BY: doesnt matter
Overall rating: 3 out of 5 3 out of 5

It is a decent computer for the price, but nothing special. I don't like the keyboard, it is difficult to type without typos.

good laptop

POSTED BY: Topaz , Jamaica, New York
Overall rating: 3 out of 5 3 out of 5

The laptop is a good laptop. The only problem I have is that it takes long to turn on. there is a problem with the turn on switch.

Pretty Good Computer

POSTED BY: Effy
Overall rating: 3 out of 5 3 out of 5

The general laptop is very good, i really love the size of it. A few things I don't like are one, how shot the battery life is, and two sometimes when using the track pad, it ru makes the sidebar menue pop and that gets kind of annoying.

new windows

POSTED BY: sanman , toms river nj
Overall rating: 3 out of 5 3 out of 5

laptop is excellent but new windows 8 is a headache

great for the price

POSTED BY: jimmie57 , Atlanta, GA
Overall rating: 3 out of 5 3 out of 5

It is a good laptop. It has the speed that I expect from an AMD cpu. the only problem is not Toshiba fault and that is windows 8 switches from desktop to start page on its own

OK machine

POSTED BY: Ike , eastern Pennsyylvania
Overall rating: 3 out of 5 3 out of 5

This is my second Toshiba laptop. It is OK, but: liked first one better! Windows 8 drags the new laptop down. Much harder to get around and touchy to use. As usual though it is a tough machine that can handle my abuse, however at times windows 8 nearly drags me to frustration that could result in a hammered or thrown laptop!

Horrible sound

POSTED BY: Lemgo , Southern VT
Overall rating: 3 out of 5 3 out of 5

The speakers are tinny, sound quality is awful. I hate Windows 8!!!!!!!!!!!! The speed seems adequate.

wifi-BAD

POSTED BY: Me , roswell, ga
Overall rating: 2 out of 5 2 out of 5

Not sure if its the PC or Windows 8 but I cannot keep WIFI running with out turning off pc and the router. It works once I turn the router back on then the PC but the next day I have to do it all over again. I have 3 other pc on the same router and they work fine. so its the pc or windows 8

Windows 8 is horrible

POSTED BY: Denise , New Jersey
Overall rating: 1 out of 5 1 out of 5

I have had many Toshiba laptops and this is the worst. Windows 8 is the most user UNFRIENDLY system. Can I blame Toshiba? Don't know, but I am thinking of installing Windows 7.

Wifi problems

POSTED BY: maddie , New York
Overall rating: 1 out of 5 1 out of 5

This computer has some wifi problems. Although I have just bought a new, stronger router and updated my signal to the highest possible and despite all 5 bars in wifi connection icon, it still takes 15-20 minutes to open the page sometimes. very frustrating!!! Restarting it doesn't help either. Don't know where the problems is, but it makes me wanting to throw it down the window. Other features are ok, but this wifi connection problem should be resolved by Toshiba people. And yes, hate Windows 8....do any tech people read these reviews?

MSRP: $437.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core A6-4400M Accelerated Processor
  • Windows 8
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)

shop for accessories