Toshiba Satellite C875D-S7120 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Product

POSTED BY: Peaches , West Helena,Ar
Overall rating: 5 out of 5 5 out of 5

The battery life could be better.

best laptop awesome company..

POSTED BY: tc , east brunswick nj
Overall rating: 5 out of 5 5 out of 5

i love my laptop it is great.my last laptop was a toshiba,i got in 1994,i had it for 13 years.the screen died so i had to get a new one.toshibas are awesome!!!!!!!

Great Laptop

POSTED BY: Grammy , Pattonville ,Texas
Overall rating: 5 out of 5 5 out of 5

This is the second Toshiba laptop I own.I have owned other Toshiba products before and was always satisfied.

Best Laptop Ever!

POSTED BY: MrsCSmooth , Detroit,MI
Overall rating: 5 out of 5 5 out of 5

I love the features of this laptop. I love the ease of use and how everything is accessible right in front of you. It easy to carry with you where ever you go and light weight. This is truly the best laptop I have ever had and would reccomend it to everyone! Thanks Toshiba!

Best laptop ever

POSTED BY: Musical Mom , Republic, MO
Overall rating: 5 out of 5 5 out of 5

So far so good like the bryan adams album.

90% perfect

POSTED BY: AnnieOakley , cozad ne
Overall rating: 5 out of 5 5 out of 5

This laptop has everything a general users wants. I watch streaming movies and shows. Play music and games, all with great ease. Only problem I have is the DVD drive. It seems to be made for a left-handed person. The button is hard to locate and press. I have to reach my right arm over the keyboard to get the right angle and pressure to trigger the opening.

Not badfor older slower user

POSTED BY: Old school , Hunker Pa
Overall rating: 5 out of 5 5 out of 5

I really like this laptop. It is faster and easier to use than my first computer. My only problem is getting used to Windows 8.

Best laptop ever.

POSTED BY: Happy Fats , Okeechobee, Fl.
Overall rating: 5 out of 5 5 out of 5

It is quick fast and in a hurry. You don't have to wait for it.

I love my laptop

POSTED BY: Nina , Atlanta, ga
Overall rating: 5 out of 5 5 out of 5

I love this laptop, I really like windows 8, and all the wonderful apps.

Great laptop

POSTED BY: Collazo , Wilmington, De
Overall rating: 5 out of 5 5 out of 5

The laptop itself is great. Great picture and sound. What I hate is Windows 8. It's not user friendly at all. I hate it.

I love this thing

POSTED BY: bob , philadelphia, pa
Overall rating: 5 out of 5 5 out of 5

I have never had a better laptop in all the years I have owned a computer.

Fast and Enjoyable

POSTED BY: Dee Dee , Naples, FL
Overall rating: 5 out of 5 5 out of 5

I was amazed on how easy it was to use. A lot o programs are pre-set which makes it a lot easier to use. There is also help and other articles to read if you need it. The graphics are great. It is just a great computer.

Satellite

POSTED BY: scampi , Jersey City, NJ
Overall rating: 5 out of 5 5 out of 5

Love my laptop with the large screen and it is very easy to use.

Love it!

POSTED BY: sammy , Bullhead City, AZ
Overall rating: 5 out of 5 5 out of 5

The only thing I don't like is Windows 8.

new to toshiba

POSTED BY: md pride , baltinore, md
Overall rating: 4 out of 5 4 out of 5

this is my first Toshiba on the recommendation of an good friend I found that it exceeds y needs good d for the price and meets my needs as novice user

Cool Laptop

POSTED BY: Mark , MS near TN
Overall rating: 4 out of 5 4 out of 5

The laptop is nice. I've had it for a month and half and I am still trying to maneaveur my self around. Hope to get there soon. I need a tutorial !!!! I LIKE IT..... I just gotta learn the computer. Great Job

Very Sound Investment

POSTED BY: benadam , Washington, DC
Overall rating: 4 out of 5 4 out of 5

Aside from one problem, which Toshiba Technical Support was able to resolve very quickly, I have found the computer to be a very sound investment. My only complaint is the Windows 8 operating system; I find it very annoying and not user friendly. If I could have found a similar computer with Windows 7, I would have been much happier.

good labtop but

POSTED BY: ray , allentown pa
Overall rating: 4 out of 5 4 out of 5

i like the labtop but the window 8 i don't to much to do in the system i regred in get the window 8 i should of got the window 7

Features

POSTED BY: Lon
Overall rating: 4 out of 5 4 out of 5

First computer I've bought that did not have excel and word. For that reason I would return it I could. Very disappointed.

Great piece and price

POSTED BY: Twoshoes , West Day, NY
Overall rating: 4 out of 5 4 out of 5

I wasn't crazy about the mouse pad but fixed that with a wireless mouse. Win 8 takes a little time to get used to. I use the laptop just about everyday and it works great.

users manual

POSTED BY: gmaL , Macomb, IL
Overall rating: 4 out of 5 4 out of 5

I just wish that the computer came with a hands on user manual. I can get one on line, but since I don't have a printer yet, kinda hard for me to refer to it if I need help.

Toshiba has always been good to me!

POSTED BY: psychmajor , west virginia
Overall rating: 4 out of 5 4 out of 5

I have always liked Toshiba. They make a good and reliable product. I cannot say the same for Windows 8. They should have stuck with the old start menu. Also, I do a lot of research and use microsoft word constantly but for some reason it formats the papers differently than from windows 7. Very frustrating!!!! I should not have to go back in and re-format my work.

Laptop

POSTED BY: ymmat , Miami, OK
Overall rating: 3 out of 5 3 out of 5

It is a good product. I'm still learning it but it's a great Laptop.

key board

POSTED BY: Rosarie , Tucson, AZ
Overall rating: 3 out of 5 3 out of 5

I do not like the keyboard. Keys are too flat and I have to hit the space bar hard to get a space. Can I get an extended warranty? How? I can't find any information on it.

Hacking and Window 8

POSTED BY: Jen , Durham, NC
Overall rating: 3 out of 5 3 out of 5

Not that Toshiba has anything to do with Windows 8, but 2 hours after I filled out their online registering page for my new computer, I started to get called by Hackers that were trying to still my windows 8 software. The calls still have not stopped and I get called constantly. Windows 8 is also a drag on this computer and is like learning a different language that is meant for a touch screen. I can barely blame toshiba for Windows 8 being a pain, but i can blame them for not securing their website and letting hackers get my phone number and call at all hours of the day.

Love Toshiba products but not this particular pc

POSTED BY: Little Red , Florida
Overall rating: 3 out of 5 3 out of 5

I have had Toshiba laptops for quite some time and love Toshiba products. However. as far as this particular Toshiba Laptop I am not happy with it and wold not recommend this one at all. I find windows 8 very user unfriendly and have been struggling with it. Wound up removing everything except Windows program and started all over. Has been very frustrating. I don't like AMD either; much prefer Pentel Pentium as it seems faster. Also the speaker system is horrible! Even my old HP laptop which is over 8 yrs old has a better speaker system than this laptop. Very disappointed in speaker system.

laptop is great

POSTED BY: disappointed , russell springs,ky
Overall rating: 3 out of 5 3 out of 5

Love the laptop ,but hate the windows 8,it is so different from all others and cannot even switch back to 7.Store where I went to look at it did not have any on display, so didn't get a chance to view before purchasing.Would love to trade it for another Toshiba with windows 7.

Slow CPU, minimal Ram.

POSTED BY: Linda R , Oregon coast
Overall rating: 3 out of 5 3 out of 5

Very disapointed in the slow CPU and low Ram. I should have paid more attention to these specks versus the sale price. Only have myself to blame. I rather had spent more and got a faster computer that would be more fun to use . The new SKYPE version isn't user friendly . Lack of the "start " button is a pain. I don't like the interface of Windows 8 but all I could get . Are we really improving customer satisfaction or hindering it with so much change ? Speaker not good ! I use external speakers .

Love Toshiba HATE Windows 8!

POSTED BY: meme24 , Raleigh NC
Overall rating: 3 out of 5 3 out of 5

I bought this 2nd Toshiba laptop as a backup to the Toshiba laptop I already own & love because my warranty was running out & it needed to go in for a week long check up. As for the laptop itself I have had no problems with it but Windows 8 is IMPOSSIBLE. Having worked with computers & programs for almost 30 years Windows 8 is terrible. I hear Microsoft is going to abandon Window 8 due to all the problems, now I am stuck with a nice but almost useless new laptop! I would highly recommend Toshiba but only after Windows 8 has been replaced with an usable operating system.

Bad Experience

POSTED BY: al
Overall rating: 2 out of 5 2 out of 5

Taught Toshiba was the best second day of ownership (laptop) fan started making noises was running hot took back Returned to store after a week Had always heard of good reviews for Toshiba (maybe got a bad one it happens) don't know if i'll try Toshiba again or any time soon

Windows 8

POSTED BY: Diann
Overall rating: 2 out of 5 2 out of 5

I don't like windows not user friendly. Hearts, Spider solitaire, games like these on desk top have to pay for games if you want to down load

Slow Slow Slow

POSTED BY: FI tucson , Tucson, AZ.
Overall rating: 1 out of 5 1 out of 5

This PC is way too slow.

Wouldn't recommend

POSTED BY: Pat Pat , Redwood City, CA
Overall rating: 1 out of 5 1 out of 5

The labtop that I received from Walmart was not good quality at all. I don't know if it was defective or what, but it ran hot, the number keys on side keyboard did not operate and the overall quality I was unhappy with. The one thing that I did like was the 17" screen and that was one of the reasons I bought it, but was disappointed with the laptop performance.

Really Slow

POSTED BY: mychannie , Virginia
Overall rating: 1 out of 5 1 out of 5

This laptop is super slow and I would prefer to return it and get something faster

POSTED BY: Bets , San Marcos, TX
Overall rating: 1 out of 5 1 out of 5

Worst computer I've ever had. Slower than a snail. I mostly sit here looking at icon spinning waiting for something to appear

MSRP: $398.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E2-1800 Accelerated Processor
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories