Satellite L305-S5909

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Gift! Laptop for my B'day!

POSTED BY: Strawberrykitty , Yauco, PR
Overall rating: 5 out of 5 5 out of 5

It have everything a person need from technology. It's a great computer! economic!

The Sergeants review

POSTED BY: Sarge , jackson MS
Overall rating: 5 out of 5 5 out of 5

Great Laptop for the money, Preformance is top notch. Many of the features on this laptop are not even available on other high end brands. Highly recommend this product to my fellow soldiers.

Great Laptop

POSTED BY: NYPR , Chula Vista, CA
Overall rating: 5 out of 5 5 out of 5

I truly enjoy using this laptop. It is fast and a great companion to my desktop. The only negative is the battery life. Within twenty minutes the battery life is down to about half.

Great laptop

POSTED BY: Paul , New Mexico
Overall rating: 5 out of 5 5 out of 5

No issues and very capable laptop for the price. My second Toshiba and I have been happy with both.

My Second Toshiba And Loving it!!!!

POSTED BY: Storm , Surprise, Az
Overall rating: 5 out of 5 5 out of 5

Always buy Toshiba. They are great!!!

very good

POSTED BY: bern , tres piedras,new mexico
Overall rating: 5 out of 5 5 out of 5

it has features that my old hp did not have and i love the color the only thing i did not like is the express card slot is to close to the USB port when adding a internet access card the antenna plug blocks the top USB port

Great Value

POSTED BY: Bobh
Overall rating: 5 out of 5 5 out of 5

Up-to-date power and features at great value. Much better than the netbooks that are out.. slightly larger but much better value for the price..great sharp looking screen; DVD writable; large hard drive; wireless n, sd reader..4gb ram pushes Vista to peak performance.. Very pleased with this machine..

The Best Laptop in the market

POSTED BY: babes , guam usa
Overall rating: 5 out of 5 5 out of 5

its the best laptop i know and ive bought it in reasonable price. now we are enjoying it as far as i know,its the best.

Great Laptop

POSTED BY: JES
Overall rating: 5 out of 5 5 out of 5

For the money, you'll be hard pressed to find a more feature packed laptop. I've been extremely pleased with the performance and reliability of my Toshiba and highly recommend it to anyone looking for looking for the most bang for their buck.

Good value

POSTED BY: Len
Overall rating: 4 out of 5 4 out of 5

Basically got this to replace a stolen Dell laptop. It's a bit slower but I think that is due to the Windows Vista which I plan to replace.

Good Value

POSTED BY: Fritz , Chandler, AZ
Overall rating: 4 out of 5 4 out of 5

I am on my second TOSHIBA lap top in six years. Previously I went through three COMPAQ's in three years. The TOSHIBA offered longer lasting higher performance making it by far the better value. To be fair, while I consider the machine to be nearly bullet proof, the WINDOWS VISTA Operating System that initially performed flawlessly in a little over a month has developed compatibility problems with other WINDOWS based software I run, even software that is designed for VISTA. So, while I blame the issues I do have on Microsoft, TOSHIBA ends up with the "ownership" of the problem. The two TOSHIBA machines I have owned are loaded with features and capabilities that provide Processer power, original memory capacity and room for "growth" without overkill and paying for features that are of little use to me. For me, the TOSHIBA Satellite series is of superior value.

POSTED BY: Cinthia , Ft Stewart Ga
Overall rating: 4 out of 5 4 out of 5

The only problem I have had is the volume.U just can't hear music and DVD's.

wasted money

POSTED BY: thermaleye , Fort Lewis, WA
Overall rating: 1 out of 5 1 out of 5

this laptop's hard drive crashed after 17 days

MSRP: $899.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor P7350
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories