Satellite L305-S5918

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

its great

POSTED BY: gloria , az
Overall rating: 5 out of 5 5 out of 5

i just bought this laptop and its great, i love it

Best Computer I have ever owned

POSTED BY: Leadslinger , Pittsburg, CA
Overall rating: 5 out of 5 5 out of 5

I have owned computers since the advent of the first desk top models. I even operated a Commodor early on. The Toshiba came to the rescue as an off brand laptop threatened to destroy all of my data. The Toshiba uploaded all of my data and kept me in business just days before my old laptop crashed forever. Saved my job and my quality of life. It doesn't get better than that. Thanks Toshiba!!

Very Happy Customer!

POSTED BY: Toshiba Lover , San Diego, CA
Overall rating: 5 out of 5 5 out of 5

I received this laptop for a Mother's Day gift and the whole family is thoroughly enjoying it! We love it!

pest picture

POSTED BY: karaoke joe , rio vista, ca
Overall rating: 5 out of 5 5 out of 5

this laptop has the best picture I have ever seen on a computer.I often veiw on my tv.You cant beat the picture quality

Great Laptop

POSTED BY: Heffrey , Rio Vista,Texas
Overall rating: 5 out of 5 5 out of 5

I have not had the opportunity to realize as yet, all the features offered, however so far, I can say I would rate this Laptop as 5 star.

Excellent tech support

POSTED BY: Keith , Garland, TX
Overall rating: 5 out of 5 5 out of 5

My laptop is fantastic. What impresses me even more is the fact that anytime I call the help line for whatever reason someone answers the phone in less than two minutes and stays with me until my problem is solved. Better than that I can actually understand what they are saying!

Fourth Toshiba I have owned

POSTED BY: Kallan , California
Overall rating: 5 out of 5 5 out of 5

Best value for the money.It totally serves my needs, and for the money it will do the same for you..

My First Laptop

POSTED BY: Laptop Lover 007 , Long Island, NY
Overall rating: 5 out of 5 5 out of 5

The L305-S5918 does everything I expected it to. It's faster than my desktop computer. The screen is very clear. Vista Home Premium is a definite plus. I had one question and called for technical assistance. My call was answered immediately. No waits at all. The only negative with this computer is that it does not come with a Vista installation disk.

Really Great Laptop

POSTED BY: Camarillo Mom , United States
Overall rating: 5 out of 5 5 out of 5

We bought two of these laptops and they're great! We bought them to run some specific software. The graphics are amazing, they have plenty of memory and speed for our applications, and overall we are more than satisfied with our purchase. We got them at a great price, too.

Gotta Love this laptop!

POSTED BY: Alonzo , Los Angeles, CA
Overall rating: 5 out of 5 5 out of 5

For the economical price, to the high end features, this is one great little laptop. It has a DVD burner, a CDR, 2GB Ram, 15.5" display, HiFi land and mobile internet, and a standard 56K dial up modem all installed. Highly recommended.

Versatile Laptop

POSTED BY: Bob , Temple City, CA
Overall rating: 5 out of 5 5 out of 5

Third Satellite/Toshiba laptop owned. This laptop satisfies my needs and functions great, even after owning it for about a year. It is cheap and will suit the average laptop user's needs.

best value

POSTED BY: Augie , Houston, TX
Overall rating: 4 out of 5 4 out of 5

had a little problem verifying what a T3400 processor really was. notebook functions just as i needed it to. seems that some S5918 come with built in video. this one didn't.

POSTED BY: Steve , Canby, OR
Overall rating: 4 out of 5 4 out of 5

This is my third Toshiba. Each has served me well. I am finding it a little difficult to adjust to Vista after using 98 and XP. It seems some programs will not work with vista.

Decent Machine for the price

POSTED BY: Texas-T , Missouri City, TX
Overall rating: 4 out of 5 4 out of 5

This was an emergency laptop purchase, and I haven't regretted it. Seems solid enough. The Caps Lock key is lit when on (nice), but the right hand edge of that key sticks up too high and I'm constantly pressing it my accident (not nice). A good purchase for the price.

POSTED BY: TM , The OC
Overall rating: 4 out of 5 4 out of 5

I wanted a low cost note book to perform some basic tasks and mostly link into my work so that I did not have to be present to get work done. My L305 was a perfect solution - very happy with purchase!

Great Laptop

POSTED BY: Corbra , phoenix, az
Overall rating: 4 out of 5 4 out of 5

I like this laptop a lot. Its great for being my 2nd

Great value, great performance

POSTED BY: Tara , Sacramento
Overall rating: 4 out of 5 4 out of 5

I'm happy with the performance of this laptop and love the wide screen and easy touch of the keyboard. I feel like it's a great value for a new laptop user.

Good Laptop For Students, Not For Multi-Media

POSTED BY: Lovinglife , San Diego, CA
Overall rating: 3 out of 5 3 out of 5

Pros: (1) Low price. (2) Fast. (3) Runs cooler than our 16" HP laptop and way, way cooler than our 15.4" and 17" Dell laptops which prematurely killed one of the batteries. Cons: (1) White is not truly white. There is a slight bluish tint. (2) The speakers sound scratchy when volume is turned on high. On low - medium volume, the sound is okay but not as good as the Dells or HP. A good pair of external speakers would remedy this problem. [Side note: Something I also noticed is that music/movie sounded better when played with Windows Media Player than with Media Player Classic (K-Lite Mega Codec 4.8.9) even when both players' equalizers were set the same way.]

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories