Satellite L305-S5926

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: jo , Alabama
Overall rating: 5 out of 5 5 out of 5

Toshiba was recommended to me by a pc expert. I was leary to begin with about a laptop. I do not move same around, but I am very happy now about my pc. I certainly helped me clean off my desk top. I have not used the battery, so your question to the left was checked because your program would not let me send this to you without it being checked

Excellent Value for Laptop

POSTED BY: mompoo , DeSoto MO
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba Satellite lap top. My first one is still going and it is more than 6 years old. I like how easy it is to use the large storage capacity and the quick and easy way to get around. I had heard so many horror stories of the Vista op sys. I was surprised how easy it is to use. I would definitely recommend this produt to friends and family.

Good laptop

POSTED BY: Beth , Laverne, OK
Overall rating: 5 out of 5 5 out of 5

The only thing I do not like about this laptop is it does not have a built in mic or webcam. I like it other than that.

Good stuff

POSTED BY: Pops , Springfield,Oh
Overall rating: 5 out of 5 5 out of 5

Wish batteries that came with lap top had a longer operational time. Up to 2.28 hrs. Not a long time when away from an AC power source.

Just what I expected

POSTED BY: Alix , Chippewa Falls WI
Overall rating: 4 out of 5 4 out of 5

So far I am quite satisfied with this laptop. It does everything it claims to and is a quality laptop.

MSRP: $529.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories