Satellite L305-S5939

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great value for money

POSTED BY: John , Houston, Tx
Overall rating: 5 out of 5 5 out of 5

Battery life at High Performance is poor.

Good laptop at a nice price point!

POSTED BY: FatKat , Tracy,ca
Overall rating: 5 out of 5 5 out of 5

I bought two laptops for work and they have been working out great for us. Also recomended one for my mother and she bought 1 too and we are enjoying are new laptops! Good laptop and a nice price point!

Great Laptop

POSTED BY: Gerry , SCW, AZ
Overall rating: 5 out of 5 5 out of 5

Loaded with everything I need incl 4Gigs Memory! Worked without a hitch since purchased.

Pretty good

POSTED BY: justme , San Antonio, TX
Overall rating: 5 out of 5 5 out of 5

Overall, it's a good computer. Battery life isn't as great as it could be. But it's fast; hasn't locked up on me yet (as many computers have). I'd recommend it to anyone who uses their computer for home/some business work.

Great Laptop!!

POSTED BY: missy , Austin, TX
Overall rating: 5 out of 5 5 out of 5

Really great product, at a good price. Would recommend it to others. Excellent pircure clarity.

Excellent quality and value

POSTED BY: duke , san diego, ca
Overall rating: 5 out of 5 5 out of 5

after research, this laptop was by far the best quality and value. memory, speed and features are excellent

satisfied over the years customer

POSTED BY: gary
Overall rating: 5 out of 5 5 out of 5

this is second toshiba laptop I have owned.. first was used in business, Realtor, it finally got tired and slow like the operator and it was retired I soon followed... now have a new fast up to date toy and hope I am performing in a like manner.... Regards Gary

Worth the wait!

POSTED BY: Bwannaggee , Dallas, TX
Overall rating: 5 out of 5 5 out of 5

This proved to be worth the wait. I had been looking for some time and found the features included in this laptop. The freedom of the wireless connectivity in my home is amazing. Sitting by the pool, in the garage, in front of the TV and checking email frees up a lot of time. Only one time has the battery alarm gone off, I forgot how long I had been online. Now if we could just figure out how to make it float.

Great New Laptop

POSTED BY: Syd , Orange County, CA.
Overall rating: 5 out of 5 5 out of 5

I am really enjoying the laptop. Quick and easy. New features are easy to understand.

Over all good

POSTED BY: jc8391 , CA
Overall rating: 5 out of 5 5 out of 5

I would recommend this labtop to anyone that is looking for a new labtop for college. Also it runs most games, so its not a bad gaming computer

Can;t beat the price!

POSTED BY: Dan the Man , Baldwin Park, CA
Overall rating: 5 out of 5 5 out of 5

I got exactly what I wanted for a very reasonable price.

Easy to Use!!

POSTED BY: Droopy , Ft. Worth ,TX.
Overall rating: 5 out of 5 5 out of 5

It is easy to navigate and works fast with little adjustment from a desktop.

Toshiba's are my favorite

POSTED BY: Redcharger , Phoenix AZ
Overall rating: 5 out of 5 5 out of 5

Fast start up, fast internet connection, great performance

First Toshiba Laptop experience

POSTED BY: Jim , AZ
Overall rating: 5 out of 5 5 out of 5

So far, I love this computer!

Nice Deal

POSTED BY: Danno , Portland, OR
Overall rating: 4 out of 5 4 out of 5

This Toshiba had all the features I needed at a price that was better than I found on any other brand. I'm glad I waitied.

nice lapton

POSTED BY: Tosi , San Jose, CA
Overall rating: 4 out of 5 4 out of 5

Thanks! This laptop has been saving me a lot of time because now I can connect online at anytime.

Excellent Overall Value

POSTED BY: campacj , Seattle, WA
Overall rating: 4 out of 5 4 out of 5

This laptop should be more than enough for most business and personal computing. The most immediate suggestion I have is that a good quality graphics card, with at least 256GB of dedicated memory should be included. I think this expectation is quite reasonable for a Vista/Win7 laptop. However, even without the GC, this is a very good value considering that it can be had for less than $600. It would be hard to beat this (as of July 17, 2009).

Toshiba Laptop

POSTED BY: Richard , Las Vegas, NV
Overall rating: 4 out of 5 4 out of 5

The Toshiba Laptop computer is a great value for the money and performs excellently.

Toshiba Laptop Review

POSTED BY: GW , Chandler, AZ
Overall rating: 4 out of 5 4 out of 5

I'm happy with the ease of use, quality, and battery life.

Slower than expected

POSTED BY: teachercel , Quezon City, Philippines
Overall rating: 3 out of 5 3 out of 5

I've had several laptops prior to this one. I bought it because it had a bigger RAM & faster processor than my old one at half the price. My first laptop was also a toshiba and to date it still works so i trust the brand. I love the built-in webcam and its features. I am just a little disappointed that it seems to take longer to start-up & to process tasks than my old laptop.

Good Laptop

POSTED BY: Milou , Irvine, Ca.
Overall rating: 3 out of 5 3 out of 5

I like Toshiba Laptop, it's my second one, because it was build thin not bulky. I wish those letters on the keyboard are much brighter and easy to see. If it can come with fax software then it is awesome. The screen should last at least 6 years before it dies on us.My first one only last 4 years and I paid a lot for it; it was a special edition. Toshiba should change the look a bit different next time. Overall I would rate it a good piece.

MSRP: $679.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor T6400
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories