Satellite L305-S59512

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: Big Don , Corvallis Oregon
Overall rating: 5 out of 5 5 out of 5

To get all this at this price is WOW.

Best Laptop Ever

POSTED BY: TEE CEE , Greenville,NC
Overall rating: 5 out of 5 5 out of 5

This is my first Laptop ,my husband brought it for me so we wouldn't have to keep sharing our hm computer.It is the best I haven't been able to put it down.I Love it & would recommend it.

Good model for the price

POSTED BY: Bearman57 , Iowa City, Iowa
Overall rating: 4 out of 5 4 out of 5

Overall this is a good model. Hard to pin down the memory type to get additional memory though.

Windows Installer problems

POSTED BY: Dixie
Overall rating: 2 out of 5 2 out of 5

This computer works good except the Windows Installer Service cannot be accessed. I have spent almost three weeks e-mailing Microsoft about it. I sent two log files to them about it which they are forwarding to a specialist team. It is too bad this was not checked before they put this computer on the market.

MSRP: $468.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4200
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories