Satellite L305D-S59222

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

poor battery

POSTED BY: sunshine , ashland,ky
Overall rating: 5 out of 5 5 out of 5

i think that the battery life should be longer than it is. my battery life span is about 1 hour or less.and to me thats not good.the computer it self i love.

Good Deal for the Price

POSTED BY: Kanga Roo , Portland, Oregon
Overall rating: 5 out of 5 5 out of 5

I go to school online and this laptop is great tool that eases my stresss by working so efficient and being so reliable! I would recommend to anyone!

I love my laptop, Love it!

POSTED BY: Beamer , PR
Overall rating: 5 out of 5 5 out of 5

I Love my laptop. Everyone who sees my laptop loves it, if they use it, they love it even more. It is light weight, which is great for me because it does not harm my ailing hands. Thanks for a great product!!

Awesome

POSTED BY: Dpars , Houston,Tx
Overall rating: 5 out of 5 5 out of 5

This is my third toshiba Laptop in the family and i cannot express how happy we have been with them my Sons age 25 and 20 both use theres in college and have helped enormosly they are very dependable and the price is awesome . Thanks Toshiba The Satellite is a good buy and would highly recommend to anyone

POSTED BY: redbird
Overall rating: 5 out of 5 5 out of 5

This is a great Laptop, my first and only one i'll ever have.

No operating manuals with this unit.

POSTED BY: Movieman , Fremont,Nebraska 68025
Overall rating: 5 out of 5 5 out of 5

HELP!

Excellent Laptop

POSTED BY: Chuck , Wabash, IN
Overall rating: 5 out of 5 5 out of 5

I'm very happy with the Laptop, but prefer not to have Norton Antivirus installed.

excellent

POSTED BY: Marine , Green valley AZ, 85622
Overall rating: 5 out of 5 5 out of 5

Need carrying case for all including accessories.

Excellent reliable laptop

POSTED BY: Ed , Miami Fl
Overall rating: 5 out of 5 5 out of 5

Large clear display, well proportioned keys, fast responsive computer. Prefer to have Caps Lock key at top or right side instead of left side. Very user friendly, virtually no learning curve from XP to Vista. Good selection of programs.

Great Product

POSTED BY: G , Wichita, KS
Overall rating: 5 out of 5 5 out of 5

Connects to net flawlessly and doesn't have lockups like previous bands that we have purchased.

Great laptop.

POSTED BY: juggyrig , Mt. Pleasant, UT
Overall rating: 5 out of 5 5 out of 5

I love the bigger screne, the built-in Web-Cam with voice recording, DVD player, and available RAM plus it's other features and programs. The only thing I don't like how long it takes to turn on and get to the start or log-in menu (about a 2 minute wait). It's moderately fast once you're in though. My old computer was faster longing in (30-45 seconds) but the other features the Toshiba offers is worth the wait.

Another great product from Toshiba

POSTED BY: Opa , Dansville, NY
Overall rating: 5 out of 5 5 out of 5

Toshiba does it again with a really great Laptop. It is not only great, but a pleasure to use. It is so much fun that it just might cause a divorce (Just kidding). Keep up the great work, Toshiba!

Best Computer

POSTED BY: DJ_Lonewolfjohn
Overall rating: 5 out of 5 5 out of 5

i will tell people it one better one out there.

Excellent Laptop

POSTED BY: repairman , Pittsfield,Ma.
Overall rating: 5 out of 5 5 out of 5

I use this laptop for work on the move all the time .It does it`s job fast and never lets me down, even when I can`t plug it in to recharge.

excellent computer

POSTED BY: radio op
Overall rating: 5 out of 5 5 out of 5

very nice computer love the features!

My Toshiba

POSTED BY: djzfire , South Charleston,WV
Overall rating: 5 out of 5 5 out of 5

I am pleased with my new laptop.It is advanced enough for my needs,yet simple to use.It makes use of equipment that I already have easy to use.

Second Toshiba Laptop

POSTED BY: bert
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba Satellite, and I like this brand very much.

Efficient & User-friendly

POSTED BY: Troublesome , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

Great buy! It is even excellent for the beginner user. Been using 10 months and had not had a problem yet. Battery power doesn't last long but for the quality that can be overlooked. I love my Toshiba and I will buy another.

Absolutely No Regrets!!!

POSTED BY: Saint , Corsicana, Texas
Overall rating: 5 out of 5 5 out of 5

I purchased this laptop for school and personal use and absolutely love it! It's as fast or faster than almost every single computer I have ever used. My roommates all have laptops and it seems every day im hearing, "I had to buy that on my computer" or "it came with that on yours???". The graphics on the small amount of games i have played have been amazing and the ease of use is always a plus. I paid on the extreme low end of the scale as far as laptops are concerned but believe it could match the pricier models any day. Highly recommend!

Webmaster laptop

POSTED BY: Rockytherock , PR
Overall rating: 5 out of 5 5 out of 5

Best laptop I've ever had, toshiba has quality and a great price. Performs A++++

Totally Toshiba

POSTED BY: denden , Jacksonville, FL
Overall rating: 5 out of 5 5 out of 5

My Toshiba delivers great quality and performance. It very user friendly and I especially like the face recognition feature.

I Love My New Laptop

POSTED BY: cruzer , Greenwood, SC
Overall rating: 5 out of 5 5 out of 5

its a great product and i love it

POSTED BY: none
Overall rating: 4 out of 5 4 out of 5

I like everythingabout the computer but the mouse, it seems to be spastic. I have to move the mouse pad alot to move it a short distance on the screen or I just barely touch the mouse pad and its all over the screen.

too new to rate

POSTED BY: BrokerBen , Tucson, Arizona
Overall rating: 4 out of 5 4 out of 5

I use the laptop sparingly so my rating is probably not "qualified". My second laptop, other unit was not Toshiba and was years ago. This I purchased because PC in shop and price was right and I had an immediate "Need". I really didn't compare much. Unit probably good+, Vista I don't like, IE 8 works when it wants to (can't correct) basic instructions for unit fair - I need to use the tutitorial on web probably.

Good Value and looks good too!!

POSTED BY: Marlfrog , Burlington, WA
Overall rating: 4 out of 5 4 out of 5

Lots of features for the price. I like that I can dim the display because I read textbooks on line and don't like the bright screen. You are also able to go in and adjust power settings and increase battery life if needed. Haven't tried the web cam yet.

Still in transition

POSTED BY: DocYou , Louisville, KY
Overall rating: 4 out of 5 4 out of 5

I have had to adjust from using an XP system to the Vista system which has caused some problems. I have little natural ability to recall the many differences and apply them well. In addition, I still use my XP PC and have had to learn how to save my work so that it may be used in the XP system. The battery life issue is confusing: sometimes it will show that I have more time left on the battery than I did when I started to use it.

Laptop

POSTED BY: musicchik
Overall rating: 4 out of 5 4 out of 5

I am extrememly happy with everything about this laptop. I wish that the battery life was longer but other than that I do not have any problems.

Not impressed yet

POSTED BY: Ron , Fort Stewart, Ga
Overall rating: 3 out of 5 3 out of 5

I don't know what happened, but it won't pick up the internet

Its good but could be better.

POSTED BY: Sheek_Luch
Overall rating: 3 out of 5 3 out of 5

My only dissatisfaction, stability...

Beginners Laptop

POSTED BY: Opinion , KANNAPOLIS, NC
Overall rating: 3 out of 5 3 out of 5

The laptop is ok for a beginner, Its nothing that I would recommend for log term use. Just something to buy to start out, and pass on. The battery life is terrible.

MSRP: $529.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Athlon™ X2 QL-62 Processor
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories