Satellite L305D-S5949

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Love it.

POSTED BY: 31togo , Atlanta, GA
Overall rating: 5 out of 5 5 out of 5

I got rid of an old HP I had with much smaller screen. This laptop suits me just fine. Great display, perfect for my internet browsing, email, and a small business that I run from it! I've had for a month and no problems! Also got it at a great price!

LOVE MY 'TOSHIBA!!!"

POSTED BY: Kat , Columbus,Oh
Overall rating: 5 out of 5 5 out of 5

I love the large screen & The smooth key pad. All the features work GREAT!!

Excellent

POSTED BY: mco328 , Orlando, FL
Overall rating: 5 out of 5 5 out of 5

Good screen, good keyboard, works easily, no issues with Vista, printer drivers load easily and function. Great stuff, no issues of any kind

i love it!

POSTED BY: goldie , Atlanta, Ga
Overall rating: 5 out of 5 5 out of 5

It has everything I could want and need for school, like speed. Im very impressed by this notebook.

My first Laptop but the best!!

POSTED BY: Pinky , Garfield Hts., OH
Overall rating: 5 out of 5 5 out of 5

I know my Toshiba is a top notch laptop. I own a 32" flatscreen tv, a dvd/vhs vcr, and now my new laptop!! All made by Toshiba!! You make your products to last and serve their purpose to your fellow customers!! Thank you very much!!

Very good laptop

POSTED BY: Brutus
Overall rating: 4 out of 5 4 out of 5

So far, this is a very good product for the price! I've had it for about 2 weeks now and it has worked out very good. I'm not a gamer, but it is not designed for active gaming. I basically use it for work. Spreadsheets, word documents, ect...

Great laptop value!

POSTED BY: darasdad , Terre Haute, IN
Overall rating: 4 out of 5 4 out of 5

Great features, great price. I really like the onboard webcam. The only minor complaint I have is the touchpad. It is the same color and on the same plane as the surrounding wrist rests and there's only a slight difference in texture between the 2 surfaces. That makes it somewhat easy to stray off the touchpad, but don't let that stop you from buying this very fine laptop. Also, I would prefer a 5400 rpm hard drive, although the 4200 does seem sufficient.

so far good

POSTED BY: dogs , des moines, IA
Overall rating: 4 out of 5 4 out of 5

orver all good

POSTED BY: beans , Cleveland, OH
Overall rating: 3 out of 5 3 out of 5

I hate windows vista. I cannot load my camera software or download it. I shows in programs that it is there but it isn't and when I try to uninstall it it will not uninstall.

MSRP: $483.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Athlon™ X2 QL-64 Processor
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 200GB HDD (4200rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories