Satellite L355-S7902

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

awesome

POSTED BY: t-homas , knoxville tn
Overall rating: 5 out of 5 5 out of 5

there is nothing not to like

My 1st Toshiba

POSTED BY: Cupcake
Overall rating: 5 out of 5 5 out of 5

This is my 1st Toshiba and it seems to be okay for now. I just have to figure out the bugs.

Picture perfect!

POSTED BY: Keith B , Burlington, ON
Overall rating: 5 out of 5 5 out of 5

This is simply the best laptop! For it's price and it's power it's unbelievable! Easily runs with 3 hours of battery life, and still manages to be super fast! I would have liked this laptop in gloss and not silver, BUT I LOVE IT!

Family Recommended

POSTED BY: KAM , Santa Barbara CA
Overall rating: 5 out of 5 5 out of 5

Why did I choose Toshiba when there are so many others to choose from? Because family and friends said they had Toshiba's and they were long lasting! I wanted to get something I could have for years to come. I get tired of having to upgrade, switch and relearn. So far, I've been extremely happy!

How did I live without this laptop before?

POSTED BY: agypsywillow , Sarasota, FL
Overall rating: 5 out of 5 5 out of 5

This has been a great find for me. It handles accounting programs, the web, and design programs seamlessly. This is the computer that was recommended to me by a friend who is an IT Manager, and he told me not to buy anything else!

Great laptop

POSTED BY: Greg , OH
Overall rating: 5 out of 5 5 out of 5

Great laptop for the value. Could have used some more popular pre-loaded software, but overall it's a very good product.

The Toshiba Experience

POSTED BY: Senior Chief , Eugene, OR
Overall rating: 5 out of 5 5 out of 5

This is by far the best Toshiba I have owned. I have owned Toshiba Laptops since 1989. My first was a "286" with 20 mb hard drive. It got me started with Toshiba and I have owned 10 more Toshiba Satelites since then.

LOVE IT

POSTED BY: tee , Columbia SC
Overall rating: 5 out of 5 5 out of 5

For a long time I didn't like the satelite laptops but having purchased one this machine rocks!! I love the way the keys are luminecent at night where even laying down i can still see what I type. The battery is great i have no problems using it for the 2 hours or longer with out the cord. I really love that this machine does not get flaming hot after being on for a long time, my old one would get hot within the first 30 minutes of use this one is so cool to touch. I just have to get a little more familiar with vista other than that I'm happy with my purchase and highly reccomend this product!!

Toshiba Laptops are best in class

POSTED BY: HDTony20 , Greenville, SC
Overall rating: 5 out of 5 5 out of 5

I have worked in the tech field for many years, and Toshiba Laptops vs HP, Sony or other brands. When you rate them Toshiba has the best in class, when you look at the series, best Laptop for the money and customer service. Try calling HP or SONY, them you will understand

very good machine for the money

POSTED BY: cragor , wichita, ks
Overall rating: 5 out of 5 5 out of 5

very slick machine. would like to have a little longer battery life. otherwise i am very happy

great laptop

POSTED BY: mayerdarwin1 , springfield MO
Overall rating: 5 out of 5 5 out of 5

i wish that it had a built in bluetooth

Great Value Laptop

POSTED BY: Joe , Glenside, PA
Overall rating: 5 out of 5 5 out of 5

I was somewhat skeptical about the product considering the reasonable price, however, after using the laptop and all its' features I was truly impressed. I like the built in web cam, and the label flash, both work well. There is plenty of memory and storage and the speed is impressive. The wireless connection setup is fast and reliable. I would definetly recommend this computer.

POSTED BY: kim
Overall rating: 5 out of 5 5 out of 5

.There is nothing not to like. It's the best PC I've ever had..

Very Good Laptop

POSTED BY: Gene , Greensboro, NC
Overall rating: 5 out of 5 5 out of 5

I had been watching this laptop at a local retailer for about 6 months. It had the features and capacity I needed for accessing work while away from the house and work environment. I finally took the plunge and bought it when I was going to be out of town for a few days. It has proven to be all that I was hoping it would be - a strong and capable machine with good capacity and versatile connectivity capabilities. The large size took a little getting accustomed to but that is no longer an issue. The on board web cam came to life very easily and proved itself to be reliable the first time I turned the machine on. I'm glad I purchased this machine.

Good product for the money

POSTED BY: MsPiggy , Rainier, OR
Overall rating: 5 out of 5 5 out of 5

This is a wonderful computer. I bought it after I had surgery and couldn't sit at my desk top. There are only 2 things I don't like. 1. The Wild Tangent games that can interfer with other programs on the computer and it operation. The Microsoft ones are fine 2. Adobe Reader/Acrobat was an OLD version and wouldn't open any pdf files on line. The folks at Adobe fixed my problem and everything is fine now. Would I buy another--absolutely! It is also fairly light weight all things considered.

A wonderful Machine

POSTED BY: Digit Al , La Pine, Oregon
Overall rating: 5 out of 5 5 out of 5

The best feature is thew on-board numerical key pad

Awesome laptop, short battery life

POSTED BY: Bay , Battle Ground, WA
Overall rating: 5 out of 5 5 out of 5

I bought this laptop to aid with schooling, the laptop is awesome, except the battery life is short, typically only about an hour and 30 minutes. It is quick to recharge, but it's still frustrating. It has all the features I was looking for, and it's quite fast, even though I've filled 3/4 of the memory already. It DOES show fingerprints and the casing scratches easily but other than those few thins, it's awesome. Fast, reliable and user friendly.

POSTED BY: lonestar , Lubbock, TX
Overall rating: 5 out of 5 5 out of 5

dont like the limited use of microsoft word

My Very Favorite

POSTED BY: SuziQ , Lawrenceville, GA
Overall rating: 5 out of 5 5 out of 5

I loved my Toshiba television so much that I had to buy the Toshiba laptop and now have a Toshiba HDTV. I am very pleased with the product, the reliability and it's capabilities. My favorite feature is the radar for networks. I easily became accustomed to Vista and everything this laptop offers. The speed, the graphic quality, the sound quality and storage capacity. I have had several other brand laptops in the past and will never buy anything but Toshiba.

I GAVE MY DELL AWAY

POSTED BY: ren , Gary, IN
Overall rating: 5 out of 5 5 out of 5

This computer was so cool and performed so well, I gave my Dell away. This is now my primary computer and I love it. It was well worh the money!

Best Lap Top...I Love it !

POSTED BY: Photography By Jim , Rio Grande, New Jersey
Overall rating: 5 out of 5 5 out of 5

I have two other Lap Tops both HP, this Toshiba runs circles around them...I Love it it is the only one I use...Cab do so many things so fast and battery time is much better. Should have bought a one a long time ago

Big step up from my Dell.

POSTED BY: magic , Trinidad & Tobago
Overall rating: 5 out of 5 5 out of 5

Bought three for our managers. We are all satisfied. Great Product @ an excellent price!

great product

POSTED BY: shari , sylmar,ca
Overall rating: 5 out of 5 5 out of 5

this is a great laptop, excellent features. i would recommend it to anyone.

Good Laptop

POSTED BY: Mark , Texas
Overall rating: 5 out of 5 5 out of 5

About 3 months ago, I purchased this laptop to replace a HP laptop that never worked right even when it was new. This Toshiba laptop has worked good so far. It cost about 50% less than the HP and is more than twice as good !

Solid Value

POSTED BY: Wllrdqn4
Overall rating: 5 out of 5 5 out of 5

This laptop continues on with the performance and solid construction that I have come to expect from having had 2 previous Toshiba Laptops and 1 PDA. I have had no hardware issues or software hangups, and I am totally satisfied with this purchase.

Best Laptop Ever for the Money!!

POSTED BY: HB , Lexington, OK
Overall rating: 5 out of 5 5 out of 5

Best features available and easy to use!!!

Great Laptop but Touchpad isn't.

POSTED BY: Swabby , Norfolk, NE
Overall rating: 5 out of 5 5 out of 5

Touchpad is too sensitive. DVD causes growl at speed

My Other Half...

POSTED BY: liljaywizzle85 , Baton Rouge, La
Overall rating: 5 out of 5 5 out of 5

Toshiba has the best products ever. Way better than ''Dell''.

First one to own

POSTED BY: Foxx , Orange, NJ
Overall rating: 5 out of 5 5 out of 5

I caught this computer as a refurbish from Toshibadirect for a great price and it looks, performs, and is an excellent product!!!!!!!!!!!!!!! Foxx

Competetively designed

POSTED BY: Dimples , Chino Hills, CA
Overall rating: 5 out of 5 5 out of 5

I recently purchased a Toshiba L355-S7902 laptop and have been very happy with it. The unit was reasonably priced and it had the features I was looking for.

Great Laptop

POSTED BY: Karen , Boise, ID
Overall rating: 5 out of 5 5 out of 5

This laptop is easy to use and has a great screen for easy viewing.

my laptop

POSTED BY: lynn , copperas cove, tx
Overall rating: 5 out of 5 5 out of 5

this is my frist laptop& i like it quite well,

Very happy with this PC

POSTED BY: Bill , Union, KY
Overall rating: 5 out of 5 5 out of 5

Very fast and easy to use.

ease of use!

POSTED BY: Sweetpea , Jacksonville, NC
Overall rating: 5 out of 5 5 out of 5

This laptop has been so easy to use, and I really do enjoy the built in keypad on the side! probably one of the best laptops I have ever owned! was not a huge fan of Window's Vista in the past, but for some reason it works much better on this system!

Very nice

POSTED BY: nczim , Greensboro, NC
Overall rating: 4 out of 5 4 out of 5

It is LARGE (more like a portable desktop with a built in monitor than a laptop!) - I like the 10 key pad built into the keyboard, it is very fast. Screen is nice and large. I like the built in media port for SD camera cards... so far no real negatives.

Life changing gift

POSTED BY: Bob , Tucson,AZ
Overall rating: 4 out of 5 4 out of 5

At 83 learned the basics of a computor so I could play games instead of sitting in front of the TV all day. A friend enlarged the print and cursor to help with my failing eyesight. It has given me a very different outlook on life!

Almost perfect

POSTED BY: amy
Overall rating: 4 out of 5 4 out of 5

My keyboard is my only complaint. i can't get a capitol letter by holding down the shift key. this makes it hard when my email address is my password, because i can't see if the @ sign 'took.' When typing i have to turn the cap locks key on and off to get capital

Excellent unit

POSTED BY: Vic , Macclenny, FL
Overall rating: 4 out of 5 4 out of 5

For the price this unit has given me excellent service and features. I purchased the unit to access the internet when I lost one of my main desktops due to a lost drive in a Raid 0 array. It performed flawlessly during the many weeks it served as a replacement. It also enabled me to record and save business transactions while it was in use. Not being used to laptops I thought that the battery storage time was somewhat short but sufficient for my usage. It is heavier than I other units I have used but the 17" screen more than makes up for the weight factor. I am pleased with the unit.

My first Laptop

POSTED BY: HBJan , Orange County, CA
Overall rating: 4 out of 5 4 out of 5

I have always had a desktop. This is my first laptop. I did A LOT of research before choosing a Toshiba and did so because of their reputation & the other reviews I read. So far I am VERY happy w/my new Toshiba/only wish the battery would last longer. But I can live w/that.

Great laptop

POSTED BY: dwim , Fairborn, Ohio
Overall rating: 4 out of 5 4 out of 5

I have purchased 2, one for me and one for my wife so she can do her own stuff, and we are both really enjoying the product. Our only beef is the standard battery life which is only two hours, but other than that, everything is really good.

Very nice lapton for the price

POSTED BY: Nata
Overall rating: 4 out of 5 4 out of 5

I love the features and the look of this laptop. It runs very fast and without any problems. Has great memory too. The only thing I wish was different is the volume. When I watch a DVD or presentations I wish volume was a little higher. I am very multi task, and do several things at the same time. I don't have the time to sit and watch a presentation, which I need to do for school and office. The volume on this laptop is very low, I have to sit and pay attention to hear those presentations

nice laptop

POSTED BY: jabbu , tn
Overall rating: 4 out of 5 4 out of 5

It's really good and the speed is excellent above my last Toshiba laptop..I only wish when you purchase a computer they would give you ALL the software discs that come loaded on them...

3rd Toshiba laptop

POSTED BY: moonman , Orange,Texas
Overall rating: 4 out of 5 4 out of 5

Seems to be fast enough,had trouble making recovery discs,so ordered same from toshiba,only used for three weeks so don't have a solid background as yet

Real neat laptop

POSTED BY: Chuck , Tulsa, Oklahoma
Overall rating: 4 out of 5 4 out of 5

I was very impressed with my Toshiba L355-S7902. It is powerful and yet easy to use. When I leave town, it goes with me so I can keep in touch with my PC in my office.

More bang for less bucks!

POSTED BY: rev.spike , Kansas City
Overall rating: 4 out of 5 4 out of 5

The L355-S7902 was recommended by a friend of mine who heard that I was about to go Mac. All in all, you would be hard pressed to find better value for your computing dollar. The processor and factory memory are more than ample to run all my applications without a hiccup (including Media Shout, a very demanding media program I use for sermons). I would have liked to see an HDMI port and a more sturdy feeling keyboard, but otherwise, this is one amazing machine. My wife has the 15" version of this notebook and she is equally thrilled. I feel a lifetime customer relationship with Toshiba coming on.

Very good laptop

POSTED BY: golfgeek , Cupertino, CA
Overall rating: 4 out of 5 4 out of 5

It has everything I need. I know its the normal design that the space between keyboard and front edge of laptop is so deep but it would certainly help my wrists if the space was it least 1/2 of what it is presently. Would like 4g RAM rather than 3g and lighter in weight.

large, but nice!

POSTED BY: Paul , Maimi, Fl
Overall rating: 4 out of 5 4 out of 5

Purchased this product for features and size, as I wanted a number pad on the key board. Pretty happy with the product and it's user friendly features

only one thing I would like to have is bluray play

POSTED BY: LARO , New York, NY
Overall rating: 4 out of 5 4 out of 5

Love my PC but like I said, I would like to know is there is a upgrade to be able to download for my PC / laptop

Good product.

POSTED BY: bbsjust4me , Kansas City, KS
Overall rating: 4 out of 5 4 out of 5

Had bad experiences with HP so I'm trying something new.

Good laptop for work vehicle

POSTED BY: Gracie , Crestview Fl
Overall rating: 4 out of 5 4 out of 5

Been pleased so far with this laptop. I use it for a small business and have it mounted in my van. Battery life stinks though.

si so

POSTED BY: mastertignes , lakewood,co
Overall rating: 3 out of 5 3 out of 5

a medium laptop top a hight price to much software inside when you buy and this last one use to much memory.

Kinda Clunky

POSTED BY: Ray , Monterey, Ca
Overall rating: 3 out of 5 3 out of 5

I bought this laptop for going to school and getting my Masters Degree. It is Ok...kinda clunky compared to some of the laptops my friends have. You can't hook it up to a Plasma TV...or atleast I can't figure out how to do it. Overall, you get what you pay for with this unit...nothing more!

Not the best at all.

POSTED BY: ynit1
Overall rating: 2 out of 5 2 out of 5

DVD drive runs hard and very loud. Most laptops does not do this.

Worst Laptop I've ever owned!

POSTED BY: Dunewoman
Overall rating: 1 out of 5 1 out of 5

There is nothing about it I like ... I'm just sick that I spent money that I really couldn't afford and that this is the result.

MSRP: $649.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 3GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories