Satellite L505D-ES5025

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Toshiba Tested, Tried, Likes-Dislikes

POSTED BY: rl , Orange County, Ca.
Overall rating: 5 out of 5 5 out of 5

Great graphics, love the OS windows7 Norton security is not liked by me as are many other PC users I talk to, Battery is Poor to Good on a fresh charge up 3.36 reads I actually get 1.5 to 2hrs before powered down occures, love everything else Toshiba has built! Great is Face log on feature You could increase battery life by twelve cell battery which gives 5 hrs. DC usage and should be a must in this model overall very happy otherwise for the value and performance packed inside this Toshiba L505D-ES5025

Dependable, easy to use

POSTED BY: Margaret , Mason City, Iowa
Overall rating: 5 out of 5 5 out of 5

Great laptop for school, easy to use for beginners in the household. Keyboard is great but primary and secondary control buttons could be more durable. Battery life could be better but overall for the price and Toshiba's reputation for laptops it's great!

Good Laptop For the Price

POSTED BY: Necrosis , Austin, Tx
Overall rating: 4 out of 5 4 out of 5

This is a Great Laptop for the Price. The only thing hardware wise it could use is a Better Video Chip. But this laptop plays games fairly well. Software side of things I would have been happier if it had not come with Symantec Norton Installed since is is only a 30 days trail and it is extremely difficult to remove Norton Products as far as am concerned this computer came with a virus Named Norton install on it. But other than that A Great Laptop.

Nice laptop

POSTED BY: Ren , ND
Overall rating: 4 out of 5 4 out of 5

Overall I really like this laptop. The keyboard is very easy to use, the video is good for a laptop, and performance is also good. But the sound is terrible. At full volume, it is still difficult to hear at times, and has a very "tinny" sound. That was a major disappointment. Otherwise I am enjoying the laptop.

MSRP: $629.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ II Dual-Core Mobile Processor M520
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 800MHz memory
  • ATI® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive

shop for accessories