Satellite L505D-S5996

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: grandma , Greencastle,Pa.
Overall rating: 5 out of 5 5 out of 5

I have just had this a month,and also went from dial up to high speed at the same time I got this laptop(my first Laptop) So far I think it is wonderfull.

love it

POSTED BY: cj , wilson nc
Overall rating: 5 out of 5 5 out of 5

Great laptop

POSTED BY: amram , Marion, NC
Overall rating: 5 out of 5 5 out of 5

I chose a Toshiba laptop as a replacement for my three year old Compaq. Thus far, I haven't been disappointed. It is fast and Windows 7 is easy to navigate. The processor does get warm, but in the wintertime that is a positive. Occasionally I do have difficulty connecting with my wireless router, but I believe that is an ISP problem, not a computer problem.

Best Laptop for the Price

POSTED BY: Tookey
Overall rating: 5 out of 5 5 out of 5

I have used laptops and desktops for many years and I love the Toshiba and the way it is set up. The customer service is just fantastic to work with and very knowledgeable about there products.

Great little work horse!

POSTED BY: edge61 , Doylestown, Pa
Overall rating: 5 out of 5 5 out of 5

This is my 3rd laptop and I am glad I got it. I am a full time student and when I'm tired of sitting at my desk top, I grab my laptop and stretch out on the couch. It is fast and even with 5 to 10 apps running at once there seems to be no loss of power and performance, great on line no crashes in the middle of a posting. It does get warm and the dvd/cd drive can be noisy. I am sorry I didn't wait till after the holidays, its going for way less then the $479.00 I paid for it!

It is a very good Laptop!

POSTED BY: lace , NY
Overall rating: 5 out of 5 5 out of 5

I'm lovin' it

POSTED BY: madhatter , NC
Overall rating: 5 out of 5 5 out of 5

For the money, this laptop has all the features I need. It doesn't have a modem, though I would like to add it if I could. The screen is bright and good sized. Having the webcam is a plus. It has good speed and runs all the apps I normally use. So far I have not been disappointed in my choice.

Very good laptop!

POSTED BY: hineski , Nashville, TN
Overall rating: 5 out of 5 5 out of 5

Everything about this laptop works great, and especially the Wi-Fi feature. The processing power is very good and fast. The screen is crystal clear with beautiful colors. The keyboard has a nice touch. Overall appearance is pleasing to the eye. All in all, I love this laptop. It was reasonably priced and is a very good value in my opinion.

My Christmas Gift

POSTED BY: t-bone , philadelphia PA
Overall rating: 5 out of 5 5 out of 5

I am very pleased with this laptop . . . easy to use, sleek design and all thats built in!!

Great Laptop

POSTED BY: blgrtooth45 , PA
Overall rating: 4 out of 5 4 out of 5

This is my first laptop purchase. I am overall happy with this product; however, the battery life is only fair and lasts about 2 hours. Otherwise, this is a great product at an affordable cost.

still working on it

POSTED BY: Siberia503
Overall rating: 4 out of 5 4 out of 5

I am frustrated at how sensitive the keyboard is and the cursor keeps jumping around when I don't want it to. Sentences will disappear if I lightly touch the part where the hands rest. I have had to start over many times.

DISAPOINTED IN LAPTOP

POSTED BY: wolf , ft mitchell ky
Overall rating: 3 out of 5 3 out of 5

THE VOLUME AND SOUND QUALITY IS PITIFUL THE BATTERY LIFE IS SUPPOSE TO BE 2 HOURS IM LUCKY IF IT LAST AN HOUR..THE START REGISTRY ON START-UP TAKES EVERYBIT OF DUAL CORE PROCESSOR TO EVEN SURF THE WEB

MSRP: $579.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ II Dual-Core Mobile Processor M500
  • Windows 7 Home Premium (32-bit)
  • 3GB DDR2 memory
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories