Satellite L555-S7929

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Pleased with performance!

POSTED BY: Dennis , Fleetwood, PA
Overall rating: 5 out of 5 5 out of 5

Was pleased to get so much computer for so little cost. I am still learning the features with the installed Windows 7. Have no problems to report after not quite three weeks use. Battery life seems to be really good - showed 45% remaining after almost three hours use.

Fantastic!!

POSTED BY: Bry , TEXAS
Overall rating: 5 out of 5 5 out of 5

Wow!!!! This l.t. rocks!!! Cant get my family off this thing! Super slim and it is so Fast!! Love the keys and also the screen is so BIG!!!! Games are the bomb and surfing the net is a snap! GREAT PRICE AND BEAUTIFUL PRODUCT!!!

i love my lap top

POSTED BY: steppie , campobello south carolina
Overall rating: 5 out of 5 5 out of 5

i love my lap top it is a great laptop i would recommend this product to a friend i was very excited when i get mine for christmas.. and i love it so much....

Toshiba, from VCR to Laptop. Always Great!

POSTED BY: Shell , Optima, Ok
Overall rating: 5 out of 5 5 out of 5

Twenty some years ago my husband bought a Toshiba VCR the best one we ever owned. We have owned several different brands since it finally bit the dust (we can no longer find Toshiba Brand media players in our area) nothing compares to the picture quality or the durabiliy of a Toshiba. I have been shopping around for over two years for a laptop and when I found one at a local retailer i didn't hesitate, it exceeded my minimum requirements and I purchased it on the spot sight unseen (they had just recieved them in and had not put one on display yet). I have not been disapointed. It is easy to use, preforms quite well, and I truely enjoy the picture quality while watching the occational DVD. BRAVO Toshiba I look forward to many years enjoyment with my new laptop!

Best laptop yet

POSTED BY: nate , Waialu,a HI
Overall rating: 5 out of 5 5 out of 5

This is my fifth laptop and my second Toshiba, I would like to share the fact that this is the best laptop i have ever had. it is trouble free fast and the windows 7 is just wonderful. this system is used every day all day and is used as our entertainment center after hours, this is a true work horse i could not be more happy with this system, as an architect i use this system to draw plans and give 3d walk through to my client,s thus far i have not had a system that could handle all that and then go home and be the mainframe for our entertainment system and be my personal pc, this system handles all of this and then some. I would highly recommend this system to everyone as it is the best work horse to date, Toshiba has rely out done the competition as far as i am concerned.

Pretty Good

POSTED BY: CustomFifteen , St. Marys, Ohio
Overall rating: 4 out of 5 4 out of 5

I've got to say, this laptop is pretty amazing. It can do so many things! The battery lasts for quite awhile and it helps me get my stuff done. Overall, I would definitely recommend this to a friend.

Excellent bang for the Buck

POSTED BY: Stroker396
Overall rating: 4 out of 5 4 out of 5

I upgraded from a very old Toshiba but it was top of the line at the time. While the performance, screen size and features are excellent I can say that the keyboard feels very cheap the speakers are poor with a tinny sound relative to the old machine. I blame part of the sound on Win 7 a real equalizer could likely help (not predetermined settings) But those are the trade offs for the price.

Terrible Laptop

POSTED BY: dennie
Overall rating: 2 out of 5 2 out of 5

Purchased computer one month ago and it freezes every time that I use it. my husband has a Dell and it is great. Never will I but another Toshiba and I will warn as many friends as I can

MSRP: $614.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4300
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 memory
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories